AM62x MCU+ SDK  09.00.00
RTI Functions

Introduction

Functions

int32_t SDL_RTI_config (SDL_RTI_InstanceType InstanceType, const SDL_RTI_configParms *pConfig)
 RTI configuration API. This API configures the specified RTI instance using the provided configuration. More...
 
int32_t SDL_RTI_verifyConfig (SDL_RTI_InstanceType InstanceType, SDL_RTI_configParms *pConfig)
 RTI API to verify the written configuration. This API can be used after calling SDL_RTI_config in order to verify the configuration. It reads back the configuration from the registers and compares it with the provided configuration. More...
 
int32_t SDL_RTI_start (SDL_RTI_InstanceType InstanceType)
 Enable the RTI instance. More...
 
int32_t SDL_RTI_service (SDL_RTI_InstanceType InstanceType)
 Service the RTI instance. More...
 
int32_t SDL_RTI_clearStatus (SDL_RTI_InstanceType InstanceType, uint32_t status)
 Clear the DWWD status. More...
 
int32_t SDL_RTI_getStatus (SDL_RTI_InstanceType InstanceType, uint32_t *pStatus)
 Clear the DWWD status. More...
 
int32_t SDL_RTI_readStaticRegs (SDL_RTI_InstanceType InstanceType, SDL_RTI_staticRegs *pStaticRegs)
 This API returns the static registers for RTI-DWWD. More...
 

Function Documentation

◆ SDL_RTI_config()

int32_t SDL_RTI_config ( SDL_RTI_InstanceType  InstanceType,
const SDL_RTI_configParms pConfig 
)

RTI configuration API. This API configures the specified RTI instance using the provided configuration.

Parameters
InstanceTypeRTI Instance
pConfigPointer to the configuration structure
Returns
SDL_PASS for Success. SDL Error Code for failure.

◆ SDL_RTI_verifyConfig()

int32_t SDL_RTI_verifyConfig ( SDL_RTI_InstanceType  InstanceType,
SDL_RTI_configParms pConfig 
)

RTI API to verify the written configuration. This API can be used after calling SDL_RTI_config in order to verify the configuration. It reads back the configuration from the registers and compares it with the provided configuration.

Parameters
InstanceTypeRTI Instance
pConfigPointer to the configuration structure
Returns
SDL_PASS if verification passed. SDL Error Code for failure.

◆ SDL_RTI_start()

int32_t SDL_RTI_start ( SDL_RTI_InstanceType  InstanceType)

Enable the RTI instance.

Parameters
InstanceTypeRTI Instance
Returns
SDL_PASS if success. SDL Error Code for failure.
Note
Should be called after configuration of the RTI

◆ SDL_RTI_service()

int32_t SDL_RTI_service ( SDL_RTI_InstanceType  InstanceType)

Service the RTI instance.

Parameters
InstanceTypeRTI Instance
Returns
SDL_PASS if success. SDL Error Code for failure.

◆ SDL_RTI_clearStatus()

int32_t SDL_RTI_clearStatus ( SDL_RTI_InstanceType  InstanceType,
uint32_t  status 
)

Clear the DWWD status.

Parameters
InstanceTypeRTI Instance
statusViolation status to clear. Values given by bitwise or of macro RTI_Status_t
Returns
SDL_PASS if success. SDL Error Code for failure.

◆ SDL_RTI_getStatus()

int32_t SDL_RTI_getStatus ( SDL_RTI_InstanceType  InstanceType,
uint32_t *  pStatus 
)

Clear the DWWD status.

Parameters
InstanceTypeRTI Instance
pStatuspointer to DWWD status. Refer macro RTI_Status_t for possible bitwise or of all return values.
Returns
SDL_PASS if success. SDL Error Code for failure.

◆ SDL_RTI_readStaticRegs()

int32_t SDL_RTI_readStaticRegs ( SDL_RTI_InstanceType  InstanceType,
SDL_RTI_staticRegs pStaticRegs 
)

This API returns the static registers for RTI-DWWD.

Parameters
InstanceTypeBase Address of the RTI instance.
pStaticRegsPointer to RTI DWWD Static Registers.
Returns
SDL_PASS if success. SDL Error Code for failure.