AM62x MCU+ SDK  09.00.00
APIs for SDL RTI

Introduction

This module contains APIs for using the RTI module. The APIs can be used to configure the controller to calculate the signature for a set of data and then compare the calculated signature value against a predetermined good signature value.

The Digital Watchdog Timer(DWT) generates reset after a programmable period, if not serviced within that period. In DWT, time-out boundary is configurable. In DWWD, along with configurable time-out boundary, the start time boundary is also configurable. The DWWD can generate Reset or Interrupt, if not serviced within window(Open Window) defined by start time and time-out boundary. Also the DWWD can generate Reset or Interrupt if serviced outside Open Window (within Closed Window). Generation of Reset or Interrupt depends on the DWWD Reaction configuration.

Sub Modules

 RTI Data Structures
 
 RTI Enumerated Data Types
 
 RTI Functions
 
 RTI IP Functions