AM62Px MCU+ SDK  12.00.00

Detailed Description

RTC Parameters.

RTC parameters are used to with the RTC_open() call. Default values for these parameters are set using RTC_paramsInit().

Data Fields

uint32_t isfreezemode
 
bool onOffCallback
 
bool offOnCallback
 

Field Documentation

◆ isfreezemode

uint32_t RTC_Params::isfreezemode

RTC freeze Mode Enabled/Disabled

◆ onOffCallback

bool RTC_Params::onOffCallback

RTC On Off Callback

◆ offOnCallback

bool RTC_Params::offOnCallback

RTC Off On Callback