AM62Px MCU+ SDK  12.00.00

Introduction

This module contains APIs to program and use the RTC module.

Files

file  rtc/v0/rtc.h
 RTC Driver API/interface file.
 

Data Structures

struct  RTC_HwAttrs
 RTC Hardware attributes. More...
 
struct  RTC_Params
 RTC Parameters. More...
 
struct  RTC_Object
 RTC driver object. More...
 
struct  RTC_Config
 RTC Global Configuration. More...
 
struct  RTC_Time
 RTC Time Structure. More...
 

Functions

void RTC_init (void)
 Initialize the RTC module. More...
 
void RTC_deinit (void)
 De-initialize the RTC module. More...
 
void RTC_paramsInit (RTC_Params *params)
 Function to set default values of RTC_Params in params. More...
 
RTC_Handle RTC_open (uint32_t idx, const RTC_Params *params)
 Open the RTC at index idx with parameters params. More...
 
void RTC_close (RTC_Handle handle)
 Function to close the RTC Peripheral specified by the handle. More...
 
int32_t RTC_setTime (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the RTC time. More...
 
int32_t RTC_getTime (RTC_Handle handle, RTC_Time *rtc_time)
 Get the current RTC time. More...
 
int32_t RTC_setOff_OnTimerEvent (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the off-on timer event / Use as timer 1 for RTC. More...
 
int32_t RTC_setOn_OffTimerEvent (RTC_Handle handle, const RTC_Time *rtc_time)
 Set the on-off timer event / Use as timer 2 for RTC. More...
 
uint32_t RTC_readScratchRegister (RTC_Handle handle, uint32_t scratchIndex)
 Read a value from a specific RTC scratch register. More...
 
int32_t RTC_writeScratchRegister (RTC_Handle handle, uint32_t scratchIndex, uint32_t value)
 Write a value to a specific RTC scratch register. More...
 
RTC_Time RTC_calculateElapsedTime (const RTC_Time *startTime, const RTC_Time *endTime)
 Calculate Elapsed Time. More...
 
int32_t RTC_adjustForDrift (RTC_Handle handle, Float32 measuredDriftInSeconds)
 Calculate Elapsed Time. More...
 
int32_t RTC_stop (RTC_Handle handle)
 Stop the RTC. More...
 
int32_t RTC_start (RTC_Handle handle)
 Start the RTC after it's stopped. More...
 
void RTC_erratumi2327Init (void)
 RTC Erratum i2327 Workaround. More...
 

Typedefs

typedef struct RTC_Config_s * RTC_Handle
 A handle that is returned from a RTC_open() call. More...
 
typedef void(* RTC_OnOffCallbackFxn) (RTC_Handle handle)
 The definition of a ON_OFF callback function used by the RTC driver. More...
 
typedef void(* RTC_OffOnCallbackFxn) (RTC_Handle handle)
 The definition of a OFF_ON callback function used by the RTC driver. More...
 

Macros

#define OSCILLATOR_FREQ_HZ   ((uint32_t) 32768U)
 32.768 kHz Crystal Oscillator Frequency More...
 
#define RTC_FREEZE_MODE   ((uint32_t) 0x02000000U)
 Enable Freeze Mode. More...
 
#define O32K_OSC_DEP_EN_MASK   (CSL_RTC_GENRAL_CTL_O32K_OSC_DEP_EN_MASK)
 O32K_OSC_DEP_EN_MASK. More...
 
#define RD_PEND_MASK   (CSL_RTC_SYNCPEND_RD_PEND_MASK)
 Read Pend Status. More...
 
#define WR_PEND_MASK   (CSL_RTC_SYNCPEND_WR_PEND_MASK)
 Write Pend Status. More...
 
#define O32K_CLK_OBS_BIT_MASK   (CSL_RTC_SYNCPEND_O32K_CLK_OBS_MASK)
 O32K_CLK_OBS_BIT_MASK. More...
 
#define RTC_SW_OFF_MASK   (CSL_RTC_GENRAL_CTL_SW_OFF_MASK)
 RTC_SW_OFF_MASK. More...
 
#define RTC_UNLOCK_MASK   (CSL_RTC_GENRAL_CTL_UNLOCK_MASK)
 Unlock State Status. More...
 
#define OSC_LOCK_WAIT   (3U)
 Wait time for stabalizing OSC. More...
 
#define KICK0_UNLOCK_VALUE   (uint32_t)0x83E70B13U
 RTC Kick unlock values. More...
 
#define KICK1_UNLOCK_VALUE   (uint32_t)0x95A4F1E0U
 
#define KICK0_LOCK_VALUE   (CSL_RTC_KICK0_RESETVAL)
 RTC Kick lock values. More...
 
#define KICK1_LOCK_VALUE   (CSL_RTC_KICK1_RESETVAL)
 
#define RTC_BASEADDR   (uint32_t)0x2B1F0000U
 RTC Base Address. More...
 

RTC Timer Interrupt Set/Indication Flags

#define RTC_TMR_INT_INT0_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_ON_OFF_MASK)
 ON_OFF status interrupt. More...
 
#define RTC_TMR_INT_INT1_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_OFF_ON_MASK)
 OFF_ON status interrupt. More...
 
#define RTC_TMR_INT_INT0_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_ON_OFF_MASK)
 ON_OFF clear interrupt. More...
 
#define RTC_TMR_INT_INT1_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_OFF_ON_MASK)
 OFF_ON clear interrupt. More...
 
#define RTC_TMR_INT_INT0_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_ON_OFF_MASK)
 ON_OFF set interrupt. More...
 
#define RTC_TMR_INT_INT1_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_OFF_ON_MASK)
 OFF_ON set interrupt. More...
 
#define RTC_TMR_INT_INT0_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_ON_OFF_MASK)
 ON_OFF raw status interrupt. More...
 
#define RTC_TMR_INT_INT1_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_OFF_ON_MASK)
 OFF_ON raw status interrupt. More...
 
#define RTC_TMR_INT_STATUS_ALL
 All interrupt status mask. More...
 
#define RTC_TMR_INT_CLEAR_ALL
 All interrupt clear mask. More...
 
#define RTC_TMR_INT_REQ_ALL
 All interrupt set mask. More...
 
#define RTC_TMR_INT_RAW_STATUS_ALL
 All interrupt raw status mask. More...
 

Macro Definition Documentation

◆ OSCILLATOR_FREQ_HZ

#define OSCILLATOR_FREQ_HZ   ((uint32_t) 32768U)

32.768 kHz Crystal Oscillator Frequency

◆ RTC_FREEZE_MODE

#define RTC_FREEZE_MODE   ((uint32_t) 0x02000000U)

Enable Freeze Mode.

◆ O32K_OSC_DEP_EN_MASK

#define O32K_OSC_DEP_EN_MASK   (CSL_RTC_GENRAL_CTL_O32K_OSC_DEP_EN_MASK)

O32K_OSC_DEP_EN_MASK.

◆ RD_PEND_MASK

#define RD_PEND_MASK   (CSL_RTC_SYNCPEND_RD_PEND_MASK)

Read Pend Status.

◆ WR_PEND_MASK

#define WR_PEND_MASK   (CSL_RTC_SYNCPEND_WR_PEND_MASK)

Write Pend Status.

◆ O32K_CLK_OBS_BIT_MASK

#define O32K_CLK_OBS_BIT_MASK   (CSL_RTC_SYNCPEND_O32K_CLK_OBS_MASK)

O32K_CLK_OBS_BIT_MASK.

◆ RTC_SW_OFF_MASK

#define RTC_SW_OFF_MASK   (CSL_RTC_GENRAL_CTL_SW_OFF_MASK)

RTC_SW_OFF_MASK.

◆ RTC_UNLOCK_MASK

#define RTC_UNLOCK_MASK   (CSL_RTC_GENRAL_CTL_UNLOCK_MASK)

Unlock State Status.

◆ OSC_LOCK_WAIT

#define OSC_LOCK_WAIT   (3U)

Wait time for stabalizing OSC.

◆ KICK0_UNLOCK_VALUE

#define KICK0_UNLOCK_VALUE   (uint32_t)0x83E70B13U

RTC Kick unlock values.

◆ KICK1_UNLOCK_VALUE

#define KICK1_UNLOCK_VALUE   (uint32_t)0x95A4F1E0U

◆ KICK0_LOCK_VALUE

#define KICK0_LOCK_VALUE   (CSL_RTC_KICK0_RESETVAL)

RTC Kick lock values.

◆ KICK1_LOCK_VALUE

#define KICK1_LOCK_VALUE   (CSL_RTC_KICK1_RESETVAL)

◆ RTC_BASEADDR

#define RTC_BASEADDR   (uint32_t)0x2B1F0000U

RTC Base Address.

◆ RTC_TMR_INT_INT0_STATUS_FLAG

#define RTC_TMR_INT_INT0_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_ON_OFF_MASK)

ON_OFF status interrupt.

◆ RTC_TMR_INT_INT1_STATUS_FLAG

#define RTC_TMR_INT_INT1_STATUS_FLAG   (CSL_RTC_IRQSTATUS_SYS_EVENT_OFF_ON_MASK)

OFF_ON status interrupt.

◆ RTC_TMR_INT_INT0_CLEAR_FLAG

#define RTC_TMR_INT_INT0_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_ON_OFF_MASK)

ON_OFF clear interrupt.

◆ RTC_TMR_INT_INT1_CLEAR_FLAG

#define RTC_TMR_INT_INT1_CLEAR_FLAG   (CSL_RTC_IRQENABLE_CLR_SYS_EN_EVENT_OFF_ON_MASK)

OFF_ON clear interrupt.

◆ RTC_TMR_INT_INT0_SET_FLAG

#define RTC_TMR_INT_INT0_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_ON_OFF_MASK)

ON_OFF set interrupt.

◆ RTC_TMR_INT_INT1_SET_FLAG

#define RTC_TMR_INT_INT1_SET_FLAG   (CSL_RTC_IRQENABLE_SET_SYS_EN_EVENT_OFF_ON_MASK)

OFF_ON set interrupt.

◆ RTC_TMR_INT_INT0_RAW_STATUS_FLAG

#define RTC_TMR_INT_INT0_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_ON_OFF_MASK)

ON_OFF raw status interrupt.

◆ RTC_TMR_INT_INT1_RAW_STATUS_FLAG

#define RTC_TMR_INT_INT1_RAW_STATUS_FLAG   (CSL_RTC_IRQSTATUS_RAW_SYS_EVENT_OFF_ON_MASK)

OFF_ON raw status interrupt.

◆ RTC_TMR_INT_STATUS_ALL

#define RTC_TMR_INT_STATUS_ALL
Value:
RTC_TMR_INT_INT1_STATUS_FLAG)

All interrupt status mask.

◆ RTC_TMR_INT_CLEAR_ALL

#define RTC_TMR_INT_CLEAR_ALL
Value:
RTC_TMR_INT_INT1_CLEAR_FLAG)

All interrupt clear mask.

◆ RTC_TMR_INT_REQ_ALL

#define RTC_TMR_INT_REQ_ALL
Value:
RTC_TMR_INT_INT1_SET_FLAG)

All interrupt set mask.

◆ RTC_TMR_INT_RAW_STATUS_ALL

#define RTC_TMR_INT_RAW_STATUS_ALL
Value:
RTC_TMR_INT_INT1_RAW_STATUS_FLAG)

All interrupt raw status mask.

Typedef Documentation

◆ RTC_Handle

typedef struct RTC_Config_s* RTC_Handle

A handle that is returned from a RTC_open() call.

◆ RTC_OnOffCallbackFxn

typedef void(* RTC_OnOffCallbackFxn) (RTC_Handle handle)

The definition of a ON_OFF callback function used by the RTC driver.

The callback will be called if the ON_OFF interrupt is enabled.

Parameters
handleRTC_Handle

◆ RTC_OffOnCallbackFxn

typedef void(* RTC_OffOnCallbackFxn) (RTC_Handle handle)

The definition of a OFF_ON callback function used by the RTC driver.

  • The callback will be called if the OFF_ON interrupt is enabled.
Parameters
handleRTC_Handle

Function Documentation

◆ RTC_init()

void RTC_init ( void  )

Initialize the RTC module.

◆ RTC_deinit()

void RTC_deinit ( void  )

De-initialize the RTC module.

◆ RTC_paramsInit()

void RTC_paramsInit ( RTC_Params params)

Function to set default values of RTC_Params in params.

Parameters
params[IN] pointer to the structure to be initialized

◆ RTC_open()

RTC_Handle RTC_open ( uint32_t  idx,
const RTC_Params params 
)

Open the RTC at index idx with parameters params.

Parameters
idx[IN] Index of RTC to open in global config
params[IN] RTC_Params values to use for opening
Returns
RTC_Handle

◆ RTC_close()

void RTC_close ( RTC_Handle  handle)

Function to close the RTC Peripheral specified by the handle.

Precondition
RTC_open() has to be called first
Parameters
handle[IN] RTC_Handle returned from RTC_open()
See also
RTC_open()

◆ RTC_setTime()

int32_t RTC_setTime ( RTC_Handle  handle,
const RTC_Time rtc_time 
)

Set the RTC time.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
rtc_time[IN] Pointer to RTC_Time structure
Returns
RTC_StatusCode

◆ RTC_getTime()

int32_t RTC_getTime ( RTC_Handle  handle,
RTC_Time rtc_time 
)

Get the current RTC time.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
rtc_time[OUT] Pointer to RTC_Time structure
Returns
RTC_StatusCode

◆ RTC_setOff_OnTimerEvent()

int32_t RTC_setOff_OnTimerEvent ( RTC_Handle  handle,
const RTC_Time rtc_time 
)

Set the off-on timer event / Use as timer 1 for RTC.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
rtc_time[IN] Pointer to RTC_Time structure
Returns
RTC_StatusCode

◆ RTC_setOn_OffTimerEvent()

int32_t RTC_setOn_OffTimerEvent ( RTC_Handle  handle,
const RTC_Time rtc_time 
)

Set the on-off timer event / Use as timer 2 for RTC.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
rtc_time[IN] Pointer to RTC_Time structure
Returns
RTC_StatusCode

◆ RTC_readScratchRegister()

uint32_t RTC_readScratchRegister ( RTC_Handle  handle,
uint32_t  scratchIndex 
)

Read a value from a specific RTC scratch register.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
scratchIndex[IN] Index of scratch register to read
Returns
Value from the specified scratch register

◆ RTC_writeScratchRegister()

int32_t RTC_writeScratchRegister ( RTC_Handle  handle,
uint32_t  scratchIndex,
uint32_t  value 
)

Write a value to a specific RTC scratch register.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
scratchIndex[IN] Index of scratch register to write
value[IN] Value to write to the scratch register
Returns
RTC_StatusCode

◆ RTC_calculateElapsedTime()

RTC_Time RTC_calculateElapsedTime ( const RTC_Time startTime,
const RTC_Time endTime 
)

Calculate Elapsed Time.

Parameters
startTime[IN] RTC_Time structure having start time
endTime[IN] RTC_Time structure having end time

◆ RTC_adjustForDrift()

int32_t RTC_adjustForDrift ( RTC_Handle  handle,
Float32  measuredDriftInSeconds 
)

Calculate Elapsed Time.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
measuredDriftInSeconds[IN] Drift Value to be adjusted in Seconds
Returns
RTC_StatusCode

◆ RTC_stop()

int32_t RTC_stop ( RTC_Handle  handle)

Stop the RTC.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
Returns
RTC_StatusCode

◆ RTC_start()

int32_t RTC_start ( RTC_Handle  handle)

Start the RTC after it's stopped.

Parameters
handle[IN] RTC_Handle returned from RTC_open()
Returns
RTC_StatusCode

◆ RTC_erratumi2327Init()

void RTC_erratumi2327Init ( void  )

RTC Erratum i2327 Workaround.

Due to a bug in initial synchronization out of cold power on, IRQ status can get locked infinitely if we do not: a) unlock RTC

This workaround must be applied within 1 second of power on, So, this is closest point to be able to guarantee the max timing.

RTC_TMR_INT_INT0_RAW_STATUS_FLAG
#define RTC_TMR_INT_INT0_RAW_STATUS_FLAG
ON_OFF raw status interrupt.
Definition: rtc/v0/rtc.h:128
RTC_TMR_INT_INT0_SET_FLAG
#define RTC_TMR_INT_INT0_SET_FLAG
ON_OFF set interrupt.
Definition: rtc/v0/rtc.h:123
RTC_TMR_INT_INT0_STATUS_FLAG
#define RTC_TMR_INT_INT0_STATUS_FLAG
ON_OFF status interrupt.
Definition: rtc/v0/rtc.h:113
RTC_TMR_INT_INT0_CLEAR_FLAG
#define RTC_TMR_INT_INT0_CLEAR_FLAG
ON_OFF clear interrupt.
Definition: rtc/v0/rtc.h:118