AM62Px MCU+ SDK  09.02.00
Dss_DctrlOverlayLayerParams Struct Reference

Detailed Description

Structure containing Overlay layer information. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_LAYER_PARAMS.

Data Fields

uint32_t overlayId
 
uint32_t pipeLayerNum [CSL_DSS_VID_PIPE_ID_MAX]
 

Field Documentation

◆ overlayId

uint32_t Dss_DctrlOverlayLayerParams::overlayId

Overlay Id. See CSL_DssOverlayId for values

◆ pipeLayerNum

uint32_t Dss_DctrlOverlayLayerParams::pipeLayerNum[CSL_DSS_VID_PIPE_ID_MAX]

Layer to which a particular Video Pipe Id is connected. For valid values see CSL_DssOverlayLayerNum