AM62Px MCU+ SDK  09.02.00

Introduction

This is hardware include layer for DSS overlay region.

Files

file  csl_dssOverlay.h
 DSS Overlay layer interface file.
 

Data Structures

struct  CSL_DssOverlayCfg
 Configuration for DSS Overlay. More...
 
struct  CSL_DssOverlayLayerCfg
 Configuration for selecting overlay input layers. More...
 
struct  CSL_DssOverlayPipePosCfg
 Video Pipe Position Configuration in Overlay. More...
 

Functions

void CSL_dssOverlaySetConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayCfg *overlayCfg)
 Configure the Overlay Params. More...
 
void CSL_dssOverlayColorBarEnable (CSL_dss_overlayRegs *overlayRegs, uint32_t enable)
 Enable the Color Bar in DSS Overlay. More...
 
void CSL_dssOverlaySetLayerConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayLayerCfg *layerCfg)
 Configure the Overlay input selection. More...
 
void CSL_dssOverlaySetPipePosConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayPipePosCfg *pipePosCfg, uint32_t layerNum)
 Configure the Video Pipe Position in Overlay. More...
 
uint32_t CSL_dssOverlayGetEnabledPipeLayerNum (const CSL_dss_overlayRegs *overlayRegs, uint32_t pipeId)
 Get the layer number where a particular Video Pipe is connected. More...
 
static void CSL_dssOverlayCfgInit (CSL_DssOverlayCfg *overlayCfg)
 CSL_DssOverlayCfg structure init function. More...
 
static void CSL_dssOverlayLayerCfgInit (CSL_DssOverlayLayerCfg *layerCfg)
 CSL_DssOverlayLayerCfg structure init function. More...
 
static void CSL_dssOverlayPipePosCfgInit (CSL_DssOverlayPipePosCfg *pipePosCfg)
 CSL_DssOverlayPipePosCfg structure init function. More...
 

Typedefs

typedef CSL_dss_ovr1Regs CSL_dss_overlayRegs
 DSS Overlay Registers. More...
 

DSS Overlay Transparency Color Key Selection

#define CSL_DSS_OVERLAY_TRANS_COLOR_DEST    ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_GDTK)
 Destination transparency color key selected. More...
 
#define CSL_DSS_OVERLAY_TRANS_COLOR_SRC    ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_VSTK)
 Source transparency color key selected. More...
 

DSS Overlay Layer Number

#define CSL_DSS_OVERLAY_LAYER_NUM_0   ((uint32_t) 0x0U)
 Overlay Layer 0. More...
 
#define CSL_DSS_OVERLAY_LAYER_NUM_1   ((uint32_t) 0x1U)
 Overlay Layer 1. More...
 
#define CSL_DSS_OVERLAY_LAYER_MAX   ((uint32_t) 0x2U)
 Maximum overlay layers. More...
 
#define CSL_DSS_OVERLAY_LAYER_INVALID   ((uint32_t) 0xFFU)
 Invalid Overlay Layer. More...
 

Macro Definition Documentation

◆ CSL_DSS_OVERLAY_TRANS_COLOR_DEST

#define CSL_DSS_OVERLAY_TRANS_COLOR_DEST    ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_GDTK)

Destination transparency color key selected.

◆ CSL_DSS_OVERLAY_TRANS_COLOR_SRC

#define CSL_DSS_OVERLAY_TRANS_COLOR_SRC    ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_VSTK)

Source transparency color key selected.

◆ CSL_DSS_OVERLAY_LAYER_NUM_0

#define CSL_DSS_OVERLAY_LAYER_NUM_0   ((uint32_t) 0x0U)

Overlay Layer 0.

◆ CSL_DSS_OVERLAY_LAYER_NUM_1

#define CSL_DSS_OVERLAY_LAYER_NUM_1   ((uint32_t) 0x1U)

Overlay Layer 1.

◆ CSL_DSS_OVERLAY_LAYER_MAX

#define CSL_DSS_OVERLAY_LAYER_MAX   ((uint32_t) 0x2U)

Maximum overlay layers.

◆ CSL_DSS_OVERLAY_LAYER_INVALID

#define CSL_DSS_OVERLAY_LAYER_INVALID   ((uint32_t) 0xFFU)

Invalid Overlay Layer.

Typedef Documentation

◆ CSL_dss_overlayRegs

DSS Overlay Registers.

DSS7 UL has two identical Overlay blocks, hence define a generic structure to have common APIs

Function Documentation

◆ CSL_dssOverlaySetConfig()

void CSL_dssOverlaySetConfig ( CSL_dss_overlayRegs overlayRegs,
const CSL_DssOverlayCfg overlayCfg 
)

Configure the Overlay Params.

Parameters
overlayRegsPointer to a CSL_dss_overlayRegs structure containing the overlay configuration
overlayCfgPointer to the CSL_DssOverlayCfg structure. This parameter should not be NULL

◆ CSL_dssOverlayColorBarEnable()

void CSL_dssOverlayColorBarEnable ( CSL_dss_overlayRegs overlayRegs,
uint32_t  enable 
)

Enable the Color Bar in DSS Overlay.

Parameters
overlayRegsPointer to a CSL_dss_overlayRegs structure containing the overlay configuration
enableEnable or disable the color bar

◆ CSL_dssOverlaySetLayerConfig()

void CSL_dssOverlaySetLayerConfig ( CSL_dss_overlayRegs overlayRegs,
const CSL_DssOverlayLayerCfg layerCfg 
)

Configure the Overlay input selection.

Parameters
overlayRegsPointer to a CSL_dss_overlayRegs structure containing the overlay configuration
layerCfgPointer to CSL_DssOverlayLayerCfg structure. This parameter should not be NULL

◆ CSL_dssOverlaySetPipePosConfig()

void CSL_dssOverlaySetPipePosConfig ( CSL_dss_overlayRegs overlayRegs,
const CSL_DssOverlayPipePosCfg pipePosCfg,
uint32_t  layerNum 
)

Configure the Video Pipe Position in Overlay.

Parameters
overlayRegsPointer to a CSL_dss_overlayRegs structure containing the overlay configuration
pipePosCfgPointer to CSL_DssOverlayPipePosCfg structure. This parameter should not be NULL
layerNumLayer Number

◆ CSL_dssOverlayGetEnabledPipeLayerNum()

uint32_t CSL_dssOverlayGetEnabledPipeLayerNum ( const CSL_dss_overlayRegs overlayRegs,
uint32_t  pipeId 
)

Get the layer number where a particular Video Pipe is connected.

Parameters
overlayRegsPointer to a CSL_dss_overlayRegs structure containing the overlay configuration
pipeIdPipe Id. Refer to CSL_DssVidPipeId for values
Returns
CSL_DssOverlayLayerNum Layer Number to which pipe is connected. API returns CSL_DSS_OVERLAY_LAYER_INVALID if pipe is not connected to any overlay layer

◆ CSL_dssOverlayCfgInit()

static void CSL_dssOverlayCfgInit ( CSL_DssOverlayCfg overlayCfg)
inlinestatic

CSL_DssOverlayCfg structure init function.

Parameters
overlayCfgPointer to CSL_DssOverlayCfg structure

◆ CSL_dssOverlayLayerCfgInit()

static void CSL_dssOverlayLayerCfgInit ( CSL_DssOverlayLayerCfg layerCfg)
inlinestatic

CSL_DssOverlayLayerCfg structure init function.

Parameters
layerCfgPointer to CSL_DssOverlayLayerCfg structure

◆ CSL_dssOverlayPipePosCfgInit()

static void CSL_dssOverlayPipePosCfgInit ( CSL_DssOverlayPipePosCfg pipePosCfg)
inlinestatic

CSL_DssOverlayPipePosCfg structure init function.

Parameters
pipePosCfgPointer to CSL_DssOverlayPipePosCfg structure