AM62L FreeRTOS SDK  11.02.00

Detailed Description

Structure containing DSS parameters. This structure is used as an argument to IOCTL_DSS_DISP_SET_DSS_PARAMS.

Data Fields

CSL_DssVidPipeCfg pipeCfg
 
CSL_DssVidPipeDmaCfg dmaCfg
 
CSL_DssVidPipeAlphaCfg alphaCfg
 
CSL_DssVidPipeVC1Cfg vc1Cfg
 
Dss_DispPipeCropParams cropParams
 
Fvid2_PosConfig layerPos
 

Field Documentation

◆ pipeCfg

CSL_DssVidPipeCfg Dss_DispParams::pipeCfg

Video pipeline configuration

◆ dmaCfg

CSL_DssVidPipeDmaCfg Dss_DispParams::dmaCfg

Video pipeline DMA configuration

◆ alphaCfg

CSL_DssVidPipeAlphaCfg Dss_DispParams::alphaCfg

Video pipeline alpha configuration

◆ vc1Cfg

CSL_DssVidPipeVC1Cfg Dss_DispParams::vc1Cfg

Video pipeline VC1 configuration

◆ cropParams

Dss_DispPipeCropParams Dss_DispParams::cropParams

Video pipeline Crop parameters, used only for J7 platform

◆ layerPos

Fvid2_PosConfig Dss_DispParams::layerPos

Position of the video buffer described using Fvid2_PosConfig

startX:
X position of the video buffer The first pixel on the left of the screen has the X-position 0

startY:
Y position of the video buffer The line at the top has the Y-position 0