AM62L FreeRTOS SDK  11.02.00

Introduction

The Display Subsystem (DSS) provides the logic to interface display peripherals. This is DSS driver documentation.

Sub Modules

 Dispay Hardware Include Layer
 
 Display Controller Driver
 
 Display Driver Configurations
 
 Display Pipe Driver
 
 Display SoC Config
 

Files

file  dss/v0/dss.h
 DSS Driver API/interface file. This is DSS's top level include for applications.
 

Data Structures

struct  Dss_InitParams
 DSS initialization parameters. More...
 
struct  Dss_ConfigPipelineParams
 Display pipeline config parameters. The test case execution happens based on values of this structure. More...
 
struct  Dss_InstObject
 Driver instance information. More...
 
struct  Dss_RegionFwlData
 Firewall data structure defining ID, start and end address. More...
 
struct  Dss_FirewallRegionConfig
 Firewall configuration structure. More...
 
struct  Dss_Object
 Test application data structure. More...
 

Functions

void Dss_initParamsInit (Dss_InitParams *dssParams)
 Dss_InitParams structure init function. More...
 
int32_t Dss_init (const Dss_InitParams *initParams)
 DSS initialization function. This function initializes the DSS hardware and drivers. This function should be called before calling any driver APIs and only once. More...
 
int32_t Dss_deInit (void)
 DSS de-initialization function. This function un-initializes the DSS hardware and drivers. This function should be called during system shutdown if Dss_init() was called by the application. More...
 

Macros

#define DSS_DISP_DRV_ID   (FVID2_DSS_DRV_BASE + 0x00U)
 Display driver ID used at the time of FVID2 create. More...
 
#define DSS_DCTRL_DRV_ID   (FVID2_DSS_DRV_BASE + 0x01U)
 Display controller driver ID used at the time of FVID2 create. More...
 
#define DSS_DISP_IOCTL_BASE   (FVID2_DSS_DRV_IOCTL_BASE + 0x000U)
 IOCTL base address for the display driver IOCTLs. More...
 
#define DSS_DCTRL_IOCTL_BASE   (FVID2_DSS_DRV_IOCTL_BASE + 0x100U)
 IOCTL base address for the display controller driver IOCTLs. More...
 
#define DSS_DISP_SOC_IOCTL_BASE   (DSS_DISP_IOCTL_BASE + 0x40U)
 IOCTL base address for the SOC specific display driver IOCTLs. More...
 
#define DSS_DCTRL_SOC_IOCTL_BASE   (DSS_DCTRL_IOCTL_BASE + 0x40U)
 IOCTL base address for the SOC specific display controller driver IOCTLs. More...
 

Macro Definition Documentation

◆ DSS_DISP_DRV_ID

#define DSS_DISP_DRV_ID   (FVID2_DSS_DRV_BASE + 0x00U)

Display driver ID used at the time of FVID2 create.

◆ DSS_DCTRL_DRV_ID

#define DSS_DCTRL_DRV_ID   (FVID2_DSS_DRV_BASE + 0x01U)

Display controller driver ID used at the time of FVID2 create.

◆ DSS_DISP_IOCTL_BASE

#define DSS_DISP_IOCTL_BASE   (FVID2_DSS_DRV_IOCTL_BASE + 0x000U)

IOCTL base address for the display driver IOCTLs.

◆ DSS_DCTRL_IOCTL_BASE

#define DSS_DCTRL_IOCTL_BASE   (FVID2_DSS_DRV_IOCTL_BASE + 0x100U)

IOCTL base address for the display controller driver IOCTLs.

◆ DSS_DISP_SOC_IOCTL_BASE

#define DSS_DISP_SOC_IOCTL_BASE   (DSS_DISP_IOCTL_BASE + 0x40U)

IOCTL base address for the SOC specific display driver IOCTLs.

◆ DSS_DCTRL_SOC_IOCTL_BASE

#define DSS_DCTRL_SOC_IOCTL_BASE   (DSS_DCTRL_IOCTL_BASE + 0x40U)

IOCTL base address for the SOC specific display controller driver IOCTLs.

Function Documentation

◆ Dss_initParamsInit()

void Dss_initParamsInit ( Dss_InitParams *  dssParams)

Dss_InitParams structure init function.

Parameters
dssParamsPointer to Dss_InitParams structure.

◆ Dss_init()

int32_t Dss_init ( const Dss_InitParams *  initParams)

DSS initialization function. This function initializes the DSS hardware and drivers. This function should be called before calling any driver APIs and only once.

Parameters
initParamsPointer to a Dss_InitParams structure containing the DSS configuration
Returns
FVID2_SOK if successful, else suitable error code

◆ Dss_deInit()

int32_t Dss_deInit ( void  )

DSS de-initialization function. This function un-initializes the DSS hardware and drivers. This function should be called during system shutdown if Dss_init() was called by the application.

Returns
FVID2_SOK if successful, else suitable error code