AM62L FreeRTOS SDK  11.02.00
Dss_DispBufPrgmCbParams Struct Reference

Detailed Description

Structure containing display buffer program callback parameters. This structure is used as an argument to IOCTL_DSS_DISP_REGISTER_BUF_PRGM_CB.

Data Fields

Dss_DispBufPrgmCbFxn bufPrgmCbFxn
 

Field Documentation

◆ bufPrgmCbFxn

Dss_DispBufPrgmCbFxn Dss_DispBufPrgmCbParams::bufPrgmCbFxn

Application callback function to be called just before programming the hardware. A value of NULL will un-register the callback.