AM62L FreeRTOS SDK  11.02.00

Detailed Description

Structure containing DSS sync operations configuration. This structure is used as a part of Dss_DctrlVpParams.

Data Fields

uint32_t enabled
 
uint32_t isPrimary
 
uint32_t syncVpIds [CSL_DSS_VP_ID_MAX]
 
uint32_t numSyncVpIds
 

Field Documentation

◆ enabled

uint32_t Dss_DctrlSyncOpCfg::enabled

Enable sync operations configuration

◆ isPrimary

uint32_t Dss_DctrlSyncOpCfg::isPrimary

Whether this VP is the primary output. Only operations on the primary VP results in H/W register operations. For secondary VPs, the enable / setGo operations pend on the corresponding operation on the primary VP

◆ syncVpIds

uint32_t Dss_DctrlSyncOpCfg::syncVpIds[CSL_DSS_VP_ID_MAX]

Array of VP Ids for Sync operations

◆ numSyncVpIds

uint32_t Dss_DctrlSyncOpCfg::numSyncVpIds

Number of valid VP Ids in syncVpIds