AM62D FreeRTOS SDK  11.02.00

Detailed Description

Request for TISCI_MSG_SET_IO_ISOLATION.

Parameters
hdrTISCI header to provide ACK/NAK flags to the host.
stateThe desired state of the IO isolation.

This message is used to enable/disable IO isolation for low power modes.

Data Fields

struct tisci_header hdr
 
uint8_t state
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_set_io_isolation_req::hdr

◆ state

uint8_t tisci_msg_set_io_isolation_req::state