DMSC controls the power management, security and resource management of the device.
Data Structures | |
| struct | tisci_msg_prepare_sleep_req |
| Request for TISCI_MSG_PREPARE_SLEEP. More... | |
| struct | tisci_msg_prepare_sleep_resp |
| Response for TISCI_MSG_PREPARE_SLEEP. More... | |
| struct | tisci_msg_enter_sleep_req |
| Request for TISCI_MSG_ENTER_SLEEP. More... | |
| struct | tisci_msg_enter_sleep_resp |
| Response for TISCI_MSG_ENTER_SLEEP. More... | |
| struct | tisci_msg_get_suspend_initiator_req |
| Request for TI_SCI_MSG_GET_SUSPEND_INITIATOR. More... | |
| struct | tisci_msg_get_suspend_initiator_resp |
| Response for TI_SCI_MSG_GET_SUSPEND_INITIATOR. More... | |
| struct | tisci_msg_firmware_load_req |
| Request for TISCI_MSG_FIRMWARE_LOAD. More... | |
| struct | tisci_msg_firmware_load_resp |
| Response for TISCI_MSG_FIRMWARE_LOAD. More... | |
| struct | tisci_msg_sync_resume_req |
| Request for TISCI_MSG_SYNC_RESUME. More... | |
| struct | tisci_msg_sync_resume_resp |
| Response for TISCI_MSG_SYNC_RESUME. More... | |
| struct | tisci_msg_continue_resume_req |
| Request for TISCI_MSG_CONTINUE_RESUME. More... | |
| struct | tisci_msg_continue_resume_resp |
| Response for TISCI_MSG_CONTINUE_RESUME. More... | |
| struct | tisci_msg_core_resume_req |
| Request for TISCI_MSG_CORE_RESUME. More... | |
| struct | tisci_msg_core_resume_resp |
| Response for TISCI_MSG_CORE_RESUME. More... | |
| struct | tisci_msg_dm_abort_sleep_req |
| Request for TISCI_MSG_DM_ABORT_SLEEP. More... | |
| struct | tisci_msg_dm_abort_sleep_resp |
| Response for TISCI_MSG_DM_ABORT_SLEEP. More... | |
| struct | tisci_msg_lpm_wake_reason_req |
| Request for TISCI_MSG_LPM_WAKE_REASON. More... | |
| struct | tisci_msg_lpm_wake_reason_resp |
| Response for TISCI_MSG_LPM_WAKE_REASON. More... | |
| struct | tisci_msg_set_io_isolation_req |
| Request for TISCI_MSG_SET_IO_ISOLATION. More... | |
| struct | tisci_msg_set_io_isolation_resp |
| Response for TISCI_MSG_SET_IO_ISOLATION. More... | |
| struct | tisci_msg_min_context_restore_req |
| Request for TISCI_MSG_MIN_CONTEXT_RESTORE. More... | |
| struct | tisci_msg_min_context_restore_resp |
| Response for TISCI_MSG_MIN_CONTEXT_RESTORE. More... | |
| struct | tisci_msg_lpm_set_device_constraint_req |
| Request for TISCI_MSG_LPM_SET_DEVICE_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_set_device_constraint_resp |
| Response for TISCI_MSG_LPM_SET_DEVICE_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_get_device_constraint_req |
| Request for TISCI_MSG_LPM_GET_DEVICE_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_get_device_constraint_resp |
| Response for TISCI_MSG_LPM_GET_DEVICE_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_set_latency_constraint_req |
| Request for TISCI_MSG_LPM_SET_LATENCY_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_set_latency_constraint_resp |
| Response for TISCI_MSG_LPM_SET_LATENCY_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_get_latency_constraint_req |
| Request for TISCI_MSG_LPM_GET_LATENCY_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_get_latency_constraint_resp |
| Response for TISCI_MSG_LPM_GET_LATENCY_CONSTRAINT. More... | |
| struct | tisci_msg_lpm_get_next_sys_mode_req |
| Request for TISCI_MSG_LPM_GET_NEXT_SYS_MODE. More... | |
| struct | tisci_msg_lpm_get_next_sys_mode_resp |
| Response for TISCI_MSG_LPM_GET_NEXT_SYS_MODE. More... | |
| struct | tisci_msg_lpm_get_next_host_state_req |
| Request for TISCI_MSG_GET_LPM_NEXT_HOST_STATE. More... | |
| struct | tisci_msg_lpm_get_next_host_state_resp |
| Response for TISCI_MSG_LPM_GET_NEXT_HOST_STATE. More... | |
| struct | tisci_msg_lpm_abort_req |
| Request for TISCI_MSG_LPM_ABORT. More... | |
| struct | tisci_msg_lpm_abort_resp |
| Response for TISCI_MSG_LPM_ABORT. More... | |
| struct | tisci_msg_lpm_save_ctx_addr_req |
| Request for TISCI_MSG_LPM_SAVE_ADDR. More... | |
| struct | tisci_msg_lpm_save_ctx_addr_resp |
| Response for TISCI_MSG_LPM_SAVE_ADDR. More... | |
Functions | |
| struct tisci_msg_prepare_sleep_req | __attribute__ ((__packed__)) |
| #define TISCI_MSG_VALUE_SLEEP_MODE_DEEP_SLEEP 0x0U |
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
DM Firmware TISCI LPM Messaging
TISCI LPM layer for managing Low Power Mode TISCI message handlers Sleep mode in which complete SOC except the wakeup domain is turned off.
| #define TISCI_MSG_VALUE_SLEEP_MODE_MCU_ONLY 0x1U |
Sleep mode in which complete SOC except the wakeup and MCU domain is turned off.
| #define TISCI_MSG_VALUE_SLEEP_MODE_IO_ONLY_PLUS_DDR 0x2U |
Sleep mode in which complete SOC except the DDR memory and CAN IOs is turned off.
| #define TISCI_MSG_VALUE_SLEEP_MODE_PARTIAL_IO 0x3U |
Sleep mode in which complete SOC except the CAN IOs is turned off.
| #define TISCI_MSG_VALUE_SLEEP_MODE_STANDBY 0x4U |
Sleep mode in which software is in low power mode but the hardware remains on.
| #define TISCI_MSG_VALUE_SLEEP_MODE_SOC_OFF 0x5U |
Sleep mode in which the complete SOC except the DDR is turned off.
| #define TISCI_MSG_VALUE_SLEEP_MODE_RTC_PLUS_DDR 0x6U |
Sleep mode in which complete SOC except the RTC and DDR is off
| #define TISCI_MSG_VALUE_SLEEP_MODE_RTC_ONLY 0x7U |
Sleep mode in which complete SOC except the RTC is turned off
| #define TISCI_MSG_VALUE_SLEEP_MODE_DM_MANAGED 0xFDU |
Value passed to request device manager for low power mode selection.
| #define TISCI_MSG_VALUE_SLEEP_MODE_NOT_SELECTED 0xFEU |
Value returned if device manager has not yet selected the low power mode.
| #define TISCI_MSG_VALUE_SLEEP_MODE_INVALID 0xFFU |
Value returned if low power mode entered is invalid.
| #define MSG_FLAG_CERT_AUTH_PASS 0x555555U |
| #define MSG_FLAG_CERT_AUTH_FAIL 0xffffffU |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_00 0x0x00000001 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_01 0x0x00000002 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_02 0x0x00000004 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_03 0x0x00000008 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_04 0x0x00000010 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_05 0x0x00000020 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_06 0x0x00000040 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_07 0x0x00000080 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_08 0x0x00000100 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_09 0x0x00000200 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_10 0x0x00000400 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_11 0x0x00000800 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_12 0x0x00001000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_13 0x0x00002000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_14 0x0x00004000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_15 0x0x00008000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_16 0x0x00010000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_17 0x0x00020000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_18 0x0x00040000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_19 0x0x00080000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_20 0x0x00100000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_21 0x0x00200000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_22 0x0x00400000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_23 0x0x00800000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_24 0x0x01000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_25 0x0x02000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_26 0x0x04000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_27 0x0x08000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_28 0x0x10000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_29 0x0x20000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_30 0x0x40000000 |
| #define TISCI_MSG_VALUE_SLEEP_DEBUG_FLAG_31 0x0x80000000 |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_I2C0 0x00U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_UART0 0x10U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_MCU_GPIO0 0x20U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_ICEMELTER0 0x30U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_TIMER0 0x40U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_TIMER1 0x41U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_WKUP_RTC0 0x50U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_RESET 0x60U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_USB0 0x70U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_USB1 0x71U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_MAIN_IO 0x80U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_MCU_IO 0x81U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_CAN_IO 0x82U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_MCU_IPC 0x90U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_EARLY_WAKE_IPOR 0xA0U |
| #define TISCI_MSG_VALUE_LPM_WAKE_SOURCE_INVALID 0xFFU |
| #define TISCI_MSG_VALUE_LPM_WAKE_PIN_INVALID 0xFFU |
Used by TISCI_MSG_LPM_WAKE_REASON to return wake pin number as invalid
| #define TISCI_MSG_VALUE_HOST_STATE_ON 1U |
Used by TISCI_MSG_GET_NEXT_HOST_STATE to return remote core's state as on
| #define TISCI_MSG_VALUE_HOST_STATE_OFF 0U |
Used by TISCI_MSG_GET_NEXT_HOST_STATE to return remote core's state as off
| #define TISCI_MSG_VALUE_HOST_STATE_INVALID 0xFFU |
Used by TISCI_MSG_GET_NEXT_HOST_STATE to return remote core's state as invalid
| #define TISCI_MSG_VALUE_IO_ENABLE 1U |
Used by TISCI_MSG_SET_IO_ISOLATION to enable IO isolation
| #define TISCI_MSG_VALUE_IO_DISABLE 0U |
Used by TISCI_MSG_SET_IO_ISOLATION to disable IO isolation
| #define TISCI_MSG_VALUE_STATE_SET 1U |
Used by set and get constraints APIs to set/get constraint for device/latency
| #define TISCI_MSG_VALUE_STATE_CLEAR 0U |
Used by set and get constraints APIs to clear/get constraint for device/latency
| struct tisci_msg_prepare_sleep_req __attribute__ | ( | (__packed__) | ) |