UDMA Low Level Driver AM62ax SOC specific file.
Go to the source code of this file.
Functions | |
uint32_t | Udma_isCacheCoherent (void) |
Returns TRUE if the memory is cache coherent. More... | |
uint8_t | Udma_isValidInstance (uint32_t instId) |
Returns TRUE if the given UDMA Instance ID is valid for this SoC. More... | |
uint32_t Udma_isCacheCoherent | ( | void | ) |
Returns TRUE if the memory is cache coherent.
uint8_t Udma_isValidInstance | ( | uint32_t | instId | ) |
Returns TRUE if the given UDMA Instance ID is valid for this SoC.