MCASP Driver API/interface file.
Go to the source code of this file.
Data Structures | |
struct | MCASP_Transaction |
Data structure used with transfer call. More... | |
struct | MCASP_ClockConfig |
Hardware setup data clock structure. More... | |
struct | MCASP_GlobalConfig |
Hardware setup global structure. More... | |
struct | MCASP_FifoConfig |
Hardware fifo setup structure. More... | |
struct | MCASP_DataConfig |
Hardware setup data structure. More... | |
struct | MCASP_HwConfig |
Hardware setup structure. More... | |
struct | MCASP_DmaChConfig |
struct | MCASP_DmaTrpdMemAlloc |
struct | MCASP_OpenParams |
MCASP Parameters. More... | |
struct | MCASP_HwIntConfig |
McASP Interrupt structures. More... | |
struct | MCASP_TransferObj |
McASP Transfer Data structure stored in driver object. More... | |
struct | MCASP_Object |
MCASP driver object. More... | |
struct | MCASP_Attrs |
MCASP instance attributes - used during init time. More... | |
struct | MCASP_Config |
Macros | |
#define | MCASP_GBLCTL_TIMEOUT (30000U) |
The time to try (in Msec) before the GBLCTL register setting timeouts if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout. More... | |
#define | MCASP_DATA_TIMEOUT (30000U) |
The time to try (in Msec) to check the XDTATA/RDATA flags in status register. if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout. More... | |
#define | MCASP_RESET ((uint32_t) 0x00U) |
McASP macros for enable/reset. More... | |
#define | MCASP_ENABLE ((uint32_t) 0x01U) |
#define | MCASP_DISABLE ((uint32_t) 0x00U) |
#define | MCASP_REG_OFFSET ((uint32_t)0x4U) |
#define | MCASP_DIR_OUT 0 |
#define | MCASP_DIR_IN 1 |
#define | MCASP_TRPD_INVALID_PTR (0xFFFFFFFF) |
Transfer Status Code | |
#define | MCASP_TRANSFER_STATUS_COMPLETED (0U) |
I/O completed successfully. More... | |
#define | MCASP_TRANSFER_STATUS_STARTED (1U) |
I/O queued and pending. More... | |
#define | MCASP_TRANSFER_STATUS_CANCELLED (2U) |
I/O cancelled. Returned by incomplete read or write requests. More... | |
#define | MCASP_TRANSFER_STATUS_FAILED (3U) |
Generic failure condition. More... | |
#define | MCASP_TRANSFER_STATUS_TIMEOUT (4U) |
I/O timeout occurred. More... | |
McASP Transfer Mode | |
#define | MCASP_TRANSFER_MODE_POLLING (0U) |
MCASP read/write APIs blocks execution. This mode can only be used when called within a Task context. More... | |
#define | MCASP_TRANSFER_MODE_INTERRUPT (1U) |
MCASP read/write APIs does not block code execution and will call a MCASP_TxCallbackFxn or MCASP_RxCallbackFxn. This mode can be used in a Task, Swi, or Hwi context. More... | |
#define | MCASP_TRANSFER_MODE_DMA (2U) |
MCASP read/write APIs does not block code execution and will use DMA for transfers. More... | |
McASP Operating Mode | |
#define | MCASP_OPMODE_MASTER (0U) |
I/O completed successfully. More... | |
#define | MCASP_OPMODE_SLAVE (1U) |
I/O queued and pending. More... | |
MCASP Channel Direction | |
#define | MCASP_CHANNEL_INPUT (0x0001U) |
MCASP Channel will receive data. More... | |
#define | MCASP_CHANNEL_OUTPUT (0x0002U) |
MCASP Channel will transmit data. More... | |
#define | MCASP_CHANNEL_INOUT (MCASP_CHANNEL_INPUT | MCASP_CHANNEL_OUTPUT) |
McASP channel transmits & recieves data. More... | |
MCASP Driver State | |
#define | MCASP_DRIVER_STATE_DELETED (0U) |
#define | MCASP_DRIVER_STATE_CREATED (1U) |
#define | MCASP_DRIVER_STATE_INITIALIZED (2U) |
#define | MCASP_DRIVER_STATE_OPENED (3U) |
#define | MCASP_DRIVER_STATE_CLOSED (4U) |
#define | MCASP_DRIVER_STATE_DEINITIALIZED (5U) |
#define | MCASP_DRIVER_STATE_POWERED_DOWN (6U) |
#define | MCASP_DRIVER_STATE_PWRM_SUSPEND (7U) |
MCASP Serializer Status | |
#define | MCASP_SERIALIZER_STATUS_FREE (0U) |
#define | MCASP_SERIALIZER_STATUS_XMT (1U) |
#define | MCASP_SERIALIZER_STATUS_RCV (2U) |
MCASP Channel Mode | |
#define | MCASP_CHANNEL_MODE_FREE (0U) |
#define | MCASP_CHANNEL_MODE_XMT_DIT (1U) |
#define | MCASP_CHANNEL_MODE_XMT_TDM (2U) |
#define | MCASP_CHANNEL_MODE_RCV (3U) |
MCASP Word Select | |
#define | MCASP_WORD_SELECT_LSW (0U) |
#define | MCASP_WORD_SELECT_MSW (1U) |
Enumerated constants to specify the supported buffer formats. | |
#define | MCASP_AUDBUFF_FORMAT_1SER_MULTISLOT_NON_INTERLEAVED (0U) |
This is used for transfer of data on a single serializer with multiple slots.please note that the slot data is not interleaved in this format. TDM with single serializer and slots > 1 uses this format. More... | |
#define | MCASP_AUDBUFF_FORMAT_1SER_MULTISLOT_INTERLEAVED (1U) |
This is used for transfer of data on a single serializer with multiple slots.please note that the slot data is interleaved in this format. TDM with single serializer and slots > 1 uses this format. More... | |
#define | MCASP_AUDBUFF_FORMAT_MULTISER_MULTISLOT_SEMI_INTERLEAVED_1 (2U) |
This is used for transfer of data with multiple serializers and also multiple slots enabled.please note that the serializer data is interleaved in this format. The slot data is also interleaved Refer to the user guide to view the sample data format. More... | |
#define | MCASP_AUDBUFF_FORMAT_MULTISER_MULTISLOT_SEMI_INTERLEAVED_2 (3U) |
This is used for transfer of data with multiple serializers and also multiple slots enabled.please note that the serializer data is NOT interleaved in this format. The slot data is interleaved. Refer to the user guide to view the sample data format. More... | |
Transmit State for McASP transfer | |
#define | MCASP_TRANSMIT_STATE_TX_RESET (0U) |
#define | MCASP_TRANSMIT_STATE_TX_FLUSH (1U) |
#define | MCASP_TRANSMIT_STATE_LOAD_INIT_BUFFER (2U) |
#define | MCASP_TRANSMIT_STATE_RELEASE_FROM_RESET (3U) |
#define | MCASP_TRANSMIT_STATE_WAIT_EVENT (4U) |
#define | MCASP_TRANSMIT_STATE_PROCESS_EVENT (5U) |
#define | MCASP_TRANSMIT_STATE_LOAD_ACTIVE_BUFFER (6U) |
#define | MCASP_TRANSMIT_STATE_DONE (7U) |
#define | MCASP_TRANSMIT_STATE_SPIN_IDLE (8U) |
#define | MCASP_TRANSMIT_STATE_ERROR (9U) |
#define | MCASP_TRANSMIT_STATE_EXIT (10U) |
Receive State for McASP transfer | |
#define | MCASP_RECEIVE_STATE_RX_RESET (0U) |
#define | MCASP_RECEIVE_STATE_RX_FLUSH (1U) |
#define | MCASP_RECEIVE_STATE_RELEASE_FROM_RESET (2U) |
#define | MCASP_RECEIVE_STATE_WAIT_EVENT (3U) |
#define | MCASP_RECEIVE_STATE_PROCESS_EVENT (4U) |
#define | MCASP_RECEIVE_STATE_DONE (5U) |
#define | MCASP_RECEIVE_STATE_SPIN_IDLE (6U) |
#define | MCASP_RECEIVE_STATE_ERROR (7U) |
#define | MCASP_RECEIVE_STATE_EXIT (8U) |
Typedefs | |
typedef void * | MCASP_Handle |
A handle that is returned from a MCASP_open() call. More... | |
typedef void(* | MCASP_TxCallbackFxn) (MCASP_Handle handle, MCASP_Transaction *transaction) |
The definition of a callback function used by the MCASP driver when used in Callback Mode. More... | |
typedef void(* | MCASP_RxCallbackFxn) (MCASP_Handle handle, MCASP_Transaction *transaction) |
Functions | |
void | MCASP_init (void) |
This function initializes the MCASP module. More... | |
void | MCASP_deinit (void) |
This function de-initializes the MCASP module. More... | |
static void | MCASP_openParamsInit (MCASP_OpenParams *openPrms) |
Function to initialize the MCASP_OpenParams struct to its defaults. More... | |
MCASP_Handle | MCASP_open (uint32_t index, const MCASP_OpenParams *openParams) |
This function opens a given MCASP peripheral. More... | |
void | MCASP_close (MCASP_Handle handle) |
Function to close a MCASP peripheral specified by the MCASP handle. More... | |
MCASP_Handle | MCASP_getHandle (uint32_t index) |
This function returns the handle of an open MCASP Instance from the instance index. More... | |
int32_t | MCASP_submitTx (MCASP_Handle handle, MCASP_Transaction *txn) |
Function to submit the buffer to McASP driver for transmission. Transaction object is held by the driver till it is returned in the callback function. It is recommended not to allocate the transaction object in stack to avoid corruption. More... | |
int32_t | MCASP_submitRx (MCASP_Handle handle, MCASP_Transaction *txn) |
Function to submit the buffer to McASP driver for reception. Transaction object is held by the driver till it is returned in the callback function. It is recommended not to allocate the transaction object in stack to avoid corruption. More... | |
MCASP_Transaction * | MCASP_withdrawTx (MCASP_Handle handle) |
Function to withdraw the buffer submitted to McASP driver for transmission. This should be called after the MCASP_stopTransferTx. These buffers are not transmitted. More... | |
MCASP_Transaction * | MCASP_withdrawRx (MCASP_Handle handle) |
Function to withdraw the buffer submitted to McASP driver for reception. This should be called after the MCASP_stopTransferRx. These buffers are not transmitted. More... | |
int32_t | MCASP_startTransferTx (MCASP_Handle handle) |
Function to start McASP transmission. More... | |
int32_t | MCASP_startTransferRx (MCASP_Handle handle) |
Function to start McASP reception. More... | |
int32_t | MCASP_stopTransferTx (MCASP_Handle handle) |
Function to stop McASP transmission. More... | |
int32_t | MCASP_stopTransferRx (MCASP_Handle handle) |
Function to stop McASP reception. More... | |
Variables | |
MCASP_Config | gMcaspConfig [] |
Externally defined driver configuration array. More... | |
uint32_t | gMcaspConfigNum |
Externally defined driver configuration array size. More... | |