AM275 FreeRTOS SDK  12.00.00
ub_logging.h File Reference

Introduction

Control logging by levels and categories.

The logging is controlled by 8 levels which is from UBL_NONE to UBL_DEBUGV. The levels are used, one is for regular console output, and the other is for debug output.

The two levels are set for each category. The categories are defined by user applications, and need to be registered by the initialization string. Registered categories must be enumerated and managed by user. Because category number 0 is used for 'unibase', in user applications starting from category number 1 is recommended.

Go to the source code of this file.

Macros

#define UBL_NONE   0
 
#define UBL_FATAL   1
 
#define UBL_ERROR   2
 
#define UBL_WARN   3
 
#define UBL_INFO   4
 
#define UBL_INFOV   5
 
#define UBL_DEBUG   6
 
#define UBL_DEBUGV   7
 
#define MAX_LOGMSG_CATEGORIES   16
 maximum number of categories More...
 
#define DBGMSG_LEVEL_MARK   {"NON", "FTL", "ERR", "WRN", "INF", "IFV", "DBG", "DBV"}
 3-charcter string to represent each logging level More...
 
#define UBL_TS_BIT_FIELDS   3
 lowest 2 bits are used for TS Clock type, use ub_clocktype_t UB_CLOCK_DEFAULT means no-timestamp More...
 
#define UB_LOG_COMPILE_LEVEL   UBL_DEBUGV
 
#define UB_LOG_IS_COMPILED(level)   (UB_LOG_COMPILE_LEVEL >= level)
 
#define UB_LOG_HELPER(level, tstype, ...)
 
#define UB_LOG_UBL_DEBUGV(...)   UB_LOG_HELPER(UBL_DEBUGV, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_DEBUGV(...)   UB_LOG_HELPER(UBL_DEBUGV, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_DEBUG(...)   UB_LOG_HELPER(UBL_DEBUG, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_DEBUG(...)   UB_LOG_HELPER(UBL_DEBUG, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_INFOV(...)   UB_LOG_HELPER(UBL_INFOV, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_INFOV(...)   UB_LOG_HELPER(UBL_INFOV, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_INFO(...)   UB_LOG_HELPER(UBL_INFO, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_INFO(...)   UB_LOG_HELPER(UBL_INFO, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_WARN(...)   UB_LOG_HELPER(UBL_WARN, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_WARN(...)   UB_LOG_HELPER(UBL_WARN, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_ERROR(...)   UB_LOG_HELPER(UBL_ERROR, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_ERROR(...)   UB_LOG_HELPER(UBL_ERROR, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_FATAL(...)   UB_LOG_HELPER(UBL_FATAL, 0, __VA_ARGS__)
 
#define UB_TLOG_UBL_FATAL(...)   UB_LOG_HELPER(UBL_FATAL, UB_LOGTSTYPE, __VA_ARGS__)
 
#define UB_LOG_UBL_NONE(...)
 
#define UB_TLOG_UBL_NONE(...)
 
#define UBL_OVERRIDE_ISTR(x, y)   ub_log_initstr_override(x,UBB_GETENV(y))
 override valuse 'x' to the value of the environment variable 'y' More...
 
#define PRINT_FORMAT_ATTRIBUTE1   __attribute__((format (printf, 1, 2)))
 let the compiler show warning when printf type format is wrong More...
 
#define PRINT_FORMAT_ATTRIBUTE4   __attribute__((format (printf, 4, 5)))
 format starts at 4th argument More...
 

Typedefs

typedef int ub_dbgmsg_level_t
 This defines different logging levels. More...
 

Functions

void ub_console_debug_select_print (bool console, bool debug, const char *astr)
 output to console out and debug out by selection More...
 
const char * ub_log_initstr_override (const char *ns, const char *os)
 override 'istr' of ub_log_inig More...
 
void ub_log_init (const char *istr)
 initialize logging by a string More...
 
int ub_log_add_category (const char *catstr)
 add a category of logging at the bottom of the index More...
 
int ub_log_print (int cat_index, int flags, ub_dbgmsg_level_t level, const char *astr)
 print log message More...
 
bool ub_clog_on (int cat_index, ub_dbgmsg_level_t level)
 check if console log is enabled or not for the indicated cat_index and level More...
 
bool ub_dlog_on (int cat_index, ub_dbgmsg_level_t level)
 check if debug log is enabled or not for the indicated cat_index and level More...
 
int ub_log_change (int cat_index, ub_dbgmsg_level_t clevel, ub_dbgmsg_level_t dlevel)
 change console log level to clevel, and debug log level to delevl More...
 
int ub_log_return (int cat_index)
 return console log level and console log level to the previous status More...
 
void ub_log_flush (void)
 flush out messages on the both of cosole log and debug log More...