AM275 FreeRTOS SDK  12.00.00
TI ENET LLD ethernet specific

Introduction

Files

file  cb_lld_ethernet.h
 TI ENET LLD specific network layer part.
 

Data Structures

struct  lld_ethhdr
 Ethernet header structure. More...
 
struct  lld_sockaddr
 Structure representing the lld_sockaddr instance. More...
 
struct  lld_ethdev_t
 Structure representing the lld_ethdev instance. More...
 
struct  cb_socket_lldcfg_update_t
 Structure representing the cb_socket_lldcfg_update instance. More...
 
struct  cb_tilld_port_stats_t
 

Functions

struct lld_ethhdr __attribute__ ((packed))
 
int cb_lld_init_devs_table (lld_ethdev_t *ethdevs, uint32_t ndevs, uint32_t enet_type, uint32_t instance_id, const LLDTsyncTsSource tsSource)
 Initialize a LLD device table. More...
 
int cb_socket_set_lldcfg_update_cb (cb_socket_lldcfg_update_cb_t lldcfg_update_cb)
 This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once. More...
 
int cb_lld_netdev_to_macport (const char *netdev)
 Convert net device name to mac port. More...
 
int cb_lld_sendto (CB_SOCKET_T sfd, void *sdata, int psize, int flags, const CB_SOCKADDR_LL_T *addr, int addrsize)
 Send a TX ethernet L2 packet. More...
 
int cb_lld_sendto_scatter (CB_SOCKET_T sfd, LLDEnetFrameScatter_t *frame, const CB_SOCKADDR_LL_T *addr)
 Send a TX ethernet L2 packet in the scatter way. More...
 
int cb_lld_recv (CB_SOCKET_T sfd, void *buf, int size, CB_SOCKADDR_LL_T *addr, int addrsize)
 Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked. More...
 
int cb_lld_recv_zerocopy (CB_SOCKET_T sfd, LLDEnetRecvCb_t cblld_recv_cb, void *cbarg)
 Receive a RX ethernet L2 packet n the zero-copy way. This should be called after a rxnotify_cb is invoked. More...
 
int cb_lld_set_txnotify_cb (CB_SOCKET_T sfd, void(*txnotify_cb)(void *arg), void *arg)
 Set the TX notify callback that is invoked when an TX packet is sent successfully. More...
 
int cb_lld_set_rxnotify_cb (CB_SOCKET_T sfd, void(*rxnotify_cb)(void *arg), void *arg)
 Set the RX notify callback that is invoked when an RX packet is ready to be received. More...
 
int cb_lld_set_default_rxdata_cb (CB_SOCKET_T sfd, void(*default_rxdata_cb)(void *data, int size, int port, void *arg), void *arg)
 Set the default RX data callback that is invoked when an RX packet does not match any filters. More...
 
int cb_lld_get_type_instance (uint32_t *enet_type, uint32_t *instance_id)
 Get enet type and instance that is set via cb_lld_init_devs_table() More...
 
int cb_lld_get_ts_source (LLDTsyncTsSource *tsSource)
 Get Timestamp source that is set via cb_lld_init_devs_table() More...
 
int cb_lld_get_netdevs (char *netdevs[], int *len)
 Get all virtual network interfaces which were defined for the TI platform. More...
 
int cb_lld_get_link_state (CB_SOCKET_T cfd, const char *dev, uint32_t *linkstate)
 get link state from device name like 'eth0' More...
 
int cb_lld_get_link_info (CB_SOCKET_T cfd, const char *dev, uint32_t *speed, uint32_t *duplex)
 get link info(speed and duplex) from device name like 'eth0' More...
 
int cb_lld_get_port_stats (CB_SOCKET_T sfd, int port, cb_tilld_port_stats_t *stats)
 Get stats info from host or mac port. More...
 
void cb_lld_reset_port_stats (CB_SOCKET_T sfd, int port)
 reset stats info from host or mac port. More...
 
int cb_lld_process_status_frames (CB_SOCKET_T sfd)
 process the Phy status frames. More...
 
void cb_lld_notify_linkchange (void)
 Nofity link change event through cbl_query_thread_data_t signal. More...
 

Typedefs

typedef struct lld_socket lld_socket_t
 Structure representing the lld_socket instance. More...
 
typedef int(* cb_socket_lldcfg_update_cb_t) (cb_socket_lldcfg_update_t *update_cfg)
 Callback function type for cb_socket_lldcfg_update. More...
 

Macros

#define LWIP_DONT_PROVIDE_BYTEORDER_FUNCTIONS
 
#define htons   __htons
 
#define ntohs   __ntohs
 
#define htonl   __htonl
 
#define ntohl   __ntohl
 
#define MAX_NUMBER_ENET_DEVS   LLDENET_MAX_PORTS
 
#define CB_SOCKET_VALID(x)   ((x)!=NULL)
 
#define CB_SOCKET_INVALID_VALUE   NULL
 
#define CB_SOCKET_T   lld_socket_t*
 
#define CB_ETHHDR_T   struct lld_ethhdr
 
#define CB_SOCKADDR_LL_T   struct lld_sockaddr
 
#define CB_SOCKADDR_T   struct lld_sockaddr
 
#define CB_SOCK_SENDTO   cb_lld_sendto
 
#define CB_SOCK_CLOSE   cb_rawsock_close
 
#define CB_OPEN   open
 
#define CB_CLOSE   close
 
#define CB_WRITE   write
 
#define CB_IN_ADDR_T   void*
 
#define IFNAMSIZ   16
 
#define ETH_ALEN   6 /* Octets in one ethernet addr */
 
#define ETH_HLEN   14 /* Total octets in header. */
 
#define ETH_DATA_LEN   1500 /* Max. octets in payload */
 
#define ETH_P_8021Q   0x8100 /* 802.1Q VLAN Extended Header */
 
#define ETH_P_1588   0x88F7 /* IEEE 1588 Timesync */
 
#define ETH_P_LLDP   0x88CC /* 802.1AB LLDP */
 
#define ETH_P_TSN   0x22F0 /* TSN (IEEE 1722) packet */
 
#define ETH_P_NETLINK   0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */
 
#define CB_MAX_NETDEVNAME   16
 
#define MKPIPE(x)   (-1)
 
#define CB_LLD_MAX_ETH_FRAME_SIZE   (1522U)
 
#define CB_TILLD_STATS_BLOCK_ELEM_NUM   (128U)
 

Macro Definition Documentation

◆ LWIP_DONT_PROVIDE_BYTEORDER_FUNCTIONS

#define LWIP_DONT_PROVIDE_BYTEORDER_FUNCTIONS

◆ htons

#define htons   __htons

◆ ntohs

#define ntohs   __ntohs

◆ htonl

#define htonl   __htonl

◆ ntohl

#define ntohl   __ntohl

◆ MAX_NUMBER_ENET_DEVS

#define MAX_NUMBER_ENET_DEVS   LLDENET_MAX_PORTS

◆ CB_SOCKET_VALID

#define CB_SOCKET_VALID (   x)    ((x)!=NULL)

◆ CB_SOCKET_INVALID_VALUE

#define CB_SOCKET_INVALID_VALUE   NULL

◆ CB_SOCKET_T

#define CB_SOCKET_T   lld_socket_t*

◆ CB_ETHHDR_T

#define CB_ETHHDR_T   struct lld_ethhdr

◆ CB_SOCKADDR_LL_T

#define CB_SOCKADDR_LL_T   struct lld_sockaddr

◆ CB_SOCKADDR_T

#define CB_SOCKADDR_T   struct lld_sockaddr

◆ CB_SOCK_SENDTO

#define CB_SOCK_SENDTO   cb_lld_sendto

◆ CB_SOCK_CLOSE

#define CB_SOCK_CLOSE   cb_rawsock_close

◆ CB_OPEN

#define CB_OPEN   open

◆ CB_CLOSE

#define CB_CLOSE   close

◆ CB_WRITE

#define CB_WRITE   write

◆ CB_IN_ADDR_T

#define CB_IN_ADDR_T   void*

◆ IFNAMSIZ

#define IFNAMSIZ   16

◆ ETH_ALEN

#define ETH_ALEN   6 /* Octets in one ethernet addr */

◆ ETH_HLEN

#define ETH_HLEN   14 /* Total octets in header. */

◆ ETH_DATA_LEN

#define ETH_DATA_LEN   1500 /* Max. octets in payload */

◆ ETH_P_8021Q

#define ETH_P_8021Q   0x8100 /* 802.1Q VLAN Extended Header */

◆ ETH_P_1588

#define ETH_P_1588   0x88F7 /* IEEE 1588 Timesync */

◆ ETH_P_LLDP

#define ETH_P_LLDP   0x88CC /* 802.1AB LLDP */

◆ ETH_P_TSN

#define ETH_P_TSN   0x22F0 /* TSN (IEEE 1722) packet */

◆ ETH_P_NETLINK

#define ETH_P_NETLINK   0x22F1 /* A virtual prototol for netlink rawsockt on TI platforms */

◆ CB_MAX_NETDEVNAME

#define CB_MAX_NETDEVNAME   16

◆ MKPIPE

#define MKPIPE (   x)    (-1)

◆ CB_LLD_MAX_ETH_FRAME_SIZE

#define CB_LLD_MAX_ETH_FRAME_SIZE   (1522U)

◆ CB_TILLD_STATS_BLOCK_ELEM_NUM

#define CB_TILLD_STATS_BLOCK_ELEM_NUM   (128U)

Typedef Documentation

◆ lld_socket_t

typedef struct lld_socket lld_socket_t

Structure representing the lld_socket instance.

◆ cb_socket_lldcfg_update_cb_t

cb_socket_lldcfg_update_cb_t

Callback function type for cb_socket_lldcfg_update.

Parameters
update_cfgPointer to the cb_socket_lldcfg_update instance.
Returns
Integer value indicating the result of the callback. 0: OK, <0: error

Function Documentation

◆ __attribute__()

struct lld_ethhdr __attribute__ ( (packed)  )

◆ cb_lld_init_devs_table()

int cb_lld_init_devs_table ( lld_ethdev_t ethdevs,
uint32_t  ndevs,
uint32_t  enet_type,
uint32_t  instance_id,
const LLDTsyncTsSource  tsSource 
)

Initialize a LLD device table.

This function should only be called once, before calling any net functions from the combase. It is recommended to call once in the main() application, not in any TSN module source. If the ethdevs[i].srcmac is all zero, the srcmac will be alloced dynamically by the the LLD layer. Please note that ethdevs[i].netdev must point to a global memory address, not a stack memory address.

Parameters
ethdevsan arrays of ethernet devices
ndevsnumber of devices in the array
enet_typeLLD ethernet type
instance_idLLD ethernet instance ID
tsSourceLLDTsync timestamp source
Returns
0: OK, <0: error, detailed error will be printed out.

◆ cb_socket_set_lldcfg_update_cb()

int cb_socket_set_lldcfg_update_cb ( cb_socket_lldcfg_update_cb_t  lldcfg_update_cb)

This function sets the callback for updating LLD config parameters. It enables the user to update config parameters for the Enet LLD layer that are not supported by the CB socket. It is important to note that this function should only be called once.

Parameters
lldcfg_update_cbupdate callback
Returns
0: OK, <0: error, detailed error will be printed out.

◆ cb_lld_netdev_to_macport()

int cb_lld_netdev_to_macport ( const char *  netdev)

Convert net device name to mac port.

Parameters
netdevnet device name e.g. eth0
Returns
>=0: MAC port, <0: error, detailed error will be printed out.

◆ cb_lld_sendto()

int cb_lld_sendto ( CB_SOCKET_T  sfd,
void *  sdata,
int  psize,
int  flags,
const CB_SOCKADDR_LL_T addr,
int  addrsize 
)

Send a TX ethernet L2 packet.

Parameters
sfdsocket fd
sdataethernet L2 packet
psizepacket size
flagsit is unused now, keep it to make it compatible with POSIX sendto
addrdestination address info
addrsizeaddress size
Returns
number of sent bytes if OK, <0: error, detailed error will be printed out.

◆ cb_lld_sendto_scatter()

int cb_lld_sendto_scatter ( CB_SOCKET_T  sfd,
LLDEnetFrameScatter_t frame,
const CB_SOCKADDR_LL_T addr 
)

Send a TX ethernet L2 packet in the scatter way.

Parameters
sfdsocket fd
frameethernet L2 packet in the scatter way
addrdestination address info
Returns
number of sent bytes if OK, <0: error, detailed error will be printed out.

◆ cb_lld_recv()

int cb_lld_recv ( CB_SOCKET_T  sfd,
void *  buf,
int  size,
CB_SOCKADDR_LL_T addr,
int  addrsize 
)

Receive a RX ethernet L2 packet. This should be called after a rxnotify_cb is invoked.

Parameters
sfdsocket fd
bufpacket buffer
sizebuffer size
addrindex of received port and packets info
addrsizesize of the addr structure.
Returns
<0: error; 0: No data available; 0xFFFF: Unmatched data filter; >0: data len

◆ cb_lld_recv_zerocopy()

int cb_lld_recv_zerocopy ( CB_SOCKET_T  sfd,
LLDEnetRecvCb_t  cblld_recv_cb,
void *  cbarg 
)

Receive a RX ethernet L2 packet n the zero-copy way. This should be called after a rxnotify_cb is invoked.

Parameters
sfdsocket fd
cblld_recv_cbthe receive callback
cbargthe callback argument
Returns
<0: error; 0: No data available; 0xFFFF: Unmatched data filter; 1: received data

◆ cb_lld_set_txnotify_cb()

int cb_lld_set_txnotify_cb ( CB_SOCKET_T  sfd,
void(*)(void *arg)  txnotify_cb,
void *  arg 
)

Set the TX notify callback that is invoked when an TX packet is sent successfully.

Parameters
sfdsocket fd
txnotify_cbcallback
argcallback argument
Returns
0: OK, <0: error, detailed error will be printed out

◆ cb_lld_set_rxnotify_cb()

int cb_lld_set_rxnotify_cb ( CB_SOCKET_T  sfd,
void(*)(void *arg)  rxnotify_cb,
void *  arg 
)

Set the RX notify callback that is invoked when an RX packet is ready to be received.

Parameters
sfdsocket fd
rxnotify_cbcallback
argcallback argument
Returns
0: OK, <0: error, detailed error will be printed out

◆ cb_lld_set_default_rxdata_cb()

int cb_lld_set_default_rxdata_cb ( CB_SOCKET_T  sfd,
void(*)(void *data, int size, int port, void *arg)  default_rxdata_cb,
void *  arg 
)

Set the default RX data callback that is invoked when an RX packet does not match any filters.

Parameters
sfdsocket fd
default_rxdata_cbcallback
argcallback argument
Returns
0: OK, <0: error, detailed error will be printed out

◆ cb_lld_get_type_instance()

int cb_lld_get_type_instance ( uint32_t *  enet_type,
uint32_t *  instance_id 
)

Get enet type and instance that is set via cb_lld_init_devs_table()

Parameters
enet_typeethernet type
instance_idethernet instance ID
Returns
0: OK, <0: error, detailed error will be printed out

◆ cb_lld_get_ts_source()

int cb_lld_get_ts_source ( LLDTsyncTsSource tsSource)

Get Timestamp source that is set via cb_lld_init_devs_table()

Parameters
tsSourcePointer to the tsSource
Returns
0: OK, <0: error, detailed error will be printed out

◆ cb_lld_get_netdevs()

int cb_lld_get_netdevs ( char *  netdevs[],
int *  len 
)

Get all virtual network interfaces which were defined for the TI platform.

Parameters
netdevsan array of pointer points to the net devices acquired by this api.
lenhow many net devices are returned by this api.
Returns
0 on success; -1 on failure

◆ cb_lld_get_link_state()

int cb_lld_get_link_state ( CB_SOCKET_T  cfd,
const char *  dev,
uint32_t *  linkstate 
)

get link state from device name like 'eth0'

Parameters
cfda socket handle coressponding to the ethernet device name specified via the second argument dev
devethernet device name like 'eth0'
linkstatea pointer for storing link state value (0:down, 1:up)
Returns
0 on success, -1 on error

◆ cb_lld_get_link_info()

int cb_lld_get_link_info ( CB_SOCKET_T  cfd,
const char *  dev,
uint32_t *  speed,
uint32_t *  duplex 
)

get link info(speed and duplex) from device name like 'eth0'

Parameters
cfda socket handle coressponding to the ethernet device name specified via the second argument dev
devethenert device name like 'eth0'
speeda pointer for storing speed value (0:unknow, 10:10Mbps, 100:100Mbps, 1000:1Gbps)
duplexa pointer for storing duplex value (0:unknow, 1:Full, 2:Half)
Returns
0 on success, -1 on error

◆ cb_lld_get_port_stats()

int cb_lld_get_port_stats ( CB_SOCKET_T  sfd,
int  port,
cb_tilld_port_stats_t stats 
)

Get stats info from host or mac port.

Parameters
sfdsocket fd
port0xFF: host port; less than 0xFF: mac port.
statsa pointer to cb_tilld_port_stats_t object
Note
valid index of mac port depends on HW platform
Returns
0 on success, -1 on failure

◆ cb_lld_reset_port_stats()

void cb_lld_reset_port_stats ( CB_SOCKET_T  sfd,
int  port 
)

reset stats info from host or mac port.

Parameters
sfdsocket fd
port0xFF: host port; less than: mac port.
Note
valid index of mac port depends on HW platform

◆ cb_lld_process_status_frames()

int cb_lld_process_status_frames ( CB_SOCKET_T  sfd)

process the Phy status frames.

Parameters
sfdsocket fd
Returns
number of status frames processed.

◆ cb_lld_notify_linkchange()

void cb_lld_notify_linkchange ( void  )

Nofity link change event through cbl_query_thread_data_t signal.

Variable Documentation

◆ __attribute__

struct lld_sockaddr __attribute__