This structure contains the different configuration used for PBIST.
Design: PROC_SDL-967
Data Fields | |
| uint32_t | override |
| uint32_t | algorithmsBitMap |
| uint64_t | memoryGroupsBitMap |
| uint64_t | scrambleValue |
| uint32_t SDL_PBIST_config::override |
Override value for memory configuration. Check SOC documentation for supported override mode for each PBIST instance.
| uint32_t SDL_PBIST_config::algorithmsBitMap |
Bitmap to select algorithms to use for test.
NOTE: For a given PBIST instance, there is a selected set of memory groups a particular Algorithm can be run. Check SOC documentation for supported algorithms for each PBIST instance.
| uint64_t SDL_PBIST_config::memoryGroupsBitMap |
Bitmap to select memory groups to run test on. Check SOC documentation for supported memory groups for each PBIST instance.
| uint64_t SDL_PBIST_config::scrambleValue |
Scramble value to be used for test. Check SOC documentation for scramble value to be used.