Data Structures | |
struct | SDL_PBIST_config |
This structure contains the different configuration used for PBIST. More... | |
struct | SDL_PBIST_configNeg |
This structure contains the different configuration used for PBIST for the failure insertion test to generate negative result. More... | |
Functions | |
int32_t | SDL_PBIST_softReset (SDL_pbistRegs *pPBISTRegs) |
PBIST Soft reset. More... | |
int32_t | SDL_PBIST_start (SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_config *pConfig) |
PBIST Start. More... | |
int32_t | SDL_PBIST_startNeg (SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_configNeg *pConfig) |
PBIST Failure Insertion Test Start. More... | |
int32_t | SDL_PBIST_checkResult (const SDL_pbistRegs *pPBISTRegs, bool *pResult) |
PBIST check result. More... | |
int32_t | SDL_PBIST_releaseTestMode (SDL_pbistRegs *pPBISTRegs) |
PBIST Release Test mode. More... | |
int32_t | SDL_PBIST_Instance (SDL_PBIST_inst instance) |
PBIST Instance. More... | |
int32_t SDL_PBIST_softReset | ( | SDL_pbistRegs * | pPBISTRegs | ) |
PBIST Soft reset.
This function resets PBIST Module. In general called before running a new test.
pPBISTRegs | [IN] Pointer to PBIST registers base |
int32_t SDL_PBIST_start | ( | SDL_pbistRegs * | pPBISTRegs, |
const SDL_PBIST_config * | pConfig | ||
) |
PBIST Start.
This function configures the paramters for PBIST and starts execution.
pPBISTRegs | [IN] Pointer to PBIST registers base |
pConfig | [IN] Pointer to PBIST configuration |
int32_t SDL_PBIST_startNeg | ( | SDL_pbistRegs * | pPBISTRegs, |
const SDL_PBIST_configNeg * | pConfig | ||
) |
PBIST Failure Insertion Test Start.
This function configures the parameters for PBIST Test for Diagnostics to insert a failure to generate the negative result and starts execution.
pPBISTRegs | [IN] Pointer to PBIST registers base |
pConfig | [IN] Pointer to PBIST configuration |
int32_t SDL_PBIST_checkResult | ( | const SDL_pbistRegs * | pPBISTRegs, |
bool * | pResult | ||
) |
PBIST check result.
This function checks if PBIST test has passed.
pPBISTRegs | [IN] Pointer to PBIST registers base |
pResult | [OUT] Pointer to variable to indicate result |
int32_t SDL_PBIST_releaseTestMode | ( | SDL_pbistRegs * | pPBISTRegs | ) |
PBIST Release Test mode.
This function releases test mode. In general called after test is complete to switch back to normal operation.
pPBISTRegs | [IN] Pointer to PBIST registers base |
int32_t SDL_PBIST_Instance | ( | SDL_PBIST_inst | instance | ) |
PBIST Instance.
This function specifies the PBITST Instance
instance | [IN] Value of PBIST instance |