MCASP driver object.
MCASP_Handle MCASP_Object::handle |
Instance handle
uint16_t MCASP_Object::instNum |
Instance number in port
uint32_t MCASP_Object::drvState |
stores the current state of the driver
uint32_t MCASP_Object::transferMode |
Polling, Blocking or Callback mode.
int32_t MCASP_Object::edmaInst |
EDMA instance used for MCASP transfer
MCASP_TransferObj MCASP_Object::XmtObj |
Holds transmit channel to the McASP.
MCASP_TransferObj MCASP_Object::RcvObj |
Holds receive channel to the McASP.
uint32_t MCASP_Object::isOpen |
Flag to indicate if the instance is already open
uint32_t MCASP_Object::isTxStarted |
Flag to indicate if the Tx is started
uint32_t MCASP_Object::isRxStarted |
Flag to indicate if the Rx is started
SemaphoreP_Object MCASP_Object::lockObj |
Driver lock object
SemaphoreP_Object MCASP_Object::transferSemObj |
Transfer Sync Semaphore object
HwiP_Object MCASP_Object::hwiObjTx |
Transmit Interrupt object
HwiP_Object MCASP_Object::hwiObjRx |
Receive Interrupt object
MCASP_EdmaConfig MCASP_Object::xmtDmaObj |
transmit dma object
MCASP_EdmaConfig MCASP_Object::rcvDmaObj |
receive dma object number of slots used by the mcasp
QueueP_Object MCASP_Object::reqQueueObjTx |
QueueP_Object MCASP_Object::curentQueueObjTx |
QueueP_Object MCASP_Object::reqQueueObjRx |
QueueP_Object MCASP_Object::curentQueueObjRx |
Queue Obj to store the application buffers
QueueP_Handle MCASP_Object::reqQueueHandleTx |
QueueP_Handle MCASP_Object::curentQueueHandleTx |
QueueP_Handle MCASP_Object::reqQueueHandleRx |
QueueP_Handle MCASP_Object::curentQueueHandleRx |
Queue handle used for storing the application buffers