MCASP edma configuration object.
Data Fields | |
uint32_t | baseAddr |
uint32_t | regionId |
uint32_t | chId |
uint32_t | paramId |
uint32_t | tccId |
uint32_t | linkParamId |
Edma_IntrObject | intrObj |
uint32_t MCASP_EdmaConfig::baseAddr |
EDMA instance base address
uint32_t MCASP_EdmaConfig::regionId |
EDMA region Id
uint32_t MCASP_EdmaConfig::chId |
DMA Channel Number. This should be the MCASP Event number
uint32_t MCASP_EdmaConfig::paramId |
EDMA parameter ram Id
uint32_t MCASP_EdmaConfig::tccId |
EDMA transfer completion code
uint32_t MCASP_EdmaConfig::linkParamId |
EDMA link parameter ram Id
Edma_IntrObject MCASP_EdmaConfig::intrObj |