AM273x MCU+ SDK  09.02.00
CCM Low-Level API

Introduction

CCM for R5F provides APIs to select the operating modes and read the status for

  1. CPU compare block
  2. Inactivity monitor
  3. VIM compare block The APIs for programming the polarity of the CPU signals are also provided. The errors issued by the RTL are routed to the ESM (error signaling module) external to the subsystem.

Functions

int32_t SDL_armR5ReadCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo)
 Read CCM Regiser. More...
 
int32_t SDL_armR5ConfigureCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo)
 Configure CCM Regiser. More...
 
int32_t SDL_armR5CCMSetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo)
 Configure Operating mode for CPU, VIM, CCM Inactivity monitor. More...
 
int32_t SDL_armR5CCMGetCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo)
 Read Compare Error status for CPU, VIM, CCM Inactivity monitor. More...
 
int32_t SDL_armR5CCMGetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo)
 Get Operation mode key value for CPU, VIM, CCM Inactivity monitor. More...
 
int32_t SDL_armR5CCMClearCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo)
 Clear Compare Error value for CPU, VIM, CCM Inactivity monitor. More...
 

CCM R5 Register IDs

enum  SDL_McuArmssCcmR5RegId {
  SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID = (0u), SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID = (1u), SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID = (2u), SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID = (3u),
  SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID = (4u), SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID = (5u), SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID = (6u), SDL_MCU_ARMSS_CCMR5_INVALID_REGID = (11u)
}
 This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs. More...
 

CCM R5 Module IDs

enum  SDL_McuArmssCcmR5ModuleId { SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID = (0u), SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID = (1u), SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID = (2u), SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID = (255u) }
 This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs. More...
 

CCM R5 Operation Mode Key values

enum  SDL_McuArmssCcmR5OpModeKey { SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE = (0u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE = (6u), SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE = (9u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE = (15u) }
 This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs. More...
 

Enumeration Type Documentation

◆ SDL_McuArmssCcmR5RegId

This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID 

register id for Status Register 1

SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID 

register id for KEY register 1

SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID 

register id for Status Register 2

SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID 

register id for KEY register 2

SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID 

register id for Status Register 3

SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID 

register id for KEY register 3

SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID 

register id for Polatiry Control Reg

SDL_MCU_ARMSS_CCMR5_INVALID_REGID 

Invalid RegID

◆ SDL_McuArmssCcmR5ModuleId

This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID 

module id for Cpu

SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID 

module id for VIM

SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID 

module id for Inactivity monitor

SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID 

invalid module id for Cpu

◆ SDL_McuArmssCcmR5OpModeKey

This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs.

Enumerator
SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE 

compare mode active operation Mode key

SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE 

Self Test active operation Mode key

SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE 

Error Force mode operation Mode key

SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE 

Self test and Error Force Mode key

Function Documentation

◆ SDL_armR5ReadCCMRegister()

int32_t SDL_armR5ReadCCMRegister ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5RegId  regId,
uint32_t *  pValToBeRead,
int32_t *  pMetaInfo 
)

Read CCM Regiser.

This function reads the contents of a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
regId[IN] CCMR5 register ID to be read
pValToBeRead[OUT] pointer to address of Register value read
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL

◆ SDL_armR5ConfigureCCMRegister()

int32_t SDL_armR5ConfigureCCMRegister ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5RegId  regId,
uint32_t  valToBeWritten,
int32_t *  pMetaInfo 
)

Configure CCM Regiser.

This function configures a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
regId[IN] CCMR5 register ID to be configured
valToBeWritten[OUT] Register value to be written to
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL

◆ SDL_armR5CCMSetOperationModeKey()

int32_t SDL_armR5CCMSetOperationModeKey ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5ModuleId  moduleId,
SDL_McuArmssCcmR5OpModeKey  opModeKey,
int32_t *  pMetaInfo 
)

Configure Operating mode for CPU, VIM, CCM Inactivity monitor.

This function configures a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
moduleId[IN] CCMR5 module ID to be configured
opModeKey[OUT] Operating mode to be set in KEY register
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL

◆ SDL_armR5CCMGetCompareError()

int32_t SDL_armR5CCMGetCompareError ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5ModuleId  moduleId,
uint32_t *  pCmpError,
int32_t *  pMetaInfo 
)

Read Compare Error status for CPU, VIM, CCM Inactivity monitor.

This function reads the a Compare Error status and returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
moduleId[IN] CCMR5 module ID to be configured
pCmpError[OUT] Pointer to Compare Error for the module
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL

◆ SDL_armR5CCMGetOperationModeKey()

int32_t SDL_armR5CCMGetOperationModeKey ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5ModuleId  moduleId,
SDL_McuArmssCcmR5OpModeKey pOpModeKey,
int32_t *  pMetaInfo 
)

Get Operation mode key value for CPU, VIM, CCM Inactivity monitor.

This function reads the a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
moduleId[IN] CCMR5 module ID to be configured
pOpModeKey[OUT] Pointer to Operation Mode for the module
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL Note: Please note that we cannot read the value that is written to the MKEY register unless the programmed key value is lockstep mode Additional information: Only 4 valid key values are expected to be programmed
  1. LOCK_STEP_MODE
  2. SELF_TEST_MODE
  3. ERR_FORCE_MODE
  4. ST_ERR_FORCE_MODE For any other value that is programmed the CCMKEYR register would reflect LOCK_STEP MODE. Also the error forcing/self test error forcing mode operates for 1 cpuclk cycle and after that the key register would reflect the LOCK STEP mode, even though the ERR FORCE & SELF TEST ERR FORCE mode would not complete in 1 cycle

◆ SDL_armR5CCMClearCompareError()

int32_t SDL_armR5CCMClearCompareError ( uintptr_t  baseAddress,
SDL_McuArmssCcmR5ModuleId  moduleId,
int32_t *  pMetaInfo 
)

Clear Compare Error value for CPU, VIM, CCM Inactivity monitor.

This function clears the a Compare Error Statusand returns the status of the operation for API caller to indicate success or failure on the operation.

Parameters
baseAddress[IN] Base address of MCU_ARMSS_CCMR5 registers
moduleId[IN] CCMR5 module ID to be configured
pMetaInfo[OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable
Returns
The SDL error code for the API. Success: SDL_PASS Fail : SDL_EFAIL