AM273x MCU+ SDK  08.06.00
MIBSPI_ControllerModeParams Struct Reference

Detailed Description

MIBSPI controller Parameters.

MIBSPI controller Parameters are used with the MIBSPI_open() call when mode is set to SPI_CONTROLLER. Default values for these parameters are set using MIBSPI_Params_init().

See also
MIBSPI_Params_init()

Data Fields

uint32_t bitRate
 
uint8_t numPeripherals
 
uint8_t t2cDelay
 
uint8_t c2tDelay
 
uint8_t wDelay
 
MIBSPI_PeripheralProfile peripheralProf [MIBSPI_PERIPHERAL_MAX]
 

Field Documentation

◆ bitRate

uint32_t MIBSPI_ControllerModeParams::bitRate

SPI bit rate in Hz

◆ numPeripherals

uint8_t MIBSPI_ControllerModeParams::numPeripherals

Number of peripherals connected to SPI controller

◆ t2cDelay

uint8_t MIBSPI_ControllerModeParams::t2cDelay

Transmit end to chip select inactive delay

◆ c2tDelay

uint8_t MIBSPI_ControllerModeParams::c2tDelay

Chip select active to transmit start delay

◆ wDelay

uint8_t MIBSPI_ControllerModeParams::wDelay

Delay in between transmissions

◆ peripheralProf

MIBSPI_PeripheralProfile MIBSPI_ControllerModeParams::peripheralProf[MIBSPI_PERIPHERAL_MAX]

Peripheral profile for each peripheral