AM273x MCU+ SDK  08.06.00
MIBSPI_PeripheralProfile Struct Reference

Detailed Description

MIBSPI peripheral profile Parameters.

When MIBSPI is configured as controller mode, it may connect to multiple peripherals. This data structure captures the the configurations for remote peripherals.

Data Fields

uint8_t chipSelect
 
uint8_t ramBufLen
 
uint32_t dmaReqLine
 

Field Documentation

◆ chipSelect

uint8_t MIBSPI_PeripheralProfile::chipSelect

CS0-CS7 signal number from 0 -7

◆ ramBufLen

uint8_t MIBSPI_PeripheralProfile::ramBufLen

RAM Length in bytes that used by the peripheral

◆ dmaReqLine

uint32_t MIBSPI_PeripheralProfile::dmaReqLine

DMA request line to be used for peripheral