AM273x MCU+ SDK  08.06.00
sdl_soc_ccm.h File Reference

Go to the source code of this file.

Macros

#define SDL_ESM_INSTANCE_MSS   (SDL_ESMG1_CCMR5_ST_ERR)
 
#define SDL_INTR_GROUP_NUM   1U
 
#define SDL_INTR_GROUP_NUMBER   2U
 
#define BASEADDRESS   SDL_MSS_CCMR_U_BASE
 
#define ESM_INSTANCE   SDL_ESM_INST_MSS_ESM
 
#define SDL_INTR_PRIORITY_LVL   1U
 
#define SDL_ENABLE_ERR_PIN   1U
 
#define SDL_ESM_MAX_EVENT_MAP_NUM   2u
 
#define SDL_MSS_CCMR   0U
 
#define SDL_CCM_MAX_INSTANCE   1U
 

Typedefs

typedef uint32_t SDL_CCM_Inst
 CCM Instance supported. More...
 

Functions

int32_t SDL_ESM_CCMapplicationCallback (SDL_ESM_Inst esmInstType, int32_t grpChannel, int32_t intSrc, void *arg)
 

Variables

static uint32_t SDL_CCM_baseAddress [SDL_CCM_MAX_INSTANCE]
 This API is used to get the base address of the instance. More...