AM273x MCU+ SDK  08.05.00

Detailed Description

HWA Paramset Config.

HWA paramset config parameters that are used with the HWA_ConfigParamSet() call.

Data Fields

uint8_t triggerMode
 
uint8_t triggerSrc
 
uint8_t accelMode
 
HWA_SourceConfig source
 
HWA_DestConfig dest
 
union {
   HWA_AccelModeFFT   fftMode
 
   HWA_AccelModeCFAR   cfarMode
 
   HWA_AccelModeLocalMax   localMaxMode
 
   HWA_AccelModeCompress   compressMode
 
accelModeArgs
 
uint8_t contextswitchCfg
 

Field Documentation

◆ triggerMode

uint8_t HWA_ParamConfig::triggerMode

4 bit value: See HWA_TRIG_MODE macros for correct values. Sets the TRIGMODE bits of HEADER in paramset

◆ triggerSrc

uint8_t HWA_ParamConfig::triggerSrc

5 bit value: If HWA_ParamConfig::triggerMode is set HWA_TRIG_MODE::HWA_TRIG_MODE_DMA, this field specifies DMA channel number to be monitored. If HWA_ParamConfig::triggerMode is set HWA_TRIG_MODE::HWA_TRIG_MODE_HARDWARE, this field specifies one of the possible csirx IRQs. this field only applied to the HWA_TRIG_MODE::HWA_TRIG_MODE_DMA and HWA_TRIG_MODE::HWA_TRIG_MODE_HARDWARE. Sets the DMA2ACC_TRIGSRC bits of HEADER in paramset

◆ accelMode

uint8_t HWA_ParamConfig::accelMode

2 bit value: See HWA_ACCELMODE macros for correct values. Configures the mode of operation of the accelerator for the current parameter-set. Sets the ACCEL_MODE bits of register HEADER in paramset

◆ source

HWA_SourceConfig HWA_ParamConfig::source

Source related params

◆ dest

HWA_DestConfig HWA_ParamConfig::dest

Dest related params

◆ fftMode

HWA_AccelModeFFT HWA_ParamConfig::fftMode

FFT mode related params

◆ cfarMode

HWA_AccelModeCFAR HWA_ParamConfig::cfarMode

CFAR mode related params

◆ localMaxMode

HWA_AccelModeLocalMax HWA_ParamConfig::localMaxMode

local maxima related params

◆ compressMode

HWA_AccelModeCompress HWA_ParamConfig::compressMode

compression and decompression related params

◆ accelModeArgs

union { ... } HWA_ParamConfig::accelModeArgs

◆ contextswitchCfg

uint8_t HWA_ParamConfig::contextswitchCfg

enable/disable the context switch, if enabled, specify if it is forced or not-forced enable See HWA_PARAMSET_CONTEXT_SWITCH_CFG macros for correct values