AM273x MCU+ SDK  08.05.00

Introduction

The HWA driver provides APIs to configure, trigger and obtain results from the hardware accelerator

Sub Modules

 HWA Driver Error Codes
 The section has a list of all the error codes which are generated by the HWA Driver module.
 
 HWA Driver External Data Structures
 The section has a list of all the data structures which are exposed to the application.
 
 HWA Driver External Functions
 The section has a list of all the exported API which the applications need to invoke in order to use the driver.