![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
39 #ifndef SDL_SOC_RTI_H_
40 #define SDL_SOC_RTI_H_
42 #include <sdl/include/am273x/sdlr_soc_baseaddress.h>
57 #define SDL_RTI_MAX_INSTANCE (0x07)
58 #define INSTANCE_INVALID (0x0U)
88 SDL_MSS_RTIC_U_BASE,SDL_DSS_RTIA_U_BASE, \
89 SDL_DSS_RTIB_U_BASE, \
90 SDL_INSTANCE_INVALID};
@ SDL_INSTANCE_DSS_WDT
Definition: sdl_soc_rti.h:72
@ SDL_INSTANCE_DSS_RTIA
Definition: sdl_soc_rti.h:76
@ SDL_INSTANCE_MSS_RTIB
Definition: sdl_soc_rti.h:74
@ SDL_INSTANCE_INVALID
Definition: sdl_soc_rti.h:78
@ SDL_INSTANCE_DSS_RTIB
Definition: sdl_soc_rti.h:77
#define SDL_RTI_MAX_INSTANCE
Definition: sdl_soc_rti.h:57
@ SDL_INSTANCE_MSS_RTIC
Definition: sdl_soc_rti.h:75
static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U]
Definition: sdl_soc_rti.h:87
@ SDL_INSTANCE_MSS_WDT
Definition: sdl_soc_rti.h:71
@ SDL_INSTANCE_MSS_RTIA
Definition: sdl_soc_rti.h:73
SDL_RTI_InstanceType
Definition: sdl_soc_rti.h:69
int32_t SDL_RTI_getBaseaddr(SDL_RTI_InstanceType instance, uint32_t *baseAddr)