The Digital Watchdog Timer(DWT) generates reset after a programmable period, if not serviced within that period. In DWT, time-out boundary is configurable. In DWWD, along with configurable time-out boundary, the start time boundary is also configurable. The DWWD can generate Reset or Interrupt, if not serviced within window(Open Window) defined by start time and time-out boundary. Also the DWWD can generate Reset or Interrupt if serviced outside Open Window (within Closed Window). Generation * of Reset or Interrupt depends on the DWWD Reaction configuration.
The Digital Watchdog Timer(DWT) generates reset after a programmable period, if not serviced within that period. In DWT, time-out boundary is configurable. In DWWD, along with configurable time-out boundary, the start time boundary is also configurable. The DWWD can generate Reset or Interrupt, if not serviced within window(Open Window) defined by start time and time-out boundary. Also the DWWD can generate Reset or Interrupt if serviced outside Open Window (within Closed Window). Generation of Reset or Interrupt depends on the DWWD Reaction configuration.
◆ SDL_RTI_MAX_INSTANCE
#define SDL_RTI_MAX_INSTANCE (0x07) |
◆ INSTANCE_INVALID
#define INSTANCE_INVALID (0x0U) |
◆ SDL_RTI_getBaseaddr()
◆ SDL_RTI_baseAddress
Initial value:= {SDL_MSS_WDT_U_BASE,SDL_DSS_WDT_U_BASE,SDL_MSS_RTIA_U_BASE,SDL_MSS_RTIB_U_BASE,
SDL_MSS_RTIC_U_BASE,SDL_DSS_RTIA_U_BASE,
SDL_DSS_RTIB_U_BASE,