Go to the source code of this file.
Macros | |
#define | SDL_HWA_CFG (uint32_t)SDL_DSS_HWA_CFG_U_BASE |
#define | SDL_HWA_BUS_CFG (uint32_t)SDL_DSS_CTRL_U_BASE |
#define | SDL_HWA_DMA0_ADDRESS (uint32_t)SDL_DSS_HWA_DMA0_U_BASE |
#define | SDL_HWA_DMA1_ADDRESS (uint32_t)SDL_DSS_HWA_DMA1_U_BASE |
Enumerations | |
enum | SDL_HWA_MemBlock { SDL_HWA_DMEM0 = 0, SDL_HWA_DMEM1 = 1, SDL_HWA_DMEM2 = 2, SDL_HWA_DMEM3 = 3, SDL_HWA_DMEM4 = 4, SDL_HWA_DMEM5 = 5, SDL_HWA_DMEM6 = 6, SDL_HWA_DMEM7 = 7, SDL_HWA_WINDOW_RAM = 8, SDL_HWA_FSM_LOCKSTEP = 9, SDL_HWA_INVALID = 10 } |
This enumerator defines the HWA memories. More... | |
enum | SDL_HWA_MemID { SDL_HWA_DMA0_MEM_ID = 0, SDL_HWA_DMA1_MEM_ID = 1, SDL_HWA_WINDOW_RAM_MEM_ID = 2, SDL_HWA_INVALID_ID = 3 } |
This enumerator defines the HWA IDs. More... | |
Functions | |
int32_t | SDL_HWA_getMemblockBaseaddr (SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock, uint32_t *baseAddr) |
This API is used to get the memory block base address. More... | |