![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
39 #ifndef SDL_HWA_SOC_H_
40 #define SDL_HWA_SOC_H_
46 #include <sdl/include/am273x/sdlr_soc_baseaddress.h>
56 #define SDL_HWA_CFG (uint32_t)SDL_DSS_HWA_CFG_U_BASE
57 #define SDL_HWA_BUS_CFG (uint32_t)SDL_DSS_CTRL_U_BASE
58 #define SDL_HWA_DMA0_ADDRESS (uint32_t)SDL_DSS_HWA_DMA0_U_BASE
59 #define SDL_HWA_DMA1_ADDRESS (uint32_t)SDL_DSS_HWA_DMA1_U_BASE
@ SDL_HWA_DMEM4
Definition: sdl_hwa_soc.h:73
SDL_HWA_MemBlock
This enumerator defines the HWA memories.
Definition: sdl_hwa_soc.h:64
@ SDL_HWA_DMEM7
Definition: sdl_hwa_soc.h:79
int32_t SDL_HWA_getMemblockBaseaddr(SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock, uint32_t *baseAddr)
This API is used to get the memory block base address.
@ SDL_HWA_DMEM1
Definition: sdl_hwa_soc.h:67
@ SDL_HWA_DMEM5
Definition: sdl_hwa_soc.h:75
@ SDL_HWA_DMA1_MEM_ID
Definition: sdl_hwa_soc.h:96
@ SDL_HWA_INVALID
Definition: sdl_hwa_soc.h:85
@ SDL_HWA_FSM_LOCKSTEP
Definition: sdl_hwa_soc.h:83
@ SDL_HWA_WINDOW_RAM_MEM_ID
Definition: sdl_hwa_soc.h:98
@ SDL_HWA_WINDOW_RAM
Definition: sdl_hwa_soc.h:81
@ SDL_HWA_DMEM2
Definition: sdl_hwa_soc.h:69
@ SDL_HWA_INVALID_ID
Definition: sdl_hwa_soc.h:100
@ SDL_HWA_DMEM3
Definition: sdl_hwa_soc.h:71
@ SDL_HWA_DMEM6
Definition: sdl_hwa_soc.h:77
SDL_HWA_MemID
This enumerator defines the HWA IDs.
Definition: sdl_hwa_soc.h:93
@ SDL_HWA_DMEM0
Definition: sdl_hwa_soc.h:65
@ SDL_HWA_DMA0_MEM_ID
Definition: sdl_hwa_soc.h:94