Go to the source code of this file.
Macros | |
#define | SDL_DSS_L3_CTRL SDL_DSS_CTRL_U_BASE |
#define | SDL_DSS_L3_BANKA_ADDRESS SDL_DSS_L3_U_BASE |
#define | SDL_DSS_L3_BANK_SIZE (0x100000U) |
#define | SDL_DSS_L3_BANKB_ADDRESS SDL_DSS_L3_BANKA_ADDRESS+SDL_DSS_L3_BANK_SIZE |
#define | SDL_DSS_L3_BANKC_ADDRESS SDL_DSS_L3_BANKB_ADDRESS+SDL_DSS_L3_BANK_SIZE |
#define | SDL_DSS_L3_BANKD_ADDRESS SDL_DSS_L3_BANKC_ADDRESS+SDL_DSS_L3_BANK_SIZE |
Enumerations | |
enum | SDL_DSS_L3_MemID { SDL_DSS_L3_BANKA_MEM_ID = 0, SDL_DSS_L3_BANKB_MEM_ID = 1, SDL_DSS_L3_BANKC_MEM_ID = 2, SDL_DSS_L3_BANKD_MEM_ID = 3, SDL_DSS_L3_INVALID_MEM_ID = 4 } |
This enumerator defines the HWA IDs. More... | |