This file contains the prototypes of the APIs present in the device abstraction layer file of MBOX. This also contains some related macros.
Go to the source code of this file.
Enumerations | |
enum | SDL_MBOX_busSftyFiType { SDL_MBOX_FI_MAIN =0, SDL_MBOX_FI_SAFE = 1, SDL_MBOX_FI_GLOBAL_MAIN =2, SDL_MBOX_FI_GLOBAL_SAFE =3, SDL_MBOX_FI_INVALID = 4 } |
enum | SDL_MBOX_busSftyFiRedType { SDL_MBOX_MAIN_CMD_INTERFACE =0, SDL_MBOX_MAIN_WRITE_INTERFACE =1, SDL_MBOX_MAIN_WRITE_STATUS_INTERFACE =2, SDL_MBOX_MAIN_READ_INTERFACE =3, SDL_MBOX_FI_TYPE_INVALID =4 } |
Functions | |
void | SDL_MSS_MBOX_secExecute (void) |
This API is used for SEC test on MSS MBOX. More... | |
void | SDL_MSS_MBOX_dedExecute (void) |
This API is used for DED test on MSS MBOX. More... | |
int32_t | SDL_MSS_MBOX_redExecute (SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType) |
This API is used for RED test on MSS MBOX. More... | |
void | SDL_MSS_MBOX_secErrorClear (void) |
This API is used to clear SEC error from MSS MBOX. More... | |
void | SDL_MSS_MBOX_dedErrorClear (void) |
This API is used to clear DED error from MSS MBOX. More... | |
void | SDL_MSS_MBOX_redErrorClear (void) |
This API is used to clear RED error from MSS MBOX. More... | |
void | SDL_DSS_MBOX_secExecute (void) |
This API is used for SEC test on DSS MBOX. More... | |
void | SDL_DSS_MBOX_dedExecute (void) |
This API is used for DED test on DSS MBOX. More... | |
int32_t | SDL_DSS_MBOX_redExecute (SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType) |
This API is used for RED test on DSS MBOX. More... | |
void | SDL_DSS_MBOX_secErrorClear (void) |
This API is used to clear SEC error from DSS MBOX. More... | |
void | SDL_DSS_MBOX_dedErrorClear (void) |
This API is used to clear DED error from DSS MBOX. More... | |
void | SDL_DSS_MBOX_redErrorClear (void) |
This API is used to clear RED error from DSS MBOX. More... | |
void | SDL_RSS_MBOX_secExecute (void) |
This API is used for SEC test on RSS MBOX. More... | |
void | SDL_RSS_MBOX_dedExecute (void) |
This API is used for DED test on RSS MBOX. More... | |
int32_t | SDL_RSS_MBOX_redExecute (SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType) |
This API is used for RED test on RSS MBOX. More... | |
void | SDL_RSS_MBOX_secErrorClear (void) |
This API is used to clear SEC error from RSS MBOX. More... | |
void | SDL_RSS_MBOX_dedErrorClear (void) |
This API is used to clear DED error from RSS MBOX. More... | |
void | SDL_RSS_MBOX_redErrorClear (void) |
This API is used to clear RED error from RSS MBOX. More... | |
uint32_t | SDL_DSS_MBOX_secErrorStatus (void) |
This API is used to get the SEC error status on DSS MBOX. More... | |
uint32_t | SDL_RSS_MBOX_secErrorStatus (void) |
This API is used to get the SEC error status on RSS MBOX. More... | |
uint32_t | SDL_DSS_MBOX_dedErrorStatus (void) |
This API is used to get the DED error status on MSS MBOX. More... | |
uint32_t | SDL_RSS_MBOX_dedErrorStatus (void) |
This API is used to get the DED error status on RSS MBOX. More... | |
uint32_t | SDL_DSS_MBOX_redErrorStatus (void) |
This API is used to get the RED error status on MSS MBOX. More... | |
uint32_t | SDL_RSS_MBOX_redErrorStatus (void) |
This API is used to get the RED error status on RSS MBOX. More... | |