![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
63 #include "sdl_mbox_hw.h"
64 #include <sdl/mbox/v0/soc/sdl_mbox_soc.h>
@ SDL_MBOX_FI_SAFE
Definition: mbox/v0/sdl_mbox.h:80
@ SDL_MBOX_FI_INVALID
Definition: mbox/v0/sdl_mbox.h:83
void SDL_MSS_MBOX_redErrorClear(void)
This API is used to clear RED error from MSS MBOX.
void SDL_RSS_MBOX_dedExecute(void)
This API is used for DED test on RSS MBOX.
void SDL_MSS_MBOX_secExecute(void)
This API is used for SEC test on MSS MBOX.
int32_t SDL_MSS_MBOX_redExecute(SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType)
This API is used for RED test on MSS MBOX.
@ SDL_MBOX_MAIN_READ_INTERFACE
Definition: mbox/v0/sdl_mbox.h:91
@ SDL_MBOX_FI_GLOBAL_MAIN
Definition: mbox/v0/sdl_mbox.h:81
@ SDL_MBOX_FI_TYPE_INVALID
Definition: mbox/v0/sdl_mbox.h:92
@ SDL_MBOX_MAIN_CMD_INTERFACE
Definition: mbox/v0/sdl_mbox.h:88
uint32_t SDL_DSS_MBOX_dedErrorStatus(void)
This API is used to get the DED error status on MSS MBOX.
void SDL_DSS_MBOX_dedExecute(void)
This API is used for DED test on DSS MBOX.
void SDL_DSS_MBOX_redErrorClear(void)
This API is used to clear RED error from DSS MBOX.
uint32_t SDL_RSS_MBOX_redErrorStatus(void)
This API is used to get the RED error status on RSS MBOX.
void SDL_RSS_MBOX_dedErrorClear(void)
This API is used to clear DED error from RSS MBOX.
void SDL_MSS_MBOX_dedExecute(void)
This API is used for DED test on MSS MBOX.
@ SDL_MBOX_FI_MAIN
Definition: mbox/v0/sdl_mbox.h:79
void SDL_MSS_MBOX_dedErrorClear(void)
This API is used to clear DED error from MSS MBOX.
uint32_t SDL_RSS_MBOX_secErrorStatus(void)
This API is used to get the SEC error status on RSS MBOX.
uint32_t SDL_RSS_MBOX_dedErrorStatus(void)
This API is used to get the DED error status on RSS MBOX.
@ SDL_MBOX_MAIN_WRITE_STATUS_INTERFACE
Definition: mbox/v0/sdl_mbox.h:90
uint32_t SDL_DSS_MBOX_redErrorStatus(void)
This API is used to get the RED error status on MSS MBOX.
uint32_t SDL_DSS_MBOX_secErrorStatus(void)
This API is used to get the SEC error status on DSS MBOX.
@ SDL_MBOX_FI_GLOBAL_SAFE
Definition: mbox/v0/sdl_mbox.h:82
void SDL_MSS_MBOX_secErrorClear(void)
This API is used to clear SEC error from MSS MBOX.
int32_t SDL_RSS_MBOX_redExecute(SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType)
This API is used for RED test on RSS MBOX.
void SDL_RSS_MBOX_redErrorClear(void)
This API is used to clear RED error from RSS MBOX.
void SDL_DSS_MBOX_secErrorClear(void)
This API is used to clear SEC error from DSS MBOX.
SDL_MBOX_busSftyFiRedType
Definition: mbox/v0/sdl_mbox.h:87
void SDL_RSS_MBOX_secErrorClear(void)
This API is used to clear SEC error from RSS MBOX.
SDL_MBOX_busSftyFiType
Definition: mbox/v0/sdl_mbox.h:78
int32_t SDL_DSS_MBOX_redExecute(SDL_MBOX_busSftyFiType fiType, SDL_MBOX_busSftyFiRedType redType)
This API is used for RED test on DSS MBOX.
void SDL_DSS_MBOX_secExecute(void)
This API is used for SEC test on DSS MBOX.
@ SDL_MBOX_MAIN_WRITE_INTERFACE
Definition: mbox/v0/sdl_mbox.h:89
void SDL_DSS_MBOX_dedErrorClear(void)
This API is used to clear DED error from DSS MBOX.
void SDL_RSS_MBOX_secExecute(void)
This API is used for SEC test on RSS MBOX.