AM273x MCU+ SDK  08.05.00
enet_cpdma.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet CPDMA data path (DMA) interface.

Go to the source code of this file.

Data Structures

struct  EnetCpdma_PktTsInfo
 CPPI buffer timestamp info. More...
 
struct  EnetCpdma_SGListEntry
 Transmit Packet scatter gather list entry. More...
 
struct  EnetCpdma_SGList
 Transmit packet scatter list info. More...
 
struct  EnetCpdma_PktInfo
 Packet data structure. More...
 
struct  EnetCpdma_OpenTxChPrms
 Param struct for the TX channel open function. More...
 
struct  EnetCpdma_OpenRxChPrms
 Param struct for the RX channel open function. More...
 
struct  EnetCpdma_RxChInitPrms
 Global Param struct for the Rx channel open. More...
 
struct  EnetCpdma_Cfg
 Config structure for Enet CPDMA. More...
 
struct  EnetDma_initCfg
 Config structure for Enet CPDMA Data Path initialization. More...
 

Macros

#define ENET_CPDMA_CPSW_MAX_SG_LIST   (4U)
 
#define ENET_CPDMA_CSUM_START_BYTE_SHIFT   (16U)
 
#define ENET_CPDMA_CSUM_START_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_START_BYTE_SHIFT)
 
#define ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT   (24U)
 
#define ENET_CPDMA_CSUM_RESULT_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT)
 
#define ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT   (0U)
 
#define ENET_CPDMA_CSUM_BYTE_COUNT_MASK   (((uint32_t) 0x3FFU) << ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT)
 
#define ENET_CPDMA_GET_CSUM_RESULT_BYTE(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_RESULT_BYTE)
 
#define ENET_CPDMA_GET_CSUM_START_BYTE(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_START_BYTE)
 
#define ENET_CPDMA_GET_CSUM_BYTE_COUNT(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_BYTE_COUNT)
 
Enet CPDMA instance configuration

Configuration macros for Enet CPDMA module.

#define ENET_CPDMA_CPSW_MAX_TX_CH   (8U)
 Maximum number of CPSW TX DMA channels. More...
 
#define ENET_CPDMA_CPSW_MAX_RX_CH   (8U)
 Maximum number of CPSW RX DMA channels. More...
 

Typedefs

typedef EnetCpdma_SGListEntry EnetDma_SGListEntry
 
typedef EnetCpdma_OpenRxChPrms EnetDma_OpenRxChPrms
 Param struct for the RX channel open function. We include this typedef as top level DMA APIs use EnetDma_OpenRxChPrms struct. More...
 
Enet DMA driver opaque handles

Enet DMA configuration structure.

Opaque handle typedefs for Enet DMA driver objects.

typedef struct EnetCpdma_Cfg_s EnetDma_Cfg
 Opaque handle that holds config Info for Enet DMA channel. More...
 
typedef void(* EnetDma_PktNotifyCb) (void *cbArg)
 Function pointer type for packet notify call back. More...
 

Functions

EnetDma_Handle EnetCpdma_open (Enet_Type enetType, uint32_t instId, const void *dmaCfg, uint32_t appCoreId)
 Set default data path parameters. More...
 
int32_t EnetCpdma_close (EnetDma_Handle hEnetDma)
 Close Enet DMA (data path). More...
 
int32_t EnetCpdma_rxThreshIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx Threshold interrupt service routine. More...
 
int32_t EnetCpdma_rxIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx interrupt service routine. More...
 
int32_t EnetCpdma_txIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Tx interrupt service routine. More...
 
int32_t EnetCpdma_miscIsrGetStatus (EnetDma_Handle hEnetDma, uint32_t *pStatusMask)
 ENET CPDMA Miscellaneous interrupt service routine. More...
 
int32_t EnetCpdma_ackMiscIsr (EnetDma_Handle hEnetDma)
 
void EnetCpdma_initParams (Enet_Type enetType, EnetDma_Cfg *pDmaConfig)
 Initialize CPDMA config params. More...