Global Param struct for the Rx channel open.
The parameter structure for the Rx channel open, containing a global channel config structure for all rx channels.
Data Fields | |
uint8_t | dmaPriority |
uint32_t | rxBufferOffset |
uint8_t EnetCpdma_RxChInitPrms::dmaPriority |
This field selects which scheduling bin the channel will be placed in for bandwidth allocation of the Rx DMA units.
uint32_t EnetCpdma_RxChInitPrms::rxBufferOffset |
Receive buffer offset