This file contains the prototypes of the APIs present in the device abstraction layer file of DSS L3. This also contains some related macros.
Go to the source code of this file.
Enumerations | |
enum | SDL_DSS_L3_busSftyFiType { SDL_DSS_L3_FI_MAIN =0, SDL_DSS_L3_FI_SAFE = 1, SDL_DSS_L3_FI_GLOBAL_MAIN =2, SDL_DSS_L3_FI_GLOBAL_SAFE =3, SDL_DSS_L3_FI_INVALID = 4 } |
enum | SDL_DSS_L3_busSftyFiRedType { SDL_DSS_L3_MAIN_CMD_INTERFACE =0, SDL_DSS_L3_MAIN_WRITE_INTERFACE =1, SDL_DSS_L3_MAIN_WRITE_STATUS_INTERFACE =2, SDL_DSS_L3_MAIN_READ_INTERFACE =3, SDL_DSS_L3_FI_TYPE_INVALID =4 } |
Functions | |
void | SDL_DSS_L3_BANKA_secExecute (void) |
This API is used for SEC test on DSS L3 Bank A. More... | |
void | SDL_DSS_L3_BANKB_secExecute (void) |
This API is used for SEC test on DSS L3 Bank B. More... | |
void | SDL_DSS_L3_BANKC_secExecute (void) |
This API is used for SEC test on DSS L3 Bank C. More... | |
void | SDL_DSS_L3_BANKD_secExecute (void) |
This API is used for SEC test on DSS L3 Bank D. More... | |
void | SDL_DSS_L3_BANKA_dedExecute (void) |
This API is used for DED test on DSS L3 Bank A. More... | |
void | SDL_DSS_L3_BANKB_dedExecute (void) |
This API is used for DED test on DSS L3 Bank B. More... | |
void | SDL_DSS_L3_BANKC_dedExecute (void) |
This API is used for DED test on DSS L3 Bank C. More... | |
void | SDL_DSS_L3_BANKD_dedExecute (void) |
This API is used for DED test on DSS L3 Bank D. More... | |
int32_t | SDL_DSS_L3_BANKA_redExecute (SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType) |
This API is used for RED test on DSS L3 Bank A. More... | |
int32_t | SDL_DSS_L3_BANKB_redExecute (SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType) |
This API is used for RED test on DSS L3 Bank B. More... | |
int32_t | SDL_DSS_L3_BANKC_redExecute (SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType) |
This API is used for RED test on DSS L3 Bank C. More... | |
int32_t | SDL_DSS_L3_BANKD_redExecute (SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType) |
This API is used for RED test on DSS L3 Bank D. More... | |
void | SDL_DSS_L3_BankA_secErrorClear (void) |
This API is used to clear SEC error from DSS_L3 Bank A. More... | |
void | SDL_DSS_L3_BankB_secErrorClear (void) |
void | SDL_DSS_L3_BankC_secErrorClear (void) |
This API is used to clear SEC error from DSS L3 Bank C. More... | |
void | SDL_DSS_L3_BankD_secErrorClear (void) |
This API is used to clear SEC error from DSS L3 Bank D. More... | |
void | SDL_DSS_L3_BankA_dedErrorClear (void) |
This API is used to clear DED error from Bank A. More... | |
void | SDL_DSS_L3_BankB_dedErrorClear (void) |
This API is used to clear DED error from Bank B. More... | |
void | SDL_DSS_L3_BankC_dedErrorClear (void) |
This API is used to clear DED error from Bank C. More... | |
void | SDL_DSS_L3_BankD_dedErrorClear (void) |
This API is used to clear DED error from Bank D. More... | |
void | SDL_DSS_L3_BankA_redErrorClear (void) |
This API is used to clear RED error from Bank A. More... | |
void | SDL_DSS_L3_BankB_redErrorClear (void) |
This API is used to clear RED error from Bank B. More... | |
void | SDL_DSS_L3_BankC_redErrorClear (void) |
This API is used to clear RED error from Bank C. More... | |
void | SDL_DSS_L3_BankD_redErrorClear (void) |
This API is used to clear RED error from Bank D. More... | |
uint32_t | SDL_DSS_L3_BankA_secErrorStatus (void) |
This API is used to get SEC error status from Bank A. More... | |
uint32_t | SDL_DSS_L3_BankB_secErrorStatus (void) |
This API is used to get SEC error status from Bank B. More... | |
uint32_t | SDL_DSS_L3_BankC_secErrorStatus (void) |
This API is used to get SEC error status from Bank C. More... | |
uint32_t | SDL_DSS_L3_BankD_secErrorStatus (void) |
This API is used to get SEC error status from Bank D. More... | |
uint32_t | SDL_DSS_L3_BankA_dedErrorStatus (void) |
This API is used to get DED error status from Bank A. More... | |
uint32_t | SDL_DSS_L3_BankB_dedErrorStatus (void) |
This API is used to get DED error status from Bank B. More... | |
uint32_t | SDL_DSS_L3_BankC_dedErrorStatus (void) |
This API is used to get DED error status from Bank C. More... | |
uint32_t | SDL_DSS_L3_BankD_dedErrorStatus (void) |
This API is used to get DED error status from Bank D. More... | |
uint32_t | SDL_DSS_L3_BankA_redErrorStatus (void) |
This API is used to get RED error status from Bank A. More... | |
uint32_t | SDL_DSS_L3_BankB_redErrorStatus (void) |
This API is used to get RED error status from Bank B. More... | |
uint32_t | SDL_DSS_L3_BankC_redErrorStatus (void) |
This API is used to get RED error status from Bank C. More... | |
uint32_t | SDL_DSS_L3_BankD_redErrorStatus (void) |
This API is used to get RED error status from Bank D. More... | |