![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
66 #include "sdl_dss_l3_hw.h"
67 #include <sdl/dss_l3/v0/soc/sdl_dss_l3_soc.h>
uint32_t SDL_DSS_L3_BankA_dedErrorStatus(void)
This API is used to get DED error status from Bank A.
void SDL_DSS_L3_BANKC_secExecute(void)
This API is used for SEC test on DSS L3 Bank C.
void SDL_DSS_L3_BankA_dedErrorClear(void)
This API is used to clear DED error from Bank A.
void SDL_DSS_L3_BANKA_secExecute(void)
This API is used for SEC test on DSS L3 Bank A.
void SDL_DSS_L3_BankC_dedErrorClear(void)
This API is used to clear DED error from Bank C.
void SDL_DSS_L3_BankB_redErrorClear(void)
This API is used to clear RED error from Bank B.
uint32_t SDL_DSS_L3_BankC_secErrorStatus(void)
This API is used to get SEC error status from Bank C.
uint32_t SDL_DSS_L3_BankD_dedErrorStatus(void)
This API is used to get DED error status from Bank D.
@ SDL_DSS_L3_FI_TYPE_INVALID
Definition: dss_l3/v0/sdl_dss_l3.h:95
@ SDL_DSS_L3_FI_GLOBAL_SAFE
Definition: dss_l3/v0/sdl_dss_l3.h:85
int32_t SDL_DSS_L3_BANKA_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank A.
void SDL_DSS_L3_BankD_redErrorClear(void)
This API is used to clear RED error from Bank D.
uint32_t SDL_DSS_L3_BankB_dedErrorStatus(void)
This API is used to get DED error status from Bank B.
uint32_t SDL_DSS_L3_BankB_redErrorStatus(void)
This API is used to get RED error status from Bank B.
void SDL_DSS_L3_BankC_redErrorClear(void)
This API is used to clear RED error from Bank C.
void SDL_DSS_L3_BankD_dedErrorClear(void)
This API is used to clear DED error from Bank D.
void SDL_DSS_L3_BankB_secErrorClear(void)
void SDL_DSS_L3_BANKC_dedExecute(void)
This API is used for DED test on DSS L3 Bank C.
int32_t SDL_DSS_L3_BANKC_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank C.
@ SDL_DSS_L3_FI_GLOBAL_MAIN
Definition: dss_l3/v0/sdl_dss_l3.h:84
void SDL_DSS_L3_BANKB_dedExecute(void)
This API is used for DED test on DSS L3 Bank B.
@ SDL_DSS_L3_FI_MAIN
Definition: dss_l3/v0/sdl_dss_l3.h:82
void SDL_DSS_L3_BANKD_dedExecute(void)
This API is used for DED test on DSS L3 Bank D.
uint32_t SDL_DSS_L3_BankC_dedErrorStatus(void)
This API is used to get DED error status from Bank C.
@ SDL_DSS_L3_MAIN_READ_INTERFACE
Definition: dss_l3/v0/sdl_dss_l3.h:94
void SDL_DSS_L3_BankD_secErrorClear(void)
This API is used to clear SEC error from DSS L3 Bank D.
void SDL_DSS_L3_BANKB_secExecute(void)
This API is used for SEC test on DSS L3 Bank B.
uint32_t SDL_DSS_L3_BankA_secErrorStatus(void)
This API is used to get SEC error status from Bank A.
void SDL_DSS_L3_BankA_redErrorClear(void)
This API is used to clear RED error from Bank A.
void SDL_DSS_L3_BANKA_dedExecute(void)
This API is used for DED test on DSS L3 Bank A.
uint32_t SDL_DSS_L3_BankA_redErrorStatus(void)
This API is used to get RED error status from Bank A.
uint32_t SDL_DSS_L3_BankC_redErrorStatus(void)
This API is used to get RED error status from Bank C.
void SDL_DSS_L3_BankA_secErrorClear(void)
This API is used to clear SEC error from DSS_L3 Bank A.
void SDL_DSS_L3_BankC_secErrorClear(void)
This API is used to clear SEC error from DSS L3 Bank C.
SDL_DSS_L3_busSftyFiType
Definition: dss_l3/v0/sdl_dss_l3.h:81
void SDL_DSS_L3_BankB_dedErrorClear(void)
This API is used to clear DED error from Bank B.
void SDL_DSS_L3_BANKD_secExecute(void)
This API is used for SEC test on DSS L3 Bank D.
uint32_t SDL_DSS_L3_BankD_secErrorStatus(void)
This API is used to get SEC error status from Bank D.
int32_t SDL_DSS_L3_BANKD_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank D.
@ SDL_DSS_L3_MAIN_WRITE_INTERFACE
Definition: dss_l3/v0/sdl_dss_l3.h:92
@ SDL_DSS_L3_MAIN_CMD_INTERFACE
Definition: dss_l3/v0/sdl_dss_l3.h:91
uint32_t SDL_DSS_L3_BankB_secErrorStatus(void)
This API is used to get SEC error status from Bank B.
@ SDL_DSS_L3_FI_INVALID
Definition: dss_l3/v0/sdl_dss_l3.h:86
int32_t SDL_DSS_L3_BANKB_redExecute(SDL_DSS_L3_busSftyFiType fiType, SDL_DSS_L3_busSftyFiRedType redType)
This API is used for RED test on DSS L3 Bank B.
@ SDL_DSS_L3_MAIN_WRITE_STATUS_INTERFACE
Definition: dss_l3/v0/sdl_dss_l3.h:93
uint32_t SDL_DSS_L3_BankD_redErrorStatus(void)
This API is used to get RED error status from Bank D.
SDL_DSS_L3_busSftyFiRedType
Definition: dss_l3/v0/sdl_dss_l3.h:90
@ SDL_DSS_L3_FI_SAFE
Definition: dss_l3/v0/sdl_dss_l3.h:83