AM273x MCU+ SDK  08.03.00

Introduction

APIs related to CSIRX debug features. Typically not used by applications.

Functions

int32_t CSIRX_debugModeSetShortPacket (CSIRX_Handle handle, uint32_t shortPacket)
 Set short packet header. More...
 
int32_t CSIRX_debugModeSetLongPacketHeader (CSIRX_Handle handle, uint32_t longPacketHeader)
 Set long packet header. More...
 
int32_t CSIRX_debugModeSetLongPacketPayload (CSIRX_Handle handle, uint32_t payload)
 Set long packet payload. More...
 
int32_t CSIRX_debugModeEnable (CSIRX_Handle handle)
 Enable debug mode. More...
 
int32_t CSIRX_debugModeDisable (CSIRX_Handle handle)
 Disable debug mode. More...
 
void CSIRX_debugModeGenerateFrames (CSIRX_Handle handle, uint16_t txFormat, uint8_t virtualChannelId, uint32_t numOfFrames, uint32_t numLinesPerFrame, uint32_t numBytesPerLine)
 Generate frames in debug mode. More...
 

Function Documentation

◆ CSIRX_debugModeSetShortPacket()

int32_t CSIRX_debugModeSetShortPacket ( CSIRX_Handle  handle,
uint32_t  shortPacket 
)

Set short packet header.

Parameters
handle[in] CSIRX driver handle
shortPacket[in] short packet header
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_debugModeSetLongPacketHeader()

int32_t CSIRX_debugModeSetLongPacketHeader ( CSIRX_Handle  handle,
uint32_t  longPacketHeader 
)

Set long packet header.

Parameters
handle[in] CSIRX driver handle
longPacketHeader[in] Long packet header
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_debugModeSetLongPacketPayload()

int32_t CSIRX_debugModeSetLongPacketPayload ( CSIRX_Handle  handle,
uint32_t  payload 
)

Set long packet payload.

Parameters
handle[in] CSIRX driver handle
payload[in] long packet payload
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_debugModeEnable()

int32_t CSIRX_debugModeEnable ( CSIRX_Handle  handle)

Enable debug mode.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_debugModeDisable()

int32_t CSIRX_debugModeDisable ( CSIRX_Handle  handle)

Disable debug mode.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_debugModeGenerateFrames()

void CSIRX_debugModeGenerateFrames ( CSIRX_Handle  handle,
uint16_t  txFormat,
uint8_t  virtualChannelId,
uint32_t  numOfFrames,
uint32_t  numLinesPerFrame,
uint32_t  numBytesPerLine 
)

Generate frames in debug mode.

CSIRX_debugModeEnable needs to be called before this API

Parameters
handle[in] CSIRX driver handle
txFormat[in] see CSIRX_DATA_FORMAT
virtualChannelId[in] 0..3
numOfFrames[in] Number of frames of debug data to generate
numLinesPerFrame[in] Lines per frame
numBytesPerLine[in] Bytes per line