AM263x MCU+ SDK  26.00.00

Introduction

This file containing the GPMC API.

The GPMC header file should be included in an application as follows:

#include <drivers/gpmc.h>

Data Structures

struct  GPMC_nandCmdParams
 Data structure to set NAND command parameters. More...
 
struct  GPMC_Transaction
 Data structure to set transaction type parameters. More...
 
struct  GPMC_Params
 GPMC driver instance parameters. More...
 
struct  GPMC_AddrRegion
 GPMC Address Region. More...
 
struct  GPMC_Object
 GPMC driver object. More...
 
struct  GPMC_timingParams
 GPMC timing parameters. More...
 
struct  GPMC_HwAttrs
 GPMC instance attributes. More...
 
struct  GPMC_Config
 GPMC Driver configuration structure. More...
 

Functions

static void GPMC_Params_init (GPMC_Params *params)
 Function to initialize the GPMC_Params struct to its defaults. More...
 
void GPMC_init (void)
 This function initializes the GPMC module. More...
 
void GPMC_deinit (void)
 This function de-initializes the GPMC module. More...
 
GPMC_Handle GPMC_open (uint32_t index, const GPMC_Params *prms)
 This function opens a given GPMC peripheral. More...
 
void GPMC_close (GPMC_Handle handle)
 Function to close a GPMC peripheral specified by the GPMC handle. More...
 
uint32_t GPMC_getInputClk (GPMC_Handle handle)
 This function returns the input clk frequency GPMC was programmed at. More...
 
GPMC_Handle GPMC_getHandle (uint32_t driverInstanceIndex)
 This function returns the handle of an open GPMC Instance from the instance index. More...
 
void GPMC_writeNandCommandParamsInit (GPMC_nandCmdParams *cmdParams)
 Function to initialise GPMC_nandCmdParams structure to default values. More...
 
int32_t GPMC_writeNandCommand (GPMC_Handle handle, GPMC_nandCmdParams *cmdParams)
 Function to write NAND command parameters. More...
 
void GPMC_transactionInit (GPMC_Transaction *trans)
 Function to initialise GPMC_Transaction structure to default values. More...
 
int32_t GPMC_nandReadData (GPMC_Handle handle, GPMC_Transaction *trans)
 Function to read data from NAND flash using DMA or CPU prefetch/post write engine. More...
 
int32_t GPMC_nandWriteData (GPMC_Handle handle, GPMC_Transaction *trans)
 Function to write data to NANDflash using CPU prefetch/post write engine. More...
 
int32_t GPMC_setDeviceSize (GPMC_Handle handle)
 Function to set device width for GPMC instance connected to external device. More...
 
int32_t GPMC_setDeviceType (GPMC_Handle handle)
 Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device. More...
 
int32_t GPMC_configureTimingParameters (GPMC_Handle handle)
 Function to configure GPMC timing parameters. More...
 
int32_t GPMC_eccValueSizeSet (GPMC_Handle handle, uint32_t eccSize, uint32_t eccSizeVal)
 Function to set ECC used and unused bytes size in nibbles. More...
 
int32_t GPMC_eccBchConfigureElm (GPMC_Handle handle, uint8_t numSectors)
 Function to configure ELM module for error correction. More...
 
int32_t GPMC_eccEngineBCHConfig (GPMC_Handle handle, uint32_t eccSteps)
 Function to configure GPMC ECC engine for BCH algorithm. More...
 
int32_t GPMC_eccEngineEnable (GPMC_Handle handle)
 Function to enable GPMC ECC engine. More...
 
void GPMC_eccResultRegisterClear (GPMC_Handle handle)
 Function to clear GPMC ECC result register. More...
 
int32_t GPMC_eccBchFillSyndromeValue (GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
 Function to fill BCH syndrome value per sector to ELM module. More...
 
int32_t GPMC_eccBchStartErrorProcessing (GPMC_Handle handle, uint8_t sector)
 Function to start error processing for a sector by ELM module. More...
 
int32_t GPMC_eccBchCheckErrorProcessingStatus (GPMC_Handle handle, uint32_t sector)
 Function to get error processing status for a sector by ELM module. More...
 
int32_t GPMC_eccBchSectorGetError (GPMC_Handle handle, uint32_t sector, uint32_t *errCount, uint32_t *errLoc)
 Function to get number of errors per sector by ELM module. More...
 
int32_t GPMC_eccCalculateBchSyndromePolynomial (GPMC_Handle handle, uint8_t *pEccdata, uint32_t sector)
 Function to compute BCH syndrome polynomial for NAND write operation. More...
 
int32_t GPMC_eccGetBchSyndromePolynomial (GPMC_Handle handle, uint32_t sector, uint32_t *bchData)
 Function to get BCH syndrome polynomial per sector NAND read operation. More...
 
int32_t GPMC_configurePrefetchPostWriteEngine (GPMC_Handle handle)
 Function to configure GPMC PREFETCH read and POST write engine. More...
 
int32_t GPMC_disableFlashWriteProtect (GPMC_Handle handle)
 Function to disable WRITE protect line. More...
 
int32_t GPMC_enableFlashWriteProtect (GPMC_Handle handle)
 Function to disable WRITE protect line. More...
 
uint8_t * GPMC_norMakeAddr (uint8_t busWidth, uint32_t blkAddr, uint32_t offset)
 Function to create correct address based on bus width. More...
 
void GPMC_norMakeCmd (uint8_t busWidth, uint32_t cmd, uint8_t *cmdBuf)
 Function to create correct NOR cmd based on bus width. More...
 
int32_t GPMC_norReadData (GPMC_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Function to read data from norlike device. More...
 
int32_t GPMC_norWriteData (GPMC_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 Function to write data to norlike device. More...
 

Typedefs

typedef GPMC_Config * GPMC_Handle
 

Enumerations

enum  GPMC_nandEccAlgo {
  GPMC_NAND_ECC_ALGO_NONE = 0x00U, GPMC_NAND_ECC_ALGO_HAMMING_1BIT, GPMC_NAND_ECC_ALGO_BCH_4BIT, GPMC_NAND_ECC_ALGO_BCH_8BIT,
  GPMC_NAND_ECC_ALGO_BCH_16BIT
}
 GPMC ECC engine algoritms. More...
 
enum  GPMC_OperatingMode { GPMC_OPERATING_MODE_BLOCKING = 0, GPMC_OPERATING_MODE_CALLBACK, GPMC_OPERATING_MODE_POLLING }
 GPMC driver operating modes. More...
 
enum  GPMC_TransferMode { GPMC_TRANSFER_MODE_BLOCKING = 0, GPMC_TRANSFER_MODE_CALLBACK }
 GPMC data transfer modes. More...
 
enum  GPMC_TransactionType { GPMC_TRANSACTION_TYPE_READ = 0, GPMC_TRANSACTION_TYPE_WRITE, GPMC_TRANSACTION_TYPE_READ_CMDREG, GPMC_TRANSACTION_TYPE_WRITE_CMDREG }
 Type of the GPMC transaction for read and write. More...
 
enum  GPMC_TransactionStatus {
  GPMC_TRANSFER_COMPLETED = 0, GPMC_TRANSFER_STARTED, GPMC_TRANSFER_CANCELED, GPMC_TRANSFER_FAILED,
  GPMC_TRANSFER_CSN_DEASSERT, GPMC_TRANSFER_TIMEOUT
}
 Transaction status codes that are set by the GPMC driver. More...
 

Macros

#define GPMC_CS_TIMING_CONFIG(CSWrOffTime, CSRdOffTime, CSExtDelayFlag, CSOnTime)
 This macro used to make the conf value which is used to configure the CS signal timing configuration. More...
 
#define GPMC_ADV_TIMING_CONFIG(ADVAADMuxWrOffTime, ADVAADMuxRdOffTime, ADVWrOffTime, ADVRdOffTime, ADVExtDelayFlag, ADVAADMuxOnTime, ADVOnTime)
 This macro used to make the conf value which is used to configure the ADV# signal timing configuration. More...
 
#define GPMC_WE_OE_TIMING_CONFIG(WEOffTime, WEExtDelayFlag, WEOnTime, OEAADMuxOffTime, OEOffTime, OEExtDelayFlag, OEAADMuxOnTime, OEOnTime)
 This macro used to make the conf value which is used to configure the WE# and OE# signal timing configuration.
. More...
 
#define GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(rdCycleTime, wrCycleTime, rdAccessTime, pageBurstAccessTime)
 This macro used to make the conf value which is used to configure the read access and cycle time timing configuration.
. More...
 
#define GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(cycle2CycleDelay, cycle2CycleDelaySameCSCfg, cycle2CycleDelayDiffCSCfg, busTAtime)
 This macro used to make the conf value which is used to configure the cycle to cycle and bus turn around time timing configuration.
. More...
 
#define GPMC_DMA_COPY_LOWER_LIMIT   (512U)
 size in bytes More...
 
#define GPMC_CS_BASE_ADDR_SHIFT   (24U)
 GPMC CHIP select base address shift value. More...
 
#define GPMC_ECC_WRAP_MODE1   (1)
 GPMC ECC Wrap mode for ECC value computation. More...
 
#define GPMC_CMD_INVALID   (0xFFFFFFFFU)
 Invalid value for params initialisation. More...
 
#define GPMC_MEM_TYPE_NAND   (0)
 
#define GPMC_MEM_TYPE_PSRAM   (1)
 
#define GPMC_MEM_TYPE_NORLIKE   (1)
 

GPMC CHIP select

Macros which can be used as to select CHIP select instance for GPMC.

#define GPMC_CHIP_SELECT_CS0   (0U)
 
#define GPMC_CHIP_SELECT_CS1   (1U)
 
#define GPMC_CHIP_SELECT_CS2   (2U)
 
#define GPMC_CHIP_SELECT_CS3   (3U)
 

GPMC Interupt status flags

Macros which can be used as 'interupt' parameter to GPMC_interuptStatusGet, GPMC_interuptStatusClear APIs.

#define GPMC_FIFOEVENT_STATUS   (0U)
 
#define GPMC_TERMINALCOUNT_STATUS   (1U)
 
#define GPMC_WAIT0EDGEDETECTION_STATUS   (2U)
 
#define GPMC_WAIT1EDGEDETECTION_STATUS   (3U)
 

GPMC Interupt Flags

Macros which can be used as 'mode' parameter to GPMC_prefetchPostWriteConfigEnable API.

#define GPMC_FIFOEVENT_INT   (0U)
 
#define GPMC_TERMINALCOUNT_INT   (1U)
 
#define GPMC_WAIT0EDGEDETECTION_INT   (2U)
 
#define GPMC_WAIT1EDGEDETECTION_INT   (3U)
 
#define GPMC_PREFETCH_ACCESSMODE_READ   (0U)
 
#define GPMC_PREFETCH_ACCESSMODE_WRITE   (1U)
 

GPMC ECC algorithm

Macros which can be used to set GPMC ECC engine algorithm.

#define GPMC_ECC_ALGORITHM_HAMMINGCODE   (0U)
 
#define GPMC_ECC_ALGORITHM_BCH   (1U)
 

GPMC ECC error correvel level.

Macros which can be used to set GPMC ECC engine error correction level.

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS   (0U)
 
#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS   (1U)
 
#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS   (2U)
 

GPMC ECC Result Register

Macros which can be used to select ECC result register for GPMC ECC engine.

#define GPMC_ECCPOINTER_RESULT_1   (1U)
 
#define GPMC_ECCPOINTER_RESULT_2   (2U)
 
#define GPMC_ECCPOINTER_RESULT_3   (3U)
 
#define GPMC_ECCPOINTER_RESULT_4   (4U)
 
#define GPMC_ECCPOINTER_RESULT_5   (5U)
 
#define GPMC_ECCPOINTER_RESULT_6   (6U)
 
#define GPMC_ECCPOINTER_RESULT_7   (7U)
 
#define GPMC_ECCPOINTER_RESULT_8   (8U)
 
#define GPMC_ECCPOINTER_RESULT_9   (9U)
 

GPMC ECC Size Config

Macros which can be used to set length of used and unsued bytes in the ECC value.

#define GPMC_ECC_SIZE_0   (0U)
 
#define GPMC_ECC_SIZE_1   (1U)
 

GPMC ECC Result Register Size

Macros which can be used to set ECC size for ECC result register.

#define GPMC_ECC_RESULT_1   (1U)
 
#define GPMC_ECC_RESULT_2   (2U)
 
#define GPMC_ECC_RESULT_3   (3U)
 
#define GPMC_ECC_RESULT_4   (4U)
 
#define GPMC_ECC_RESULT_5   (5U)
 
#define GPMC_ECC_RESULT_6   (6U)
 
#define GPMC_ECC_RESULT_7   (7U)
 
#define GPMC_ECC_RESULT_8   (8U)
 
#define GPMC_ECC_RESULT_9   (9U)
 

GPMC BCH RESULT

Macros which can be used to get BCH syndrome polynomial in GPMC_eccBchResultGet API.

#define GPMC_BCH_RESULT0   (0U)
 
#define GPMC_BCH_RESULT1   (1U)
 
#define GPMC_BCH_RESULT2   (2U)
 
#define GPMC_BCH_RESULT3   (3U)
 
#define GPMC_BCH_RESULT4   (4U)
 
#define GPMC_BCH_RESULT5   (5U)
 
#define GPMC_BCH_RESULT6   (6U)
 

GPMC CHIP Select SIZE

Macros which can be used to set chip select address size.

#define GPMC_CS_MASK_ADDR_SIZE_256MB   (0x00U)
 
#define GPMC_CS_MASK_ADDR_SIZE_128MB   (0x08U)
 
#define GPMC_CS_MASK_ADDR_SIZE_64MB   (0x0cU)
 
#define GPMC_CS_MASK_ADDR_SIZE_32MB   (0x0eU)
 
#define GPMC_CS_MASK_ADDR_SIZE_16MB   (0x0fU)
 

Macro Definition Documentation

◆ GPMC_CHIP_SELECT_CS0

#define GPMC_CHIP_SELECT_CS0   (0U)

◆ GPMC_CHIP_SELECT_CS1

#define GPMC_CHIP_SELECT_CS1   (1U)

◆ GPMC_CHIP_SELECT_CS2

#define GPMC_CHIP_SELECT_CS2   (2U)

◆ GPMC_CHIP_SELECT_CS3

#define GPMC_CHIP_SELECT_CS3   (3U)

◆ GPMC_FIFOEVENT_STATUS

#define GPMC_FIFOEVENT_STATUS   (0U)

◆ GPMC_TERMINALCOUNT_STATUS

#define GPMC_TERMINALCOUNT_STATUS   (1U)

◆ GPMC_WAIT0EDGEDETECTION_STATUS

#define GPMC_WAIT0EDGEDETECTION_STATUS   (2U)

◆ GPMC_WAIT1EDGEDETECTION_STATUS

#define GPMC_WAIT1EDGEDETECTION_STATUS   (3U)

◆ GPMC_FIFOEVENT_INT

#define GPMC_FIFOEVENT_INT   (0U)

◆ GPMC_TERMINALCOUNT_INT

#define GPMC_TERMINALCOUNT_INT   (1U)

◆ GPMC_WAIT0EDGEDETECTION_INT

#define GPMC_WAIT0EDGEDETECTION_INT   (2U)

◆ GPMC_WAIT1EDGEDETECTION_INT

#define GPMC_WAIT1EDGEDETECTION_INT   (3U)

◆ GPMC_PREFETCH_ACCESSMODE_READ

#define GPMC_PREFETCH_ACCESSMODE_READ   (0U)

◆ GPMC_PREFETCH_ACCESSMODE_WRITE

#define GPMC_PREFETCH_ACCESSMODE_WRITE   (1U)

◆ GPMC_ECC_ALGORITHM_HAMMINGCODE

#define GPMC_ECC_ALGORITHM_HAMMINGCODE   (0U)

◆ GPMC_ECC_ALGORITHM_BCH

#define GPMC_ECC_ALGORITHM_BCH   (1U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS   (0U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS   (1U)

◆ GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS

#define GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS   (2U)

◆ GPMC_ECCPOINTER_RESULT_1

#define GPMC_ECCPOINTER_RESULT_1   (1U)

◆ GPMC_ECCPOINTER_RESULT_2

#define GPMC_ECCPOINTER_RESULT_2   (2U)

◆ GPMC_ECCPOINTER_RESULT_3

#define GPMC_ECCPOINTER_RESULT_3   (3U)

◆ GPMC_ECCPOINTER_RESULT_4

#define GPMC_ECCPOINTER_RESULT_4   (4U)

◆ GPMC_ECCPOINTER_RESULT_5

#define GPMC_ECCPOINTER_RESULT_5   (5U)

◆ GPMC_ECCPOINTER_RESULT_6

#define GPMC_ECCPOINTER_RESULT_6   (6U)

◆ GPMC_ECCPOINTER_RESULT_7

#define GPMC_ECCPOINTER_RESULT_7   (7U)

◆ GPMC_ECCPOINTER_RESULT_8

#define GPMC_ECCPOINTER_RESULT_8   (8U)

◆ GPMC_ECCPOINTER_RESULT_9

#define GPMC_ECCPOINTER_RESULT_9   (9U)

◆ GPMC_ECC_SIZE_0

#define GPMC_ECC_SIZE_0   (0U)

◆ GPMC_ECC_SIZE_1

#define GPMC_ECC_SIZE_1   (1U)

◆ GPMC_ECC_RESULT_1

#define GPMC_ECC_RESULT_1   (1U)

◆ GPMC_ECC_RESULT_2

#define GPMC_ECC_RESULT_2   (2U)

◆ GPMC_ECC_RESULT_3

#define GPMC_ECC_RESULT_3   (3U)

◆ GPMC_ECC_RESULT_4

#define GPMC_ECC_RESULT_4   (4U)

◆ GPMC_ECC_RESULT_5

#define GPMC_ECC_RESULT_5   (5U)

◆ GPMC_ECC_RESULT_6

#define GPMC_ECC_RESULT_6   (6U)

◆ GPMC_ECC_RESULT_7

#define GPMC_ECC_RESULT_7   (7U)

◆ GPMC_ECC_RESULT_8

#define GPMC_ECC_RESULT_8   (8U)

◆ GPMC_ECC_RESULT_9

#define GPMC_ECC_RESULT_9   (9U)

◆ GPMC_BCH_RESULT0

#define GPMC_BCH_RESULT0   (0U)

◆ GPMC_BCH_RESULT1

#define GPMC_BCH_RESULT1   (1U)

◆ GPMC_BCH_RESULT2

#define GPMC_BCH_RESULT2   (2U)

◆ GPMC_BCH_RESULT3

#define GPMC_BCH_RESULT3   (3U)

◆ GPMC_BCH_RESULT4

#define GPMC_BCH_RESULT4   (4U)

◆ GPMC_BCH_RESULT5

#define GPMC_BCH_RESULT5   (5U)

◆ GPMC_BCH_RESULT6

#define GPMC_BCH_RESULT6   (6U)

◆ GPMC_CS_MASK_ADDR_SIZE_256MB

#define GPMC_CS_MASK_ADDR_SIZE_256MB   (0x00U)

◆ GPMC_CS_MASK_ADDR_SIZE_128MB

#define GPMC_CS_MASK_ADDR_SIZE_128MB   (0x08U)

◆ GPMC_CS_MASK_ADDR_SIZE_64MB

#define GPMC_CS_MASK_ADDR_SIZE_64MB   (0x0cU)

◆ GPMC_CS_MASK_ADDR_SIZE_32MB

#define GPMC_CS_MASK_ADDR_SIZE_32MB   (0x0eU)

◆ GPMC_CS_MASK_ADDR_SIZE_16MB

#define GPMC_CS_MASK_ADDR_SIZE_16MB   (0x0fU)

◆ GPMC_CS_TIMING_CONFIG

#define GPMC_CS_TIMING_CONFIG (   CSWrOffTime,
  CSRdOffTime,
  CSExtDelayFlag,
  CSOnTime 
)
Value:
((uint32_t) (((CSWrOffTime) << CSL_GPMC_CONFIG2_CSWROFFTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSWROFFTIME_MASK) | \
(((CSRdOffTime) << CSL_GPMC_CONFIG2_CSRDOFFTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSRDOFFTIME_MASK) | \
(((CSExtDelayFlag) << CSL_GPMC_CONFIG2_CSEXTRADELAY_SHIFT) \
& CSL_GPMC_CONFIG2_CSEXTRADELAY_MASK) | \
(((CSOnTime) << CSL_GPMC_CONFIG2_CSONTIME_SHIFT) \
& CSL_GPMC_CONFIG2_CSONTIME_MASK))

This macro used to make the conf value which is used to configure the CS signal timing configuration.

Parameters
CSWrOffTimeCS# de-assertion time from start cycle time for write accesses in GPMC_FCLK cycles.
CSRdOffTimeCS# de-assertion time from start cycle time for read accesses in GPMC_FCLK cycles
CSExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to CS or not.
This can take one of the following values :
CSL_GPMC_CONFIG2_CSEXTRADELAY_DELAYED : CS# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG2_CSEXTRADELAY_NOTDELAYED : CS# Timing control signal is not delayed.
CSOnTimeCS# assertion time from start cycle time in GPMC_FCLK cycles.

◆ GPMC_ADV_TIMING_CONFIG

#define GPMC_ADV_TIMING_CONFIG (   ADVAADMuxWrOffTime,
  ADVAADMuxRdOffTime,
  ADVWrOffTime,
  ADVRdOffTime,
  ADVExtDelayFlag,
  ADVAADMuxOnTime,
  ADVOnTime 
)
Value:
((uint32_t) (((ADVAADMuxWrOffTime) << \
CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXWROFFTIME_MASK) | \
(((ADVAADMuxRdOffTime) << CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXRDOFFTIME_MASK) | \
(((ADVWrOffTime) << CSL_GPMC_CONFIG3_ADVWROFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVWROFFTIME_MASK) | \
(((ADVRdOffTime) << CSL_GPMC_CONFIG3_ADVRDOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVRDOFFTIME_MASK) | \
(((ADVExtDelayFlag) << CSL_GPMC_CONFIG3_ADVEXTRADELAY_SHIFT) & \
CSL_GPMC_CONFIG3_ADVEXTRADELAY_MASK) | \
(((ADVAADMuxOnTime) << CSL_GPMC_CONFIG3_ADVAADMUXONTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVAADMUXONTIME_MASK) | \
(((ADVOnTime) << CSL_GPMC_CONFIG3_ADVONTIME_SHIFT) & \
CSL_GPMC_CONFIG3_ADVONTIME_MASK))

This macro used to make the conf value which is used to configure the ADV# signal timing configuration.

Parameters
ADVAADMuxWrOffTimeADV# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
ADVAADMuxRdOffTimeADV# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
ADVWrOffTimeADV# de-assertion time in GPMC_FCLK cycles from start cycle time for write accesses
ADVRdOffTimeADV# de-assertion time in GPMC_FCLK cycles from start cycle time for write accesses
ADVExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to ADV or not.
This can take one of the following values :
CSL_GPMC_CONFIG3_ADVEXTRADELAY_DELAYED : ADV# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG3_ADVEXTRADELAY_NOTDELAYED : ADV# Timing control signal is not delayed.
ADVAADMuxOnTimeADV# assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Multiplexed protocol.
ADVOnTimeADV# assertion time from start cycle time in GPMC_FCLK cycles.

◆ GPMC_WE_OE_TIMING_CONFIG

#define GPMC_WE_OE_TIMING_CONFIG (   WEOffTime,
  WEExtDelayFlag,
  WEOnTime,
  OEAADMuxOffTime,
  OEOffTime,
  OEExtDelayFlag,
  OEAADMuxOnTime,
  OEOnTime 
)
Value:
((uint32_t) (((WEOffTime) << \
CSL_GPMC_CONFIG4_WEOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG4_WEOFFTIME_MASK) | \
(((WEExtDelayFlag) << \
CSL_GPMC_CONFIG4_WEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_WEEXTRADELAY_MASK) | \
(((WEOnTime) << \
CSL_GPMC_CONFIG4_WEONTIME_SHIFT) & CSL_GPMC_CONFIG4_WEONTIME_MASK) | \
(((OEAADMuxOffTime) << \
CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_SHIFT) & \
CSL_GPMC_CONFIG4_OEAADMUXOFFTIME_MASK) | \
(((OEOffTime) << \
CSL_GPMC_CONFIG4_OEOFFTIME_SHIFT) & CSL_GPMC_CONFIG4_OEOFFTIME_MASK) | \
(((OEExtDelayFlag) << \
CSL_GPMC_CONFIG4_OEEXTRADELAY_SHIFT) & CSL_GPMC_CONFIG4_OEEXTRADELAY_MASK) | \
(((OEAADMuxOnTime) << \
CSL_GPMC_CONFIG4_OEAADMUXONTIME_SHIFT) & \
CSL_GPMC_CONFIG4_OEAADMUXONTIME_MASK) | \
(((OEOnTime) << \
CSL_GPMC_CONFIG4_OEONTIME_SHIFT) & CSL_GPMC_CONFIG4_OEONTIME_MASK))

This macro used to make the conf value which is used to configure the WE# and OE# signal timing configuration.
.

Parameters
WEOffTimeWE# de-assertion time in GPMC_FCLK cycles from start cycle time.
WEExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to WE or not.
This can take one of the following values :
CSL_GPMC_CONFIG4_WEEXTRADELAY_DELAYED : WE# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG4_WEEXTRADELAY_NOTDELAYED : WE# Timing control signal is not delayed.
WEOnTimeWE# assertion time in GPMC_FCLK cycles from start cycle time.
OEAADMuxOffTimeOE# de-assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
OEOffTimeOE# de-assertion time in GPMC_FCLK cycles from start cycle time.
OEExtDelayFlagFlag to indicate whether to add half GPMC_FCLK delay to OE or not.
This can take one of the following values : CSL_GPMC_CONFIG4_OEEXTRADELAY_DELAYED : OE# Timing control signal is delayed of half GPMC_FCLK cycle.
CSL_GPMC_CONFIG4_OEEXTRADELAY_NOTDELAYED : OE# Timing control signal is not delayed.
OEAADMuxOnTimeOE# assertion time in GPMC_FCLK cycles for first address phase when using the AAD-Mux prorocol.
OEOnTimeOE# assertion time in GPMC_FCLK cycles from start cycle time.

◆ GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG

#define GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG (   rdCycleTime,
  wrCycleTime,
  rdAccessTime,
  pageBurstAccessTime 
)
Value:
((uint32_t) (((rdCycleTime) << \
CSL_GPMC_CONFIG5_RDCYCLETIME_SHIFT) & \
CSL_GPMC_CONFIG5_RDCYCLETIME_MASK) | \
(((wrCycleTime) << \
CSL_GPMC_CONFIG5_WRCYCLETIME_SHIFT) & CSL_GPMC_CONFIG5_WRCYCLETIME_MASK) | \
(((rdAccessTime) << \
CSL_GPMC_CONFIG5_RDACCESSTIME_SHIFT) & CSL_GPMC_CONFIG5_RDACCESSTIME_MASK) | \
(((pageBurstAccessTime) << \
CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_SHIFT) & \
CSL_GPMC_CONFIG5_PAGEBURSTACCESSTIME_MASK))

This macro used to make the conf value which is used to configure the read access and cycle time timing configuration.
.

Parameters
rdCycleTimeTotal read cycle time in GPMC_FCLK cycles.
wrCycleTimeTotal write cycle time in GPMC_FCLK cycles.
rdAccessTimeRead access time (Delay between start cycle time and first data valid) in GPMC_FCLK cycles.
pageBurstAccessTimePage burest access time (Delay between successive words in a multiple access)in GPMC_FCLK cycles.

◆ GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG

#define GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG (   cycle2CycleDelay,
  cycle2CycleDelaySameCSCfg,
  cycle2CycleDelayDiffCSCfg,
  busTAtime 
)
Value:
((uint32_t) (((cycle2CycleDelay) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDELAY_MASK) | \
(((cycle2CycleDelaySameCSCfg) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_MASK) | \
(((cycle2CycleDelayDiffCSCfg) << \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_SHIFT) & \
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_MASK) | \
(((busTAtime) << \
CSL_GPMC_CONFIG6_BUSTURNAROUND_SHIFT) & CSL_GPMC_CONFIG6_BUSTURNAROUND_MASK))

This macro used to make the conf value which is used to configure the cycle to cycle and bus turn around time timing configuration.
.

Parameters
cycle2CycleDelayCycle to cycle delay (Chip select high pulse delay between two successive accesses)in GPMC_FCLK cycles.
cycle2CycleDelaySameCSCfgSpecified whether to add the cycle to cycle delay between two successive accesses or not (to the same chip-select).
This can take one of the following values :
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_C2CDELAY : To add the delay.
CSL_GPMC_CONFIG6_CYCLE2CYCLESAMECSEN_NOC2CDELAY : Don't add the delay.
cycle2CycleDelayDiffCSCfgSpecified whether to add the cycle to cycle delay between two successive accesses or not (to the diffrent chip-select).
This can take one of the following values :
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_C2CDELAY : To add the delay.
CSL_GPMC_CONFIG6_CYCLE2CYCLEDIFFCSEN_NOC2CDELAY : Don't add the delay.
busTAtimeBus turn aroung time between two successive accesses to the same chip-select (read to write) or to a diff chip-select in GPMC_FCLK cycles.

◆ GPMC_DMA_COPY_LOWER_LIMIT

#define GPMC_DMA_COPY_LOWER_LIMIT   (512U)

size in bytes

◆ GPMC_CS_BASE_ADDR_SHIFT

#define GPMC_CS_BASE_ADDR_SHIFT   (24U)

GPMC CHIP select base address shift value.

◆ GPMC_ECC_WRAP_MODE1

#define GPMC_ECC_WRAP_MODE1   (1)

GPMC ECC Wrap mode for ECC value computation.

◆ GPMC_CMD_INVALID

#define GPMC_CMD_INVALID   (0xFFFFFFFFU)

Invalid value for params initialisation.

◆ GPMC_MEM_TYPE_NAND

#define GPMC_MEM_TYPE_NAND   (0)

◆ GPMC_MEM_TYPE_PSRAM

#define GPMC_MEM_TYPE_PSRAM   (1)

◆ GPMC_MEM_TYPE_NORLIKE

#define GPMC_MEM_TYPE_NORLIKE   (1)

Typedef Documentation

◆ GPMC_Handle

Enumeration Type Documentation

◆ GPMC_nandEccAlgo

GPMC ECC engine algoritms.

Enumerator
GPMC_NAND_ECC_ALGO_NONE 
GPMC_NAND_ECC_ALGO_HAMMING_1BIT 
GPMC_NAND_ECC_ALGO_BCH_4BIT 
GPMC_NAND_ECC_ALGO_BCH_8BIT 
GPMC_NAND_ECC_ALGO_BCH_16BIT 

◆ GPMC_OperatingMode

GPMC driver operating modes.

Enumerator
GPMC_OPERATING_MODE_BLOCKING 

Interupt based blocking mode

GPMC_OPERATING_MODE_CALLBACK 

Interupt based callback mode

GPMC_OPERATING_MODE_POLLING 

Non interupt base blocking mode

◆ GPMC_TransferMode

GPMC data transfer modes.

Enumerator
GPMC_TRANSFER_MODE_BLOCKING 

GPMC driver transaction blocks execution. This mode can only be used when called within a Task context and is interrupt based.

GPMC_TRANSFER_MODE_CALLBACK 

GPMC driver transaction does not block code execution and will call a callback function. This mode can be used in a Task, Swi, or Hwi context.

◆ GPMC_TransactionType

Type of the GPMC transaction for read and write.

Enumerator
GPMC_TRANSACTION_TYPE_READ 

Read transaction

GPMC_TRANSACTION_TYPE_WRITE 

Write transaction

GPMC_TRANSACTION_TYPE_READ_CMDREG 

Read transaction with command register

GPMC_TRANSACTION_TYPE_WRITE_CMDREG 

Write transaction with command register

◆ GPMC_TransactionStatus

Transaction status codes that are set by the GPMC driver.

Enumerator
GPMC_TRANSFER_COMPLETED 
GPMC_TRANSFER_STARTED 
GPMC_TRANSFER_CANCELED 
GPMC_TRANSFER_FAILED 
GPMC_TRANSFER_CSN_DEASSERT 
GPMC_TRANSFER_TIMEOUT 

Function Documentation

◆ GPMC_Params_init()

static void GPMC_Params_init ( GPMC_Params *  params)
inlinestatic

Function to initialize the GPMC_Params struct to its defaults.

Parameters
paramsPointer to GPMC_Params structure for initialization

◆ GPMC_init()

void GPMC_init ( void  )

This function initializes the GPMC module.

◆ GPMC_deinit()

void GPMC_deinit ( void  )

This function de-initializes the GPMC module.

◆ GPMC_open()

GPMC_Handle GPMC_open ( uint32_t  index,
const GPMC_Params *  prms 
)

This function opens a given GPMC peripheral.

Precondition
GPMC controller has been initialized using GPMC_init()
Parameters
indexIndex of config to use in the GPMC_Handle array
prmsPointer to parameters GPMC_Params to open the driver instance.
Returns
A GPMC_Handle on success or a NULL on an error or if it has been opened already
See also
GPMC_init()
GPMC_close()

◆ GPMC_close()

void GPMC_close ( GPMC_Handle  handle)

Function to close a GPMC peripheral specified by the GPMC handle.

Precondition
GPMC_open() has to be called first
Parameters
handleGPMC_Handle returned from GPMC_open()
See also
GPMC_open()

◆ GPMC_getInputClk()

uint32_t GPMC_getInputClk ( GPMC_Handle  handle)

This function returns the input clk frequency GPMC was programmed at.

Precondition
GPMC controller has been opened using GPMC_open()
Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
GPMC RCLK in Hertz

◆ GPMC_getHandle()

GPMC_Handle GPMC_getHandle ( uint32_t  driverInstanceIndex)

This function returns the handle of an open GPMC Instance from the instance index.

Precondition
GPMC controller has been opened using GPMC_open()
Parameters
driverInstanceIndexIndex of config to use in the GPMC_Handle array
Returns
An GPMC_Handle if it has been opened already or NULL otherwise
See also
GPMC_init()
GPMC_open()

◆ GPMC_writeNandCommandParamsInit()

void GPMC_writeNandCommandParamsInit ( GPMC_nandCmdParams *  cmdParams)

Function to initialise GPMC_nandCmdParams structure to default values.

Parameters
cmdParamsPointer to GPMC_nandCmdParams structure

◆ GPMC_writeNandCommand()

int32_t GPMC_writeNandCommand ( GPMC_Handle  handle,
GPMC_nandCmdParams *  cmdParams 
)

Function to write NAND command parameters.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
cmdParamsPointer to GPMC_nandCmdParams structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_transactionInit()

void GPMC_transactionInit ( GPMC_Transaction *  trans)

Function to initialise GPMC_Transaction structure to default values.

Parameters
transPointer to GPMC_Transaction structure

◆ GPMC_nandReadData()

int32_t GPMC_nandReadData ( GPMC_Handle  handle,
GPMC_Transaction *  trans 
)

Function to read data from NAND flash using DMA or CPU prefetch/post write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
transPointer to GPMC_Transaction structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_nandWriteData()

int32_t GPMC_nandWriteData ( GPMC_Handle  handle,
GPMC_Transaction *  trans 
)

Function to write data to NANDflash using CPU prefetch/post write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
transPointer to GPMC_Transaction structure
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_setDeviceSize()

int32_t GPMC_setDeviceSize ( GPMC_Handle  handle)

Function to set device width for GPMC instance connected to external device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_setDeviceType()

int32_t GPMC_setDeviceType ( GPMC_Handle  handle)

Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_configureTimingParameters()

int32_t GPMC_configureTimingParameters ( GPMC_Handle  handle)

Function to configure GPMC timing parameters.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccValueSizeSet()

int32_t GPMC_eccValueSizeSet ( GPMC_Handle  handle,
uint32_t  eccSize,
uint32_t  eccSizeVal 
)

Function to set ECC used and unused bytes size in nibbles.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
eccSizeParam to set GPMC_ECC_SIZE_0 (used bytes) or GPMC_ECC_SIZE_1 unused bytes
eccSizeValECC used or ununsed bytes value in nibbles.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchConfigureElm()

int32_t GPMC_eccBchConfigureElm ( GPMC_Handle  handle,
uint8_t  numSectors 
)

Function to configure ELM module for error correction.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
numSectorsNumber of 512 bytes sector in a NAND page.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccEngineBCHConfig()

int32_t GPMC_eccEngineBCHConfig ( GPMC_Handle  handle,
uint32_t  eccSteps 
)

Function to configure GPMC ECC engine for BCH algorithm.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
eccStepsNumber of 512 bytes sectors to process BCH syndrome polynomial computation.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccEngineEnable()

int32_t GPMC_eccEngineEnable ( GPMC_Handle  handle)

Function to enable GPMC ECC engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccResultRegisterClear()

void GPMC_eccResultRegisterClear ( GPMC_Handle  handle)

Function to clear GPMC ECC result register.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()

◆ GPMC_eccBchFillSyndromeValue()

int32_t GPMC_eccBchFillSyndromeValue ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  bchData 
)

Function to fill BCH syndrome value per sector to ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
bchDataPointer to syndrome polynomial value.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchStartErrorProcessing()

int32_t GPMC_eccBchStartErrorProcessing ( GPMC_Handle  handle,
uint8_t  sector 
)

Function to start error processing for a sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchCheckErrorProcessingStatus()

int32_t GPMC_eccBchCheckErrorProcessingStatus ( GPMC_Handle  handle,
uint32_t  sector 
)

Function to get error processing status for a sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccBchSectorGetError()

int32_t GPMC_eccBchSectorGetError ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  errCount,
uint32_t *  errLoc 
)

Function to get number of errors per sector by ELM module.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
errCountPointer to store number of errors in a sector
errLocPointer to store error locations in a sector
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccCalculateBchSyndromePolynomial()

int32_t GPMC_eccCalculateBchSyndromePolynomial ( GPMC_Handle  handle,
uint8_t *  pEccdata,
uint32_t  sector 
)

Function to compute BCH syndrome polynomial for NAND write operation.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
pEccdataPointer to store BCH syndrome polynomial.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_eccGetBchSyndromePolynomial()

int32_t GPMC_eccGetBchSyndromePolynomial ( GPMC_Handle  handle,
uint32_t  sector,
uint32_t *  bchData 
)

Function to get BCH syndrome polynomial per sector NAND read operation.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
sectorSector number
bchDataPointer to store BCH syndrome polynomial.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_configurePrefetchPostWriteEngine()

int32_t GPMC_configurePrefetchPostWriteEngine ( GPMC_Handle  handle)

Function to configure GPMC PREFETCH read and POST write engine.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_disableFlashWriteProtect()

int32_t GPMC_disableFlashWriteProtect ( GPMC_Handle  handle)

Function to disable WRITE protect line.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_enableFlashWriteProtect()

int32_t GPMC_enableFlashWriteProtect ( GPMC_Handle  handle)

Function to disable WRITE protect line.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_norMakeAddr()

uint8_t* GPMC_norMakeAddr ( uint8_t  busWidth,
uint32_t  blkAddr,
uint32_t  offset 
)

Function to create correct address based on bus width.

Parameters
busWidthBus width for the NOR Flash device.
blkAddrBase address for NOR Flash.
offsetBase address for NOR Flash.
Returns
Pointer to Address

◆ GPMC_norMakeCmd()

void GPMC_norMakeCmd ( uint8_t  busWidth,
uint32_t  cmd,
uint8_t *  cmdBuf 
)

Function to create correct NOR cmd based on bus width.

Parameters
busWidthBus width for the NOR Flash device.
cmdCommand to be sent on Data Lines.
cmdBufBuffer pointer to store the modified cmd.

◆ GPMC_norReadData()

int32_t GPMC_norReadData ( GPMC_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Function to read data from norlike device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
offsetOffset of read address from GPMC data baseaddress.
bufPointer to buffer for storing read data.
lenNumber of bytes to read.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ GPMC_norWriteData()

int32_t GPMC_norWriteData ( GPMC_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

Function to write data to norlike device.

Parameters
handleAn GPMC_Handle returned from an GPMC_open()
offsetOffset of write address from GPMC data baseaddress.
bufPointer to buffer for storing read data.
lenNumber of bytes to write.
Returns
SystemP_SUCCESS or SystemP_FAILURE

Variable Documentation

◆ gGpmcConfig

GPMC_Config gGpmcConfig[]
extern

Externally defined driver configuration array.

◆ gGpmcConfigNum

uint32_t gGpmcConfigNum
extern

Externally defined driver configuration array size.