AM263x MCU+ SDK  26.00.00
SDL CCM

Introduction

This example demonstrates the usage of the SDL R5 CCM module. The example shows how to setup and use the R5 CCM Safety Diagnostic operation.

Use Cases

Use Case Description
UC-1 self test on R5 CCM.
UC-2 self test with error force on R5 CCM.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss1-0 nortos
Toolchain ti-arm-clang
Board am263x-cc
Example folder examples/sdl/ccm/sdl_ccm_example/

Steps to Run the Example

Steps to Test the Example

  • CCM example should only be tested in QSPI boot mode and should not be tested in no boot mode with debugger connected.
  • Follow the below procedure to test the CCM and CCM_VIM example.
    1. A quick recap of steps done so far that are needed for the flashing to work
      • Make sure the UART port used for terminal is identified as mentioned in Setup UART Terminal
      • Make sure python3 is installed as mentioned in Python3
      • Make sure you have the EVM power cable and UART cable connected as shown in Cable Connections
    2. Build the hello world application as mentioned in Build a Hello World example, Build a Hello World example
    3. As part of the build process in the final step a file with extension .appimage is generated. This is the file we need to flash.
    4. When building with makefiles and single-core projects, this file can be found here
         ${SDK_INSTALL_PATH}/examples/sdl/ccm/sdl_ccm_example/{board}/r5fss0-0_nortos/ti-arm-clang/sdl_ccm_example.release.appimage
      
    5. A default configuration file can be found at below path. You can edit this file directly or take a copy and edit this file.
         ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/{board}/default_sbl_qspi.cfg
      
    6. Edit below line in the config file to point to your application .appimage file. Give the absolute path to the .appimage file or path relative to ${SDK_INSTALL_PATH}/tools/boot. Make sure to use forward slash / in the filename path. –file=../../examples/sdl/ccm/sdl_ccm_example/{board}/r5fss0-0_nortos/ti-arm-clang/sdl_ccm_example.release.appimage –operation=flash –flash-offset=0x80000
      • NOTE : edit sdl_ccm_example to sdl_ccm_vim for ccm vim example testing.
    7. Save and close the config file.
    8. Flash the application by follow the steps mentioned in the page, Flash a Hello World example

See Also

CCM

Sample Output

Shown below is a sample output when the CCM application is run.

R5 CPU Application
CCM Example Test Started: R5F0
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CPU Functionality
Passed.
All tests have passed.
R5 CPU Application
CCM Example Test Started: R5F0
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CCM Example Test Started: R5F1
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CPU Functionality
Passed.
All tests have passed.

Shown below is a sample output when the TMU application is run.