Go to the source code of this file.
Macros | |
#define | SDL_CCM_ESM_U_BASE (SDL_ESM0_CCM_0_SELFTEST_ERR) |
#define | SDL_R5SS0_CCM 0U |
#define | SDL_R5SS1_CCM 1U |
#define | SDL_CCM_MAX_INSTANCE (SDL_R5SS1_CCM + 1U) |
Typedefs | |
typedef uint32_t | SDL_CCM_Inst |
CCM Instance supported. More... | |
Variables | |
static uint32_t | SDL_CCM_baseAddress [SDL_CCM_MAX_INSTANCE] |
This API is used to get the base address of the instance. More... | |