The SDL CCM module provides API for CCM Diagnostics
Sub Modules | |
CCM API | |
CCM Low-Level API | |
Typedefs | |
typedef uint32_t | SDL_CCM_Inst |
CCM Instance supported. More... | |
Macros | |
#define | SDL_CCM_ESM_U_BASE (SDL_ESM0_CCM_0_SELFTEST_ERR) |
#define | SDL_R5SS0_CCM 0U |
#define | SDL_R5SS1_CCM 1U |
#define | SDL_CCM_MAX_INSTANCE (SDL_R5SS1_CCM + 1U) |
#define SDL_CCM_ESM_U_BASE (SDL_ESM0_CCM_0_SELFTEST_ERR) |
#define SDL_R5SS0_CCM 0U |
CCM INSTANCE R5F0
#define SDL_R5SS1_CCM 1U |
CCM INSTANCE R5F1
#define SDL_CCM_MAX_INSTANCE (SDL_R5SS1_CCM + 1U) |
Maximum
typedef uint32_t SDL_CCM_Inst |
CCM Instance supported.
|
static |
This API is used to get the base address of the instance.