CCM for R5F provides APIs to select the operating modes and read the status for
Functions | |
int32_t | SDL_armR5ReadCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo) |
Read CCM Regiser. More... | |
int32_t | SDL_armR5ConfigureCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo) |
Configure CCM Regiser. More... | |
int32_t | SDL_armR5CCMSetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo) |
Configure Operating mode for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo) |
Read Compare Error status for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo) |
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMClearCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo) |
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor. More... | |
CCM R5 Register IDs | |
enum | SDL_McuArmssCcmR5RegId { SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID = (0u), SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID = (1u), SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID = (2u), SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID = (3u), SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID = (4u), SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID = (5u), SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID = (6u), SDL_MCU_ARMSS_CCMR5_INVALID_REGID = (7u) } |
This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs. More... | |
CCM R5 Module IDs | |
enum | SDL_McuArmssCcmR5ModuleId { SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID = (0u), SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID = (1u), SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID = (2u), SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID = (255u) } |
This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs. More... | |
CCM R5 Operation Mode Key values | |
enum | SDL_McuArmssCcmR5OpModeKey { SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE = (0u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE = (6u), SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE = (9u), SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE = (15u) } |
This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs. More... | |
This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs.
This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs.
This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 APIs.
int32_t SDL_armR5ReadCCMRegister | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5RegId | regId, | ||
uint32_t * | pValToBeRead, | ||
int32_t * | pMetaInfo | ||
) |
Read CCM Regiser.
This function reads the contents of a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
regId | [IN] CCMR5 register ID to be read |
pValToBeRead | [OUT] pointer to address of Register value read |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5ConfigureCCMRegister | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5RegId | regId, | ||
uint32_t | valToBeWritten, | ||
int32_t * | pMetaInfo | ||
) |
Configure CCM Regiser.
This function configures a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
regId | [IN] CCMR5 register ID to be configured |
valToBeWritten | [OUT] Register value to be written to |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMSetOperationModeKey | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
SDL_McuArmssCcmR5OpModeKey | opModeKey, | ||
int32_t * | pMetaInfo | ||
) |
Configure Operating mode for CPU, VIM, CCM Inactivity monitor.
This function configures a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
opModeKey | [OUT] Operating mode to be set in KEY register |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMGetCompareError | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
uint32_t * | pCmpError, | ||
int32_t * | pMetaInfo | ||
) |
Read Compare Error status for CPU, VIM, CCM Inactivity monitor.
This function reads the a Compare Error status and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pCmpError | [OUT] Pointer to Compare Error for the module |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMGetOperationModeKey | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
SDL_McuArmssCcmR5OpModeKey * | pOpModeKey, | ||
int32_t * | pMetaInfo | ||
) |
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor.
This function reads the a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pOpModeKey | [OUT] Pointer to Operation Mode for the module |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMClearCompareError | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
int32_t * | pMetaInfo | ||
) |
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor.
This function clears the a Compare Error Statusand returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |