AM263x MCU+ SDK  08.02.01
MPU_FIREWALL_Config Struct Reference

Detailed Description

MPU Firewall Parameters.

This structure contains parameters associated with an MPU Firewall.

Data Fields

uint32_t baseAddr
 
uint32_t numRegions
 

Field Documentation

◆ baseAddr

uint32_t MPU_FIREWALL_Config::baseAddr

< Base address of the firewall Number of regions in the firewall

◆ numRegions

uint32_t MPU_FIREWALL_Config::numRegions