AM263x MCU+ SDK  08.02.01

Introduction

This module contains APIs to program the MPU Firewall module.

Files

file  mpu_firewall/v0/mpu_firewall.h
 MPU Firewall Driver API/interface file.
 

Data Structures

struct  MPU_FIREWALL_RegionParams
 MPU Region Parameters. More...
 
struct  MPU_FIREWALL_Config
 MPU Firewall Parameters. More...
 

Functions

void MPU_FIREWALL_init ()
 This function initializes the MPU Firewall module. More...
 
int32_t MPU_FIREWALL_setRegion (MPU_FIREWALL_RegionParams *mpuParams)
 Function to configure a Firewall region. More...
 
int32_t MPU_FIREWALL_getFirewallConfig (uint32_t firewallId, MPU_FIREWALL_Config **firewallConfig)
 Function to get parameters of a firewall. More...
 
void MPU_FIREWALL_RegionParams_init (MPU_FIREWALL_RegionParams *mpuParams)
 Function to initialize the parameters of a region. More...
 
uint32_t MPU_FIREWALL_readFaultAddress (uint32_t baseAddr)
 Function to read the fault address that created the firewall violation. More...
 
uint32_t MPU_FIREWALL_readFaultStatus (uint32_t baseAddr)
 Function to read the fault status register. It contains information on the kind of firewall violation that had occurred. More...
 
void MPU_FIREWALL_clearFault (uint32_t baseAddr)
 Function to clear MPU Firewall fault address and fault status register . More...
 
void MPU_FIREWALL_interruptEnable (uint32_t baseAddr, uint32_t flag)
 Function to enable MPU Firewall interrupt. More...
 
void MPU_FIREWALL_clearInterruptEnable (uint32_t baseAddr, uint32_t flag)
 Function to disable MPU Firewall interrupt. More...
 
void MPU_FIREWALL_setInterruptStatus (uint32_t baseAddr, uint32_t flag)
 Function to set interrupt. This can be used for testing interrupts. More...
 
uint32_t MPU_FIREWALL_getInterruptStatus (uint32_t baseAddr)
 Function to read interrupt status. More...
 
void MPU_FIREWALL_clearInterruptStatus (uint32_t baseAddr, uint32_t flag)
 Function to clear interrupt status. More...
 

Function Documentation

◆ MPU_FIREWALL_init()

void MPU_FIREWALL_init ( )

This function initializes the MPU Firewall module.

◆ MPU_FIREWALL_setRegion()

int32_t MPU_FIREWALL_setRegion ( MPU_FIREWALL_RegionParams mpuParams)

Function to configure a Firewall region.

Parameters
mpuParamsStructure containing all region configuration parameters.
Returns
SystemP_SUCCESS on successful region configuration; else error on failure

◆ MPU_FIREWALL_getFirewallConfig()

int32_t MPU_FIREWALL_getFirewallConfig ( uint32_t  firewallId,
MPU_FIREWALL_Config **  firewallConfig 
)

Function to get parameters of a firewall.

Parameters
firewallIdFirewall ID.
firewallConfigStructure to save firewall config.
Returns
SystemP_SUCCESS on successful config read; else error on failure

◆ MPU_FIREWALL_RegionParams_init()

void MPU_FIREWALL_RegionParams_init ( MPU_FIREWALL_RegionParams mpuParams)

Function to initialize the parameters of a region.

Parameters
mpuParamsRegion parameter structure to be initialized.

◆ MPU_FIREWALL_readFaultAddress()

uint32_t MPU_FIREWALL_readFaultAddress ( uint32_t  baseAddr)

Function to read the fault address that created the firewall violation.

Parameters
baseAddrMPU Firewall base address
Returns
Fault address

◆ MPU_FIREWALL_readFaultStatus()

uint32_t MPU_FIREWALL_readFaultStatus ( uint32_t  baseAddr)

Function to read the fault status register. It contains information on the kind of firewall violation that had occurred.

Parameters
baseAddrMPU Firewall base address
Returns
Value of fault status register

◆ MPU_FIREWALL_clearFault()

void MPU_FIREWALL_clearFault ( uint32_t  baseAddr)

Function to clear MPU Firewall fault address and fault status register .

Parameters
baseAddrMPU Firewall base address

◆ MPU_FIREWALL_interruptEnable()

void MPU_FIREWALL_interruptEnable ( uint32_t  baseAddr,
uint32_t  flag 
)

Function to enable MPU Firewall interrupt.

Parameters
baseAddrMPU Firewall base address
flagFlag to denote the different firewall interrupts to be enabled.

◆ MPU_FIREWALL_clearInterruptEnable()

void MPU_FIREWALL_clearInterruptEnable ( uint32_t  baseAddr,
uint32_t  flag 
)

Function to disable MPU Firewall interrupt.

Parameters
baseAddrMPU Firewall base address
flagFlag to denote the different firewall interrupts to be disabled.

◆ MPU_FIREWALL_setInterruptStatus()

void MPU_FIREWALL_setInterruptStatus ( uint32_t  baseAddr,
uint32_t  flag 
)

Function to set interrupt. This can be used for testing interrupts.

Parameters
baseAddrMPU Firewall base address
flagFlag to denote the different firewall interrupts to be set.

◆ MPU_FIREWALL_getInterruptStatus()

uint32_t MPU_FIREWALL_getInterruptStatus ( uint32_t  baseAddr)

Function to read interrupt status.

Parameters
baseAddrMPU Firewall base address
Returns
Value of interrupt status register.

◆ MPU_FIREWALL_clearInterruptStatus()

void MPU_FIREWALL_clearInterruptStatus ( uint32_t  baseAddr,
uint32_t  flag 
)

Function to clear interrupt status.

Parameters
baseAddrMPU Firewall base address
flagFlag to denote the different firewall interrupts to be cleared.