The SOC driver provides API to configure SOC specific features like clocks.
Features Supported
- API to enable/disable a module clock
- API to set clock frequency for module
- Generic utility API like get CPU clock, get core name string, control module MMR lock/unlock API
- API's to configure all the SOC and Time Sync XBAR's
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- SOC driver is integrated with each of the drivers. User need not perform any explicit configuration for this driver
- The Input for every XBAR output instance can be configured through SysConfig (Input-Signals going into the XBAR, Instance-Each output signal from the XBAR)
- Refer to the following examples on how to configure XBAR through SysConfig - EPWM HR duty cycle, ECAP APWM mode, EQEP frequency measurement
- XBAR outputs routed to other XBAR's get automatically configured when input is selected for the end XBAR
Sample XBAR Configuration
- XBAR configuration also possible from the SysConfig module to which it is connected. For example, DMA Trigger XBAR can be configured from EDMA module.
Features NOT Supported
NA
Important Usage Guidelines
- Most of these APIs are already integrated with SysConfig tool and the generated code does the required call to enable a module, set the required clock and so on. User need to use these APIs in their application only for exceptional scenarios.
Example Usage
Include the below file to access the APIs
Get Core Name String
Get CPU Clock Frequency
uint64_t cpuClockRate;
DebugP_log(
"CPU Clock Frequency: %u\r\n", cpuClockRate);
API
APIs for SOC Specific Functions
APIs for SOC Reset and Clock Functions
APIs for SOC Xbars