AM263Px MCU+ SDK  26.00.00

Introduction

Functions

int32_t SDL_DCC_configure (SDL_DCC_Inst instance, const SDL_DCC_config *pConfig)
 This API is used to configure DCC module. More...
 
int32_t SDL_DCC_verifyConfig (SDL_DCC_Inst instance, const SDL_DCC_config *pConfig)
 This API is used to verify the configuration for DCC module. More...
 
int32_t SDL_DCC_enable (SDL_DCC_Inst instance)
 This API is used to enable the DCC module. More...
 
int32_t SDL_DCC_disable (SDL_DCC_Inst instance)
 This API is used to disable the DCC module. More...
 
int32_t SDL_DCC_getStatus (SDL_DCC_Inst instance, SDL_DCC_Status *pStatus)
 This API is used to get the stauts of DCC module. More...
 
int32_t SDL_DCC_enableIntr (SDL_DCC_Inst instance, SDL_DCC_intrType intr)
 This API is used to Enable the interrupts. More...
 
int32_t SDL_DCC_clearIntr (SDL_DCC_Inst instance, SDL_DCC_intrType intr)
 This API is used to clear the interrupts. More...
 
int32_t SDL_DCC_getStaticRegs (SDL_DCC_Inst instance, SDL_DCC_staticRegs *pStaticRegs)
 This API is used to get the value of static registers for DCC module. More...
 

Function Documentation

◆ SDL_DCC_configure()

int32_t SDL_DCC_configure ( SDL_DCC_Inst  instance,
const SDL_DCC_config *  pConfig 
)

This API is used to configure DCC module.

Parameters
instanceHolds the instance for DCC module.
pConfigpointer to the DCC config structure

NOTE: If the value of 'seedValid0' is less then 4 then it will programmed as 4. Since minimum programmable value of the 'seedValid0' is 4.

◆ SDL_DCC_verifyConfig()

int32_t SDL_DCC_verifyConfig ( SDL_DCC_Inst  instance,
const SDL_DCC_config *  pConfig 
)

This API is used to verify the configuration for DCC module.

Parameters
instanceHolds the instance for DCC module.
pConfigpointer to the DCC config structure

◆ SDL_DCC_enable()

int32_t SDL_DCC_enable ( SDL_DCC_Inst  instance)

This API is used to enable the DCC module.

Parameters
instanceHolds the instance for DCC module.

◆ SDL_DCC_disable()

int32_t SDL_DCC_disable ( SDL_DCC_Inst  instance)

This API is used to disable the DCC module.

Parameters
instanceHolds the instance for DCC module.

◆ SDL_DCC_getStatus()

int32_t SDL_DCC_getStatus ( SDL_DCC_Inst  instance,
SDL_DCC_Status *  pStatus 
)

This API is used to get the stauts of DCC module.

Parameters
instanceHolds the instance for DCC module.
pStatuspointer to the SDL_DCC_status structure

◆ SDL_DCC_enableIntr()

int32_t SDL_DCC_enableIntr ( SDL_DCC_Inst  instance,
SDL_DCC_intrType  intr 
)

This API is used to Enable the interrupts.

Parameters
instanceHolds the instance for DCC module.
intrInterrupts to be enabled.

◆ SDL_DCC_clearIntr()

int32_t SDL_DCC_clearIntr ( SDL_DCC_Inst  instance,
SDL_DCC_intrType  intr 
)

This API is used to clear the interrupts.

Parameters
instanceHolds the instance for DCC module.
intrInterrupts to disable.

◆ SDL_DCC_getStaticRegs()

int32_t SDL_DCC_getStaticRegs ( SDL_DCC_Inst  instance,
SDL_DCC_staticRegs *  pStaticRegs 
)

This API is used to get the value of static registers for DCC module.

Parameters
instanceHolds the instance for DCC module.
pStaticRegsPointer to the SDL_DCC_staticRegs structure.