USB intialization parameter block.
Data Fields | |
| uint32_t | instanceNum |
| uint32_t | clkSrcSel |
| uint32_t | pllRefSel |
| uint32_t | usb2Enable |
| uint32_t | invertPolarity |
| uint32_t | vbusSel |
| uint32_t | isHostMode |
| uint32_t usb_init_param_t::instanceNum |
| uint32_t usb_init_param_t::clkSrcSel |
| uint32_t usb_init_param_t::pllRefSel |
| uint32_t usb_init_param_t::usb2Enable |
| uint32_t usb_init_param_t::invertPolarity |
| uint32_t usb_init_param_t::vbusSel |
| uint32_t usb_init_param_t::isHostMode |