AM261x MCU+ SDK  26.00.00
FlashBankCopy_t Struct Reference

Detailed Description

This is active bank to dormant bank copy request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices.

Parameters
cpuFlashBankTypeC29 CPU1, C29 CPU3 or HSM CPU image that is to be copied to dormant bank from current active bank

Data Fields

uint8_t cpuFlashBankType
 

Field Documentation

◆ cpuFlashBankType

uint8_t FlashBankCopy_t::cpuFlashBankType