AM261x MCU+ SDK  26.00.00

Introduction

See HSM client for more details.

Data Structures

union  HsmVer_t
 type for reading HSMRt version. More...
 
struct  HsmClient_t
 This is a HSMClient type which holds the information needed by hsm client to communicate with HSM . More...
 
struct  NvmOtpRead_t
 This is an NvmOtpRead type which holds the information of NvmOtp row index and row data corresponding to it . For F29H85x, the rowdIdx corresponds to the Flash Offsets. For AM26x, the rowIdx corresponds to efuse row offsets. More...
 
struct  NvmOtpRowWrite_t
 This is an NvmOtpRowWrite type which holds the information regarding programming NvmOtp row. For F29H85x, the rowdIdx corresponds to the Flash Offsets. For AM26x, the rowIdx corresponds to efuse row offsets. More...
 
struct  NvmOtpRowCount_t
 This is an NvmOtpRowCount type which holds the information regarding NvmOtp row count and size of each row in bits. More...
 
struct  NvmOtpRowProt_t
 This is a NvmOtpRowProt type which holds the information of NvmOtp row index and protection status corresponding to the row index. This structure is not valid for f29h85x. More...
 
struct  KeyWriterCertHeader_t
 This is a keywriter_cert_header type which holds the information of customer key certificate and debug responce. More...
 
struct  FirewallRegionReq_t
 This is a FirewallRegionReq type which holds the information of Firewall region configuration. More...
 
struct  FirewallReq_t
 This is a FirewallReq_t type which holds the information of Firewall configuration. More...
 
struct  FirewallIntrReq_t
 This is a FirewallIntrReq type which holds the information of MPU Firewall request for interrupt enable, interrupt enable clear, interrupt enable status clear and fault clear. More...
 
struct  SWRev_t
 This is SWRev type which holds the information regarding Revision identifier and value corresponding to it . More...
 
struct  DKEK_t
 This is DKEK type which holds the label and context for derivation. This also holds the 256 derived KEK value which is returned by TIFS. More...
 
struct  RNGReq_t
 This is RNG type which holds the resultPtr for derivation which is returned by TIFS. This also holds the resultLength and DRBG Mode along with seedValue and seedSize. More...
 
struct  SecureBoot_Stream_t_
 This is the SecureBoot Stream type which holds the data for a specific bootloader to HSM call. This packet is needed by HSM the to do the required operation. More...
 
struct  FirmwareUpdateReq_t
 This is Firmware Update request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. More...
 
struct  OTFA_Region_t
 This is the OTFA Region structure which holds individual region specific information to be written to corresponding OTFA registers. In AM263Px and AM261x, there are 4 OTFA regions. More...
 
struct  OTFA_readRegion_t
 This is the OTFA Region structure which holds individual region specific information to be read from OTFA registers. More...
 
struct  OTFA_Config_t
 This is the entire OTFA structure which holds all regions' information 4 regions in AM263Px and AM261x. More...
 
struct  SecCfgValidate_t
 This is Sec-Cfg validation request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices. More...
 
struct  FlashBankCopy_t
 This is active bank to dormant bank copy request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices. More...
 
struct  CryptoServiceReq_t
 Outer request struct for HSM_MSG_CRYPTO_SERVICE. Note: These services are only available in HSSE mode. More...
 
struct  CMACArgs_t
 Args for CMAC generate and verify Note: These services are only available in HSSE mode. More...
 
struct  HMACArgs_t
 Args for HMAC generate and verify Note: These services are only available in HSSE mode. More...
 
struct  GMACArgs_t
 Args for GMAC generate and verify Note: These services are only available in HSSE mode. More...
 
struct  BankSwapReq_t
 This is bank swap request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. Valid only for F29x family of devices. More...
 
struct  DeviceConfigSafety_t
 
struct  DeviceConfigSecurity_t
 Security configuration structure containing security-related device information. More...
 
struct  DeviceConfigDebug_t
 Debug status structure containing debug access information. Total size: SIZE_OF_DEBUG_DEVICE_CONFIG (16 bytes) More...
 
struct  DeviceConfigRead_t
 This is device configuration read request structure passed to HSM core via SIPC as argument, these parameters are required by the service handler. More...
 
struct  HsmMsg_t_
 HSM client / server message format struct. More...
 

Functions

union HsmVer_t_ __attribute__ ((packed)) HsmVer_t
 type for reading HSMRt version. More...
 
int32_t HsmClient_checkAndWaitForBootNotification (void)
 This API waits for HSMRT load if requested and then waits for boot notification. In case of failure in HSMRT load it returns SystemP_FAILURE. More...
 
int32_t HsmClient_init (SIPC_Params *params)
 Initialize the HSM client for current core. More...
 
void HsmClient_deInit (void)
 De initialize the HSM client for current core. More...
 
void HsmClient_SecureBootQueueInit (uint32_t configured_hsm_client_msg_queue_size)
 Customize the size of the HSM client message queue. More...
 
int32_t HsmClient_getVersion (HsmClient_t *HsmClient, HsmVer_t *verId, uint32_t timeToWaitInTick)
 populates the current HSMRT version Id by default the hsm flag is set to HSM_FLAG_AOP for this service More...
 
int32_t HsmClient_getUID (HsmClient_t *HsmClient, uint8_t *uid, uint32_t timeout)
 The service issued to HSM Server populates the Device UID by default the hsm flag is set to HSM_FLAG_AOP for this service. More...
 
int32_t HsmClient_openDbgFirewall (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and by default the hsm flag is set to HSM_FLAG_AOP for this service. More...
 
int32_t HsmClient_importKeyring (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and imports the keys from the certificate. More...
 
int32_t HsmClient_readOTPRow (HsmClient_t *HsmClient, NvmOtpRead_t *readRow)
 The service issued to HSM Server retrieves the data of GP OTP row based on row index provided as param. More...
 
int32_t HsmClient_writeOTPRow (HsmClient_t *HsmClient, NvmOtpRowWrite_t *writeRow)
 The service issued to HSM Server writes the data to extended OTP efuse row based on row index provided as param. More...
 
int32_t HsmClient_lockOTPRow (HsmClient_t *HsmClient, NvmOtpRowProt_t *rowProt)
 The service issued to HSM Server sets the protection status bit of the specified row to 1. This API is not valid for F29H85x. More...
 
int32_t HsmClient_getOTPRowCount (HsmClient_t *HsmClient, NvmOtpRowCount_t *rowCount)
 The service issued to HSM Server retrieves the count of extended OTP rows. More...
 
int32_t HsmClient_getOTPRowProtection (HsmClient_t *HsmClient, NvmOtpRowProt_t *rowProt)
 The service issued to HSM Server retrieves the extended otp efuse row protection status. This API is not valid for F29H85x. More...
 
int32_t HsmClient_procAuthBoot (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 The service issued to HSM Server helps with extended secure boot for applications. More...
 
int32_t HsmClient_procAuthBootStart (HsmClient_t *HsmClient, SecureBoot_Stream_t *secureBootInfo)
 The service issued to HSM Server helps with extended secure boot for applications. More...
 
int32_t HsmClient_procAuthBootUpdate (HsmClient_t *HsmClient, SecureBoot_Stream_t *secureBootInfo)
 The service issued to HSM Server helps with extended secure boot for applications. More...
 
int32_t HsmClient_procAuthBootFinish (HsmClient_t *HsmClient, SecureBoot_Stream_t *secureBootInfo)
 The service issued to HSM Server helps with extended secure boot for applications. More...
 
int32_t HsmClient_setFirewall (HsmClient_t *HsmClient, FirewallReq_t *FirewallReqObj, uint32_t timeout)
 The service issued to HSM Server sets the firewall for the given firewall id and region. More...
 
int32_t HsmClient_FirewallIntr (HsmClient_t *HsmClient, FirewallIntrReq_t *FirewallIntrReqObj, uint32_t timeout)
 The service issued to HSM Server sets the firewall interrupt request for the given firewall id. More...
 
int32_t HsmClient_keyWriter (HsmClient_t *HsmClient, KeyWriterCertHeader_t *certHeader, uint32_t timeout)
 The service issued to HSM Server verifies the certificate and process the keywriter operations,. More...
 
int32_t HsmClient_readSWRev (HsmClient_t *HsmClient, SWRev_t *readSWRev)
 The service issued to HSM Server retrieves the SWRevision value based on identifier as param. More...
 
int32_t HsmClient_writeSWRev (HsmClient_t *HsmClient, SWRev_t *writeSWRev)
 The service issued to HSM Server writes the SWRevision value based on identifier as param. More...
 
int32_t HsmClient_getDKEK (HsmClient_t *HsmClient, DKEK_t *getDKEK, uint32_t timeout)
 The service issued to HSM Server retrieves the derived KEK based on identifier as param. More...
 
int32_t HsmClient_register (HsmClient_t *HsmClient, uint8_t clientId)
 register a client to a particular ClientId More...
 
void HsmClient_unregister (HsmClient_t *HsmClient, uint8_t clientId)
 unregister a client to a particular ClientId More...
 
int32_t HsmClient_waitForBootNotify (HsmClient_t *HsmClient, uint32_t timeToWaitInTicks)
 Current core will wait for bootnotify message from HSM core. More...
 
int32_t Hsmclient_loadHSMRtFirmware (HsmClient_t *gHSMClient, const uint8_t *pHSMRt_firmware)
 Loads the HSMRt firmware. This is typically called by SBL. More...
 
int32_t Hsmclient_loadHSMRtFirmwareNonBlocking (const uint8_t *pHSMRt_firmware)
 Loads the HSMRt firmware but does wait for ROM response and boot notification. This is typically called by SBL. More...
 
int32_t HsmClient_getRandomNum (HsmClient_t *HsmClient, RNGReq_t *getRandomNum)
 Returns the Random Number Generated. More...
 
int32_t HsmClient_firmwareUpdate_CertProcess (HsmClient_t *HsmClient, FirmwareUpdateReq_t *pFirmwareUpdateObject)
 service request issued to HSM server to parse the certificate to validate authenticity and identify the firmware component undergoing update This service is valid only for F29H85x SOC More...
 
int32_t HsmClient_firmwareUpdate_CodeProgram (HsmClient_t *HsmClient, FirmwareUpdateReq_t *pFirmwareUpdateObject)
 service request issued to HSM server to program the incoming firmware to device dormant banks This service is valid only for F29H85x SOC More...
 
int32_t HsmClient_firmwareUpdate_CodeVerify (HsmClient_t *HsmClient, FirmwareUpdateReq_t *pFirmwareUpdateObject)
 service request issued to HSM server to decrypt the firmware programmed in dormant flash bank in place, perform integrity checks on the decrypted firmware and program the certificate in flash memory This service is valid only for F29H85x SOC More...
 
int32_t HsmClient_VerifyROTSwitchingCertificate (HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
 service request issued to HSM server to validate RoT Switching Certificate More...
 
int32_t HsmClient_UpdateKeyRevsion (HsmClient_t *HsmClient, uint32_t timeout)
 service request issued to HSM server to update key revision to 0x2 which changes the root of trust key from secondary keys to back up keys. More...
 
int32_t HsmClient_configOTFARegions (HsmClient_t *HsmClient, OTFA_Config_t *OTFA_ConfigInfo, uint32_t timeout)
 Client request to configure the OTFA regions. More...
 
int32_t HsmClient_readOTFARegions (HsmClient_t *HsmClient, OTFA_readRegion_t *OTFA_readRegion, uint32_t timeout)
 Client request to read the OTFA regions. More...
 
int32_t HsmClient_secCfgValidate (HsmClient_t *HsmClient, SecCfgValidate_t *pSecCfgParams, uint32_t timeout)
 Client request to validate sec-cfg Valid only for F29x family of devices. More...
 
int32_t HsmClient_activeToDormantBankCopy (HsmClient_t *HsmClient, FlashBankCopy_t *pFlashBankCopyObject, uint32_t timeout)
 Client request to copy active flash bank contents to dormant flash bank Valid only for F29x family of devices. More...
 
int32_t HsmClient_SecCfgUpdate (HsmClient_t *HsmClient, FirmwareUpdateReq_t *pFirmwareUpdateObject)
 Client request to update device Sec-Cfg Valid only for F29x family of devices. More...
 
int32_t HsmClient_getDeviceConfig (HsmClient_t *HsmClient, DeviceConfigRead_t *pDeviceConfigObject, uint32_t timeout)
 Client request to get device configuration from HSM This is a blocking call that waits for HSM response. More...
 
int32_t HsmClient_CryptoService (HsmClient_t *HsmClient, CryptoServiceReq_t *svcReq, uint32_t timeout)
 Submit a generic crypto service request to the HSM. Set svcReq->algoId to the algorithm (HSM_CRYPTO_SVC_MAC_CMAC, etc.) and svcReq->subSvcId to the operation (HSM_CRYPTO_SVC_MAC_GENERATE, etc.). Set svcReq->keyId to the keyring index and point svcReq->ptrArgs at the corresponding args struct (e.g. CMACArgs_t). More...
 
int32_t HsmClient_runTimeBankSwap (HsmClient_t *HsmClient, BankSwapReq_t *pBankSwapObject)
 Client request to Swap C29 CPU flash banks Valid only for F29x family of devices. More...
 

Enumerations

enum  HSM_ClientIds_t {
  HSM_BOOT_NOTIFY_CLIENT_ID = 0, HSM_CLIENT_ID_1, HSM_CLIENT_ID_2, HSM_CLIENT_ID_3,
  HSM_CLIENT_ID_4
}
 

Macros

#define LABEL_AND_CONTEXT_LEN_MAX   48U
 
#define HSMRT_LOAD_NOT_REQUESTED   (0U)
 HSMRT load has not been requested. More...
 
#define HSMRT_LOAD_REQUESTED   (1U)
 HSMRT load has been requested. More...
 
#define HSMRT_LOAD_FAILED   (2U)
 HSMRT load has failed. More...
 
#define HSMRT_LOAD_SUCCEEDED   (3U)
 HSMRT load has succeeded. More...
 
#define HSM_CRYPTO_SVC_MAC_CMAC   (0x0001U)
 Algorithm: AES-CMAC. More...
 
#define HSM_CRYPTO_SVC_MAC_HMAC   (0x0002U)
 Algorithm: HMAC. More...
 
#define HSM_CRYPTO_SVC_MAC_GMAC   (0x0003U)
 Algorithm: GMAC. More...
 
#define HSM_CRYPTO_HMAC_SHA256   (0x6U) /* matches DTHE_SHA_ALGO_SHA256 */
 HMAC with SHA-256 (32-byte tag) More...
 
#define HSM_CRYPTO_HMAC_SHA512   (0x4U) /* matches DTHE_SHA_ALGO_SHA512 */
 HMAC with SHA-512 (64-byte tag) More...
 
#define HSM_CRYPTO_SVC_MAC_GENERATE   (0x0001U)
 MAC: compute tag and write to ptrTag (used for CMAC, HMAC, GMAC) More...
 
#define HSM_CRYPTO_SVC_MAC_VERIFY   (0x0002U)
 MAC: compute tag and compare against ptrTag (used for CMAC, HMAC, GMAC) More...
 
#define DEVICE_CONFIG_TYPE_SAFETY   (0U)
 Safety configuration (dedFotaInfo, hsmPbistStatus) More...
 
#define DEVICE_CONFIG_TYPE_SECURITY   (1U)
 Security configuration (SecCfg validation, SW revisions, boot retry counts) More...
 
#define DEVICE_CONFIG_TYPE_DEBUG   (2U)
 Debug configuration (TBD) More...
 
#define DEVICE_CONFIG_TYPE_ALL   (0xFFU)
 All configuration types. More...
 
#define SIZE_OF_SAFETY_DEVICE_CONFIG   (8U)
 Size of Safety configuration data in bytes (2 uint32_t values) More...
 
#define SIZE_OF_SECURITY_DEVICE_CONFIG   (44U)
 Size of security configuration data in bytes (11 uint32_t values) More...
 
#define SIZE_OF_DEBUG_DEVICE_CONFIG   (16U)
 Size of Debug configuration data in bytes (4 uint32_t values) More...
 
#define HSM_MSG_GET_VERSION   (0x0002)
 GetVersion service type ID. More...
 
#define HSM_MSG_BOOT_NOTIFY   (0x000A)
 Boot Notify service type ID. More...
 
#define HSM_MSG_GET_DEVICE_CONFIG   (0x000B)
 Get device configuration from HSM. More...
 
#define HSM_MSG_GET_UID   (0x9021)
 Get UID service type ID. More...
 
#define HSM_MSG_OPEN_DBG_FIREWALLS   (0x900C)
 Open Debug Firewalls service type ID. More...
 
#define HSM_MSG_READ_OTP_ROW   (0x9022)
 Read Extended otp row type ID. More...
 
#define HSM_MSG_WRITE_OTP_ROW   (0x9023)
 Write Extended otp row type ID. More...
 
#define HSM_MSG_PROT_OTP_ROW   (0x9024)
 Protect Extended otp row type ID. More...
 
#define HSM_MSG_GET_OTP_ROW_PROT   (0x9026)
 Get Extended otp row protection type ID. More...
 
#define HSM_MSG_GET_OTP_ROW_COUNT   (0x9027)
 Get Extended otp row count service type ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT   (0xC120)
 Secure Boot service type ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT_START   (0xC12A)
 Secure Boot Streaming Start service type ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT_UPDATE   (0xC12B)
 Secure Boot Streaming Update service type ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT_FINISH   (0xC12C)
 Secure Boot Streaming Finish service type ID. More...
 
#define HSM_MSG_SET_FIREWALL   (0x9000U)
 Set Firewall service type ID. More...
 
#define HSM_MSG_SET_FIREWALL_INTR   (0x9002)
 Set Firewall Interrupt service type ID. More...
 
#define HSM_KEYWRITER_SEND_CUST_KEY_CERT   (0x9028)
 send KeyWriter customer key certificate More...
 
#define HSM_MSG_READ_SWREV   (0x9033)
 Read Software Revision service type ID. More...
 
#define HSM_MSG_WRITE_SWREV   (0x9032)
 Write Software Revision service type ID. More...
 
#define HSM_MSG_GET_DKEK   (0x9029)
 Get DKEK service type ID. More...
 
#define HSM_MSG_GET_RAND   (0x9001)
 Get RNG service type ID. More...
 
#define HSM_MSG_KEYRING_IMPORT   (0x9039)
 Get KEYRING import service type ID. More...
 
#define HSM_MSG_FW_UPDATE_CERT_PROCESS   (0x9040)
 Process certificate during firmware update/code provisioning. More...
 
#define HSM_MSG_FW_UPDATE_CODE_PROGRAM   (0x9041)
 Program firmware during firmware update/code provisioning. More...
 
#define HSM_MSG_FW_UPDATE_CODE_VERIFY   (0x9043)
 Program firmware during firmware update/code provisioning. More...
 
#define HSM_MSG_VERIFY_ROT_CERT   (0x9044)
 Veriy RoT Switching Certificate Service type ID. More...
 
#define HSM_MSG_UPDATE_KEY_REV   (0x9045)
 Update Key Revision Service type ID. More...
 
#define HSM_MSG_CONFIGURE_OTFA   (0x9056)
 Configure OTFA service ID. More...
 
#define HSM_MSG_READ_OTFA   (0x9057)
 Read OTFA service ID. More...
 
#define HSM_MSG_PROC_AUTH_BOOT_SEC_CFG   (0x9058)
 Validate Sec-Cfg service ID. More...
 
#define HSM_MSG_FLASH_BANK_COPY   (0x9059)
 Copy active flash bank contents to dormant flash bank. More...
 
#define HSM_MSG_FW_UPDATE_SECCFG   (0x905AU)
 Program Sec-Cfg to SOC non main flash. More...
 
#define HSM_MSG_BANK_SWAP   (0x905BU)
 Swap C29 CPU-1/3 flash banks. More...
 
#define HSM_MSG_CRYPTO_SERVICE   (0xA001U)
 Generic Crypto service ID. More...
 
#define HSM_FLAG_AOP   (0x11)
 HSM FLAG used by HSM client to indicate that it expects ACK messasge from HSM and will wait for a response message. More...
 
#define HSM_FLAG_NAOP   (0x22)
 HSM FLAG used by HSM client to indicate that it does not expects an ACK messasge from HSM and will not wait for a response message. More...
 
#define HSM_FLAG_ACK   (0xAA)
 HSM FLAG used by HSM server to indicate that the request has been processed. More...
 
#define HSM_FLAG_NACK   (0x55)
 HSM FLAG used by HSM server to indicate that the request has not been processed. More...
 
#define HSM_CLIENT_ID   (0x01)
 HSM server SIPC client Id. More...
 
#define HSM_UID_SIZE   (64U)
 UID or Unique ID is a device specific ID of 64 bytes. More...
 
#define HSM_DBG_CERT_SIZE   (4096U)
 Maximum Certificate Size allowed for Debug Open. More...
 
#define HSM_KEYRING_CERT_SIZE   (10280U)
 Maximum Certificate Size allowed for Keyring Import. More...
 
#define HSM_FIRMWARE_CHUNK_SIZE   (16384U)
 Maximum firmware Size allowed for code provisioning. More...
 
#define CERT_TYPE_SECCFG_CPU1   (0x3U)
 Certificate type for C29 CPU1 Sec-cfg. More...
 
#define CERT_TYPE_SECCFG_CPU2   (0x5U)
 Certificate type for C29 CPU2 Sec-cfg. More...
 
#define CERT_TYPE_SECCFG_CPU3   (0x6U)
 Certificate type for C29 CPU3 Sec-cfg. More...
 
#define C29_CPU1_FLASH_BANK   (0x1U)
 C29 CPU1 macro to be used while requesting active to dormant flash bank copy or C29 CPU flash bank swap services. Valid only for F29x family of devices. More...
 
#define C29_CPU3_FLASH_BANK   (0x3U)
 C29 CPU3 macro to be used while requesting active to dormant flash bank copy or C29 CPU flash bank swap services. Valid only for F29x family of devices. More...
 
#define HSM_CPU_FLASH_BANK   (0x0U)
 HSM CPU macro to be used while requesting active to dormant flash bank copy Valid only for F29x family of devices. More...
 
#define LFU_BANK_SWAP_READY   (0x5AU)
 MACRO used by HSM for LFU synchronizsation. More...
 

Macro Definition Documentation

◆ LABEL_AND_CONTEXT_LEN_MAX

#define LABEL_AND_CONTEXT_LEN_MAX   48U

◆ HSMRT_LOAD_NOT_REQUESTED

#define HSMRT_LOAD_NOT_REQUESTED   (0U)

HSMRT load has not been requested.

◆ HSMRT_LOAD_REQUESTED

#define HSMRT_LOAD_REQUESTED   (1U)

HSMRT load has been requested.

◆ HSMRT_LOAD_FAILED

#define HSMRT_LOAD_FAILED   (2U)

HSMRT load has failed.

◆ HSMRT_LOAD_SUCCEEDED

#define HSMRT_LOAD_SUCCEEDED   (3U)

HSMRT load has succeeded.

◆ HSM_CRYPTO_SVC_MAC_CMAC

#define HSM_CRYPTO_SVC_MAC_CMAC   (0x0001U)

Algorithm: AES-CMAC.

◆ HSM_CRYPTO_SVC_MAC_HMAC

#define HSM_CRYPTO_SVC_MAC_HMAC   (0x0002U)

Algorithm: HMAC.

◆ HSM_CRYPTO_SVC_MAC_GMAC

#define HSM_CRYPTO_SVC_MAC_GMAC   (0x0003U)

Algorithm: GMAC.

◆ HSM_CRYPTO_HMAC_SHA256

#define HSM_CRYPTO_HMAC_SHA256   (0x6U) /* matches DTHE_SHA_ALGO_SHA256 */

HMAC with SHA-256 (32-byte tag)

◆ HSM_CRYPTO_HMAC_SHA512

#define HSM_CRYPTO_HMAC_SHA512   (0x4U) /* matches DTHE_SHA_ALGO_SHA512 */

HMAC with SHA-512 (64-byte tag)

◆ HSM_CRYPTO_SVC_MAC_GENERATE

#define HSM_CRYPTO_SVC_MAC_GENERATE   (0x0001U)

MAC: compute tag and write to ptrTag (used for CMAC, HMAC, GMAC)

◆ HSM_CRYPTO_SVC_MAC_VERIFY

#define HSM_CRYPTO_SVC_MAC_VERIFY   (0x0002U)

MAC: compute tag and compare against ptrTag (used for CMAC, HMAC, GMAC)

◆ DEVICE_CONFIG_TYPE_SAFETY

#define DEVICE_CONFIG_TYPE_SAFETY   (0U)

Safety configuration (dedFotaInfo, hsmPbistStatus)

◆ DEVICE_CONFIG_TYPE_SECURITY

#define DEVICE_CONFIG_TYPE_SECURITY   (1U)

Security configuration (SecCfg validation, SW revisions, boot retry counts)

◆ DEVICE_CONFIG_TYPE_DEBUG

#define DEVICE_CONFIG_TYPE_DEBUG   (2U)

Debug configuration (TBD)

◆ DEVICE_CONFIG_TYPE_ALL

#define DEVICE_CONFIG_TYPE_ALL   (0xFFU)

All configuration types.

◆ SIZE_OF_SAFETY_DEVICE_CONFIG

#define SIZE_OF_SAFETY_DEVICE_CONFIG   (8U)

Size of Safety configuration data in bytes (2 uint32_t values)

◆ SIZE_OF_SECURITY_DEVICE_CONFIG

#define SIZE_OF_SECURITY_DEVICE_CONFIG   (44U)

Size of security configuration data in bytes (11 uint32_t values)

◆ SIZE_OF_DEBUG_DEVICE_CONFIG

#define SIZE_OF_DEBUG_DEVICE_CONFIG   (16U)

Size of Debug configuration data in bytes (4 uint32_t values)

◆ HSM_MSG_GET_VERSION

#define HSM_MSG_GET_VERSION   (0x0002)

GetVersion service type ID.

◆ HSM_MSG_BOOT_NOTIFY

#define HSM_MSG_BOOT_NOTIFY   (0x000A)

Boot Notify service type ID.

◆ HSM_MSG_GET_DEVICE_CONFIG

#define HSM_MSG_GET_DEVICE_CONFIG   (0x000B)

Get device configuration from HSM.

◆ HSM_MSG_GET_UID

#define HSM_MSG_GET_UID   (0x9021)

Get UID service type ID.

◆ HSM_MSG_OPEN_DBG_FIREWALLS

#define HSM_MSG_OPEN_DBG_FIREWALLS   (0x900C)

Open Debug Firewalls service type ID.

◆ HSM_MSG_READ_OTP_ROW

#define HSM_MSG_READ_OTP_ROW   (0x9022)

Read Extended otp row type ID.

◆ HSM_MSG_WRITE_OTP_ROW

#define HSM_MSG_WRITE_OTP_ROW   (0x9023)

Write Extended otp row type ID.

◆ HSM_MSG_PROT_OTP_ROW

#define HSM_MSG_PROT_OTP_ROW   (0x9024)

Protect Extended otp row type ID.

◆ HSM_MSG_GET_OTP_ROW_PROT

#define HSM_MSG_GET_OTP_ROW_PROT   (0x9026)

Get Extended otp row protection type ID.

◆ HSM_MSG_GET_OTP_ROW_COUNT

#define HSM_MSG_GET_OTP_ROW_COUNT   (0x9027)

Get Extended otp row count service type ID.

◆ HSM_MSG_PROC_AUTH_BOOT

#define HSM_MSG_PROC_AUTH_BOOT   (0xC120)

Secure Boot service type ID.

◆ HSM_MSG_PROC_AUTH_BOOT_START

#define HSM_MSG_PROC_AUTH_BOOT_START   (0xC12A)

Secure Boot Streaming Start service type ID.

◆ HSM_MSG_PROC_AUTH_BOOT_UPDATE

#define HSM_MSG_PROC_AUTH_BOOT_UPDATE   (0xC12B)

Secure Boot Streaming Update service type ID.

◆ HSM_MSG_PROC_AUTH_BOOT_FINISH

#define HSM_MSG_PROC_AUTH_BOOT_FINISH   (0xC12C)

Secure Boot Streaming Finish service type ID.

◆ HSM_MSG_SET_FIREWALL

#define HSM_MSG_SET_FIREWALL   (0x9000U)

Set Firewall service type ID.

◆ HSM_MSG_SET_FIREWALL_INTR

#define HSM_MSG_SET_FIREWALL_INTR   (0x9002)

Set Firewall Interrupt service type ID.

◆ HSM_KEYWRITER_SEND_CUST_KEY_CERT

#define HSM_KEYWRITER_SEND_CUST_KEY_CERT   (0x9028)

send KeyWriter customer key certificate

◆ HSM_MSG_READ_SWREV

#define HSM_MSG_READ_SWREV   (0x9033)

Read Software Revision service type ID.

◆ HSM_MSG_WRITE_SWREV

#define HSM_MSG_WRITE_SWREV   (0x9032)

Write Software Revision service type ID.

◆ HSM_MSG_GET_DKEK

#define HSM_MSG_GET_DKEK   (0x9029)

Get DKEK service type ID.

◆ HSM_MSG_GET_RAND

#define HSM_MSG_GET_RAND   (0x9001)

Get RNG service type ID.

◆ HSM_MSG_KEYRING_IMPORT

#define HSM_MSG_KEYRING_IMPORT   (0x9039)

Get KEYRING import service type ID.

◆ HSM_MSG_FW_UPDATE_CERT_PROCESS

#define HSM_MSG_FW_UPDATE_CERT_PROCESS   (0x9040)

Process certificate during firmware update/code provisioning.

◆ HSM_MSG_FW_UPDATE_CODE_PROGRAM

#define HSM_MSG_FW_UPDATE_CODE_PROGRAM   (0x9041)

Program firmware during firmware update/code provisioning.

◆ HSM_MSG_FW_UPDATE_CODE_VERIFY

#define HSM_MSG_FW_UPDATE_CODE_VERIFY   (0x9043)

Program firmware during firmware update/code provisioning.

◆ HSM_MSG_VERIFY_ROT_CERT

#define HSM_MSG_VERIFY_ROT_CERT   (0x9044)

Veriy RoT Switching Certificate Service type ID.

◆ HSM_MSG_UPDATE_KEY_REV

#define HSM_MSG_UPDATE_KEY_REV   (0x9045)

Update Key Revision Service type ID.

◆ HSM_MSG_CONFIGURE_OTFA

#define HSM_MSG_CONFIGURE_OTFA   (0x9056)

Configure OTFA service ID.

◆ HSM_MSG_READ_OTFA

#define HSM_MSG_READ_OTFA   (0x9057)

Read OTFA service ID.

◆ HSM_MSG_PROC_AUTH_BOOT_SEC_CFG

#define HSM_MSG_PROC_AUTH_BOOT_SEC_CFG   (0x9058)

Validate Sec-Cfg service ID.

◆ HSM_MSG_FLASH_BANK_COPY

#define HSM_MSG_FLASH_BANK_COPY   (0x9059)

Copy active flash bank contents to dormant flash bank.

◆ HSM_MSG_FW_UPDATE_SECCFG

#define HSM_MSG_FW_UPDATE_SECCFG   (0x905AU)

Program Sec-Cfg to SOC non main flash.

◆ HSM_MSG_BANK_SWAP

#define HSM_MSG_BANK_SWAP   (0x905BU)

Swap C29 CPU-1/3 flash banks.

◆ HSM_MSG_CRYPTO_SERVICE

#define HSM_MSG_CRYPTO_SERVICE   (0xA001U)

Generic Crypto service ID.

◆ HSM_FLAG_AOP

#define HSM_FLAG_AOP   (0x11)

HSM FLAG used by HSM client to indicate that it expects ACK messasge from HSM and will wait for a response message.

◆ HSM_FLAG_NAOP

#define HSM_FLAG_NAOP   (0x22)

HSM FLAG used by HSM client to indicate that it does not expects an ACK messasge from HSM and will not wait for a response message.

◆ HSM_FLAG_ACK

#define HSM_FLAG_ACK   (0xAA)

HSM FLAG used by HSM server to indicate that the request has been processed.

◆ HSM_FLAG_NACK

#define HSM_FLAG_NACK   (0x55)

HSM FLAG used by HSM server to indicate that the request has not been processed.

◆ HSM_CLIENT_ID

#define HSM_CLIENT_ID   (0x01)

HSM server SIPC client Id.

◆ HSM_UID_SIZE

#define HSM_UID_SIZE   (64U)

UID or Unique ID is a device specific ID of 64 bytes.

◆ HSM_DBG_CERT_SIZE

#define HSM_DBG_CERT_SIZE   (4096U)

Maximum Certificate Size allowed for Debug Open.

◆ HSM_KEYRING_CERT_SIZE

#define HSM_KEYRING_CERT_SIZE   (10280U)

Maximum Certificate Size allowed for Keyring Import.

◆ HSM_FIRMWARE_CHUNK_SIZE

#define HSM_FIRMWARE_CHUNK_SIZE   (16384U)

Maximum firmware Size allowed for code provisioning.

◆ CERT_TYPE_SECCFG_CPU1

#define CERT_TYPE_SECCFG_CPU1   (0x3U)

Certificate type for C29 CPU1 Sec-cfg.

◆ CERT_TYPE_SECCFG_CPU2

#define CERT_TYPE_SECCFG_CPU2   (0x5U)

Certificate type for C29 CPU2 Sec-cfg.

◆ CERT_TYPE_SECCFG_CPU3

#define CERT_TYPE_SECCFG_CPU3   (0x6U)

Certificate type for C29 CPU3 Sec-cfg.

◆ C29_CPU1_FLASH_BANK

#define C29_CPU1_FLASH_BANK   (0x1U)

C29 CPU1 macro to be used while requesting active to dormant flash bank copy or C29 CPU flash bank swap services. Valid only for F29x family of devices.

◆ C29_CPU3_FLASH_BANK

#define C29_CPU3_FLASH_BANK   (0x3U)

C29 CPU3 macro to be used while requesting active to dormant flash bank copy or C29 CPU flash bank swap services. Valid only for F29x family of devices.

◆ HSM_CPU_FLASH_BANK

#define HSM_CPU_FLASH_BANK   (0x0U)

HSM CPU macro to be used while requesting active to dormant flash bank copy Valid only for F29x family of devices.

◆ LFU_BANK_SWAP_READY

#define LFU_BANK_SWAP_READY   (0x5AU)

MACRO used by HSM for LFU synchronizsation.

Enumeration Type Documentation

◆ HSM_ClientIds_t

Enumerator
HSM_BOOT_NOTIFY_CLIENT_ID 
HSM_CLIENT_ID_1 
HSM_CLIENT_ID_2 
HSM_CLIENT_ID_3 
HSM_CLIENT_ID_4 

Function Documentation

◆ __attribute__()

union HsmVer_t_ __attribute__ ( (packed)  )

type for reading HSMRt version.

HSM client / server message format struct.

This is the SecureBoot Stream type which holds the data for a specific bootloader to HSM call. This packet is needed by HSM the to do the required operation.

◆ HsmClient_checkAndWaitForBootNotification()

int32_t HsmClient_checkAndWaitForBootNotification ( void  )

This API waits for HSMRT load if requested and then waits for boot notification. In case of failure in HSMRT load it returns SystemP_FAILURE.

Returns
  1. SystemP_SUCCESS if HSMRT load is successful.
  2. SystemP_FAILURE if HSMRT load fails.

◆ HsmClient_init()

int32_t HsmClient_init ( SIPC_Params *  params)

Initialize the HSM client for current core.

Parameters
params[IN] SIPC_notify params.
Returns
  1. SystemP_SUCCESS if init sequence successful.
  2. SystemP_FAILURE if init sequence fails.

◆ HsmClient_deInit()

void HsmClient_deInit ( void  )

De initialize the HSM client for current core.

◆ HsmClient_SecureBootQueueInit()

void HsmClient_SecureBootQueueInit ( uint32_t  configured_hsm_client_msg_queue_size)

Customize the size of the HSM client message queue.

Parameters
configured_hsm_client_msg_queue_sizeDesired size of the HSM client message queue passed by the user.

◆ HsmClient_getVersion()

int32_t HsmClient_getVersion ( HsmClient_t *  HsmClient,
HsmVer_t *  verId,
uint32_t  timeToWaitInTick 
)

populates the current HSMRT version Id by default the hsm flag is set to HSM_FLAG_AOP for this service

Parameters
timeToWaitInTick[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this getversion API.
verId[OUT] populates HsmVer_t struct which describes current version. This object's memory address needs to be cache aligned.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_getUID()

int32_t HsmClient_getUID ( HsmClient_t *  HsmClient,
uint8_t *  uid,
uint32_t  timeout 
)

The service issued to HSM Server populates the Device UID by default the hsm flag is set to HSM_FLAG_AOP for this service.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this getUID API.
uid[OUT] populates UID value.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_openDbgFirewall()

int32_t HsmClient_openDbgFirewall ( HsmClient_t *  HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and by default the hsm flag is set to HSM_FLAG_AOP for this service.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this openDbgFirewalls API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_importKeyring()

int32_t HsmClient_importKeyring ( HsmClient_t *  HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and imports the keys from the certificate.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this importKeyring API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_readOTPRow()

int32_t HsmClient_readOTPRow ( HsmClient_t *  HsmClient,
NvmOtpRead_t *  readRow 
)

The service issued to HSM Server retrieves the data of GP OTP row based on row index provided as param.

Parameters
HsmClient[IN] HsmClient object.
readRow[IN] populates NvmOtpRead_t struct with rowData corresponding to rowIdx.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_writeOTPRow()

int32_t HsmClient_writeOTPRow ( HsmClient_t *  HsmClient,
NvmOtpRowWrite_t *  writeRow 
)

The service issued to HSM Server writes the data to extended OTP efuse row based on row index provided as param.

Parameters
HsmClient[IN] HsmClient object.
writeRow[IN] populates NvmOtpRowWrite_t struct with rowData corresponding to rowIdx.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_lockOTPRow()

int32_t HsmClient_lockOTPRow ( HsmClient_t *  HsmClient,
NvmOtpRowProt_t *  rowProt 
)

The service issued to HSM Server sets the protection status bit of the specified row to 1. This API is not valid for F29H85x.

Parameters
HsmClient[IN] HsmClient object.
rowProt[IN] Pointer to NvmOtpRowProt_t struct which contains the row index and row protection status
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getOTPRowCount()

int32_t HsmClient_getOTPRowCount ( HsmClient_t *  HsmClient,
NvmOtpRowCount_t *  rowCount 
)

The service issued to HSM Server retrieves the count of extended OTP rows.

Parameters
HsmClient[IN] HsmClient object.
rowCount[IN] Pointer to NvmOtpRowCount_t struct which is populated by HSM server with row count and row size
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getOTPRowProtection()

int32_t HsmClient_getOTPRowProtection ( HsmClient_t *  HsmClient,
NvmOtpRowProt_t *  rowProt 
)

The service issued to HSM Server retrieves the extended otp efuse row protection status. This API is not valid for F29H85x.

Parameters
HsmClient[IN] HsmClient object.
rowProt[IN] Pointer to NvmOtpRowProt_t struct which is populated by HSM server with row protection status
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_procAuthBoot()

int32_t HsmClient_procAuthBoot ( HsmClient_t *  HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

The service issued to HSM Server helps with extended secure boot for applications.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this openDbgFirewalls API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_procAuthBootStart()

int32_t HsmClient_procAuthBootStart ( HsmClient_t *  HsmClient,
SecureBoot_Stream_t *  secureBootInfo 
)

The service issued to HSM Server helps with extended secure boot for applications.

Parameters
HsmClient[IN] Client object which is using this openDbgFirewalls API.
secureBootInfo[IN] pointer to the secure boot information object in shared memory.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_procAuthBootUpdate()

int32_t HsmClient_procAuthBootUpdate ( HsmClient_t *  HsmClient,
SecureBoot_Stream_t *  secureBootInfo 
)

The service issued to HSM Server helps with extended secure boot for applications.

Parameters
HsmClient[IN] Client object which is using this openDbgFirewalls API.
secureBootInfo[IN] pointer to the secure boot information object in shared memory.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_procAuthBootFinish()

int32_t HsmClient_procAuthBootFinish ( HsmClient_t *  HsmClient,
SecureBoot_Stream_t *  secureBootInfo 
)

The service issued to HSM Server helps with extended secure boot for applications.

Parameters
HsmClient[IN] Client object which is using this openDbgFirewalls API.
secureBootInfo[IN] pointer to the secure boot information object in shared memory
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_setFirewall()

int32_t HsmClient_setFirewall ( HsmClient_t *  HsmClient,
FirewallReq_t *  FirewallReqObj,
uint32_t  timeout 
)

The service issued to HSM Server sets the firewall for the given firewall id and region.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
FirewallReqObj[IN] Pointer to FirewallReq_t struct which contains information required for HSM to process set firewall request.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_FirewallIntr()

int32_t HsmClient_FirewallIntr ( HsmClient_t *  HsmClient,
FirewallIntrReq_t *  FirewallIntrReqObj,
uint32_t  timeout 
)

The service issued to HSM Server sets the firewall interrupt request for the given firewall id.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
FirewallIntrReqObj[IN] Pointer to FirewallIntrReq_t struct which contains information required for HSM to process firewall interrupt request.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_keyWriter()

int32_t HsmClient_keyWriter ( HsmClient_t *  HsmClient,
KeyWriterCertHeader_t *  certHeader,
uint32_t  timeout 
)

The service issued to HSM Server verifies the certificate and process the keywriter operations,.

Parameters
HsmClient[IN] Client object which is using this API.
certHeader[IN] point to the location of certificate in the device memory. This object's memory address needs to be cache aligned.
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_readSWRev()

int32_t HsmClient_readSWRev ( HsmClient_t *  HsmClient,
SWRev_t *  readSWRev 
)

The service issued to HSM Server retrieves the SWRevision value based on identifier as param.

Parameters
HsmClient[IN] HsmClient object.
readSWRev[IN] populates SWRev_t struct with SWRev value corresponding to identifier.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_writeSWRev()

int32_t HsmClient_writeSWRev ( HsmClient_t *  HsmClient,
SWRev_t *  writeSWRev 
)

The service issued to HSM Server writes the SWRevision value based on identifier as param.

Parameters
HsmClient[IN] HsmClient object.
writeSWRev[IN] updates the SWRev efuses with SWRev value corresponding to identifier.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getDKEK()

int32_t HsmClient_getDKEK ( HsmClient_t *  HsmClient,
DKEK_t *  getDKEK,
uint32_t  timeout 
)

The service issued to HSM Server retrieves the derived KEK based on identifier as param.

The service issued to HSM Server retrieves the derived KEK.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] HsmClient object.
getDKEK[IN] Pointer to DKEK_t which contains the request structure for Derived KEK.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_register()

int32_t HsmClient_register ( HsmClient_t *  HsmClient,
uint8_t  clientId 
)

register a client to a particular ClientId

Parameters
HsmClient[IN] HsmClient object.
clientId[IN] enable HSM <--> R5 communication for given clientID
Returns
  1. SystemP_SUCCESS if clientId is available
  2. SystemP_FAILURE if clientId is not available or already in use.

◆ HsmClient_unregister()

void HsmClient_unregister ( HsmClient_t *  HsmClient,
uint8_t  clientId 
)

unregister a client to a particular ClientId

Parameters
HsmClient[IN] HsmClient object
clientId[IN] disable HSM <--> R5 communication for given clientId

◆ HsmClient_waitForBootNotify()

int32_t HsmClient_waitForBootNotify ( HsmClient_t *  HsmClient,
uint32_t  timeToWaitInTicks 
)

Current core will wait for bootnotify message from HSM core.

Parameters
HsmClient[IN] HsmClient object
timeToWaitInTicks[IN] amount of time to block waiting for semaphore to be available, in units of SystemP_timeout if timeout exception occours.system ticks (see KERNEL_DPL_CLOCK_PAGE)
Returns
  1. SystemP_SUCCESS -: when BootNotify received
  2. SystemP_FAILURE -: if faulty msg received

◆ Hsmclient_loadHSMRtFirmware()

int32_t Hsmclient_loadHSMRtFirmware ( HsmClient_t *  gHSMClient,
const uint8_t *  pHSMRt_firmware 
)

Loads the HSMRt firmware. This is typically called by SBL.

Parameters
gHSMClient[IN] Pointer to registered HSM Client
pHSMRt_firmware[IN] Pointer to signed HSMRt binary
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

◆ Hsmclient_loadHSMRtFirmwareNonBlocking()

int32_t Hsmclient_loadHSMRtFirmwareNonBlocking ( const uint8_t *  pHSMRt_firmware)

Loads the HSMRt firmware but does wait for ROM response and boot notification. This is typically called by SBL.

Parameters
pHSMRt_firmware[IN] Pointer to signed HSMRt binary
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

◆ HsmClient_getRandomNum()

int32_t HsmClient_getRandomNum ( HsmClient_t *  HsmClient,
RNGReq_t *  getRandomNum 
)

Returns the Random Number Generated.

Parameters
HsmClient[IN] HsmClient object
getRandomNum[IN] Pointer to RNGReq_t which contains the request structure for Random Number Generated.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_firmwareUpdate_CertProcess()

int32_t HsmClient_firmwareUpdate_CertProcess ( HsmClient_t *  HsmClient,
FirmwareUpdateReq_t *  pFirmwareUpdateObject 
)

service request issued to HSM server to parse the certificate to validate authenticity and identify the firmware component undergoing update This service is valid only for F29H85x SOC

Parameters
HsmClient[IN] Client object which is using this API.
pFirmwareUpdateObject[IN] Pointer to arguments to be passed to HSM core via SIPC.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_firmwareUpdate_CodeProgram()

int32_t HsmClient_firmwareUpdate_CodeProgram ( HsmClient_t *  HsmClient,
FirmwareUpdateReq_t *  pFirmwareUpdateObject 
)

service request issued to HSM server to program the incoming firmware to device dormant banks This service is valid only for F29H85x SOC

Parameters
HsmClient[IN] Client object which is using this API.
pFirmwareUpdateObject[IN] Pointer to arguments to be passed to HSM core via SIPC.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_firmwareUpdate_CodeVerify()

int32_t HsmClient_firmwareUpdate_CodeVerify ( HsmClient_t *  HsmClient,
FirmwareUpdateReq_t *  pFirmwareUpdateObject 
)

service request issued to HSM server to decrypt the firmware programmed in dormant flash bank in place, perform integrity checks on the decrypted firmware and program the certificate in flash memory This service is valid only for F29H85x SOC

Parameters
HsmClient[IN] Client object which is using this API.
pFirmwareUpdateObject[IN] Pointer to arguments to be passed to HSM core via SIPC.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_VerifyROTSwitchingCertificate()

int32_t HsmClient_VerifyROTSwitchingCertificate ( HsmClient_t *  HsmClient,
uint8_t *  cert,
uint32_t  cert_size,
uint32_t  timeout 
)

service request issued to HSM server to validate RoT Switching Certificate

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this RoT Switching API.
cert[IN] point to the location of certificate in the device memory.
cert_size[IN] size of certificate.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_UpdateKeyRevsion()

int32_t HsmClient_UpdateKeyRevsion ( HsmClient_t *  HsmClient,
uint32_t  timeout 
)

service request issued to HSM server to update key revision to 0x2 which changes the root of trust key from secondary keys to back up keys.

Parameters
timeout[IN] amount of time to block waiting for semaphore to be available, in units of system ticks (see KERNEL_DPL_CLOCK_PAGE)
HsmClient[IN] Client object which is using this RoT Switching API.
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.
  3. SystemP_TIMEOUT if timeout exception occours.

◆ HsmClient_configOTFARegions()

int32_t HsmClient_configOTFARegions ( HsmClient_t *  HsmClient,
OTFA_Config_t *  OTFA_ConfigInfo,
uint32_t  timeout 
)

Client request to configure the OTFA regions.

Parameters
HsmClient[IN] HsmClient object
OTFA_ConfigInfo[IN] OTFA Config Info
timeout[IN] timeout
Returns
  1. SystemP_SUCCESS if returns successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_readOTFARegions()

int32_t HsmClient_readOTFARegions ( HsmClient_t *  HsmClient,
OTFA_readRegion_t *  OTFA_readRegion,
uint32_t  timeout 
)

Client request to read the OTFA regions.

Parameters
HsmClient[IN] HsmClient object
OTFA_readRegion[IN] OTFA Read Region
timeout[IN] timeout
Returns
  1. SystemP_SUCCESS if reading done successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_secCfgValidate()

int32_t HsmClient_secCfgValidate ( HsmClient_t *  HsmClient,
SecCfgValidate_t *  pSecCfgParams,
uint32_t  timeout 
)

Client request to validate sec-cfg Valid only for F29x family of devices.

Parameters
HsmClient[IN] HsmClient object
pSecCfgParams[IN] Sec-Cfg object
timeout[IN] timeout
Returns
  1. SystemP_SUCCESS if validation done successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_activeToDormantBankCopy()

int32_t HsmClient_activeToDormantBankCopy ( HsmClient_t *  HsmClient,
FlashBankCopy_t *  pFlashBankCopyObject,
uint32_t  timeout 
)

Client request to copy active flash bank contents to dormant flash bank Valid only for F29x family of devices.

Parameters
HsmClient[IN] HsmClient object
pFlashBankCopyObject[IN] Flash Bank copy object
timeout[IN] timeout
Returns
  1. SystemP_SUCCESS if copy done successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_SecCfgUpdate()

int32_t HsmClient_SecCfgUpdate ( HsmClient_t *  HsmClient,
FirmwareUpdateReq_t *  pFirmwareUpdateObject 
)

Client request to update device Sec-Cfg Valid only for F29x family of devices.

Parameters
HsmClient[IN] HsmClient object
pFirmwareUpdateObject[IN] Pointer to arguments to be passed to HSM core via SIPC.
Returns
  1. SystemP_SUCCESS if copy done successfully
  2. SystemP_FAILURE if NACK message is received or client id not registered.

◆ HsmClient_getDeviceConfig()

int32_t HsmClient_getDeviceConfig ( HsmClient_t *  HsmClient,
DeviceConfigRead_t *  pDeviceConfigObject,
uint32_t  timeout 
)

Client request to get device configuration from HSM This is a blocking call that waits for HSM response.

Parameters
HsmClient[IN] HsmClient object
pDeviceConfigObject[IN] Pointer to device config read request structure
timeout[IN] Timeout in system ticks
Returns
  1. SystemP_SUCCESS if operation successful
  2. SystemP_FAILURE if NACK received or client not registered
  3. SystemP_TIMEOUT if timeout occurs

◆ HsmClient_CryptoService()

int32_t HsmClient_CryptoService ( HsmClient_t *  HsmClient,
CryptoServiceReq_t *  svcReq,
uint32_t  timeout 
)

Submit a generic crypto service request to the HSM. Set svcReq->algoId to the algorithm (HSM_CRYPTO_SVC_MAC_CMAC, etc.) and svcReq->subSvcId to the operation (HSM_CRYPTO_SVC_MAC_GENERATE, etc.). Set svcReq->keyId to the keyring index and point svcReq->ptrArgs at the corresponding args struct (e.g. CMACArgs_t).

Parameters
HsmClient[IN] HsmClient object
svcReq[IN/OUT] Pointer to CryptoServiceReq_t; for generate operations, output is written to ptrTag on success
timeout[IN] Timeout in ticks (SystemP_WAIT_FOREVER to block)
Returns
SystemP_SUCCESS on ACK, SystemP_FAILURE on NACK or error.

◆ HsmClient_runTimeBankSwap()

int32_t HsmClient_runTimeBankSwap ( HsmClient_t *  HsmClient,
BankSwapReq_t *  pBankSwapObject 
)

Client request to Swap C29 CPU flash banks Valid only for F29x family of devices.

Parameters
HsmClient[IN] HsmClient object
pBankSwapObject[IN] Pointer to arguments to be passed to HSM core via SIPC.
Returns
  1. SystemP_SUCCESS if message sent successfully
  2. SystemP_FAILURE if message not sent.